Skip to main content

Wood ledger board

Posted by ROBERT SCHMITZover 4 years ago
Wood ledger board

Is it possible to use PROFIS to model a wood ledger board attached to a masonry or concrete wall? Such as a wood deck to a foundation wall.

use HILTI profis softvare,wood deck ledger

1 Reply
Posted by Emily over 4 years ago
Hilti Verified

Hi Robert,

Steel ledger angles per AISC standards can be modeled within PROFIS Engineering under the anchor plate tab. Wood ledger angles and wood anchor plates are not currently an option within the software.

Regards,
Emily


1 comment on this reply
Posted by ROBERT SCHMITZover 4 years ago
Hello Emily, I realize that but to get an idea I used a 1 1/2" thick plate 11.25" (2 x 12) by 20" long plate loaded with a 1" thk plate in the middle (T-shaped config.) also anchored to concrete FDN wall. Distribution to anchors probably not equal due to wood versus steel, 4 bolt arrangement, 2 each side of load. This would be an application Hilti should consider adding.