Skip to main content

What is the minimum gap/space required to install 9 inch long HDA-T anchor?

Posted by PRBHASH SHAHover 2 years ago
What is the minimum gap/space required to install 9 inch long HDA-T anchor?

When installing anchors in confined space; for example, between two walls (1 ft inward from the outside face), or slab opening, what should be the minimum gap required to be able to install HDA-T anchor?
What's minimum size of drill chuck assembly?

Thank you

installation equipment,HDA-T undercut anchor

1 Reply
Posted by Ashley Couronover 2 years ago
Hilti Verified

Hi Prbhash,

In order to provide the best assistance, please reach out to hnatechnicalservices@hilti.com and include the tool that you are planning on using for the installation as well as the diameter of the HDA-T.

Regards,
Ashley

HDA-T undercut anchor