Skip to main content

We are designing anchorage for a 20,000 lb Electron Mocroscope. The vendor is requesting 16mm HIS-N anchors at 2-3/8 spacing. Is this possible?

Posted by tony moorealmost 2 years ago
We are designing anchorage for a 20,000 lb Electron Mocroscope. The vendor is requesting 16mm HIS-N anchors at 2-3/8 spacing. Is this possible?

ESR-3814 specifies minimum center-center spacing for 16mm HIS-N anchors as 5"
The electron microscope that we are trying to anchor has anchor hole spacing of 2-3/8"
The microscope vendor is specifying the HIS-N anchors. Can this be installed with a reduced allowable load?

anchor,load,spacing,reduced

1 Reply
Posted by Mia Brownellalmost 2 years ago
Hilti Verified

Hi Tony,

Load adjustment factor tables for Hilti’s HIT-RE 500 V3 adhesive and the HIS-N internally threaded insert can be found on page 138 of the Anchor Product Technical Guide. The decision to install the HIS-N anchor bolts at a spacing smaller than what is published is ultimately at the discretion of the Engineer of Record on the project.

If you have any further questions, please reach out to hnatechnicalservices@hilti.com.

Best,
Mia

HIT-RE 500 V3,anchor spacing,HIS-N