Skip to main content

Void at Non-Rated Exterior Wall / Non-Rated Floor Intersection

Posted by Kenneth Filarabout 4 years ago
Void at Non-Rated Exterior Wall / Non-Rated Floor Intersection

We have a project where we're being asked to close the void at all of the Non-Rated Exterior Wall / Non-Rated Floor Intersections, despite the fact that these floors have been chosen to be open to each other without shaft protection (most of the upper floor level looks down into the floor below). What section of the code would allow the void to remain open?

Void,intersection,non-rated

1 Reply
Posted by JESSICA STARKSabout 4 years ago
Hilti Verified

Kenneth,

I am not sure if you are using the IBC Code, but 2018 Version of IBC Code addresses this. This would be Section 715.4.1 (and section 715.5 for the 2021 IBC Code). The code states that "[v]oids created at the intersection of exterior curtain wall assemblies and nonfire-resistance-rated floor or floor/ceiling assemblies shall be sealed with an approved material or system to retard the interior spread of fire and hot gases between stories." This tells us that something--whatever the "approved material" may be--does need to be installed at that joint intersection.

If you want documentation for a non fire-rated solution showing an "approved material," we can address your application through an Engineering Judgment, which will be a custom detail showing your exact application with the firestop components required to maintain the stated ratings.
 
We are proud to announce the launch of the HILTI CONSTRUCTION PLATFORM (HCP), our company’s new engineering service website. This platform will be the home for all of your Fire Protection Design needs. Instead of emailing a PDF form for a request, the platform enables you to create new Engineering Judgment (EJ) requests, submit revisions to previously completed EJs or connect with an FPE on a question. HCP also enables you to track the status of your request.

You can find more information on how to access this new platform here: http://www.hilti.com/ej (US) or http://www.hilti.ca/ej (Canada.) If you have any questions or require assistance navigating the platform, please call Customer Service for help at 1-800-879-8000 (US) or 1-800-363-4458 (Canada.)
 
Along with HCP, Hilti is excited to announce our new mobile app for all your firestop needs: Hilti Firestop Selector. Using the Firestop Selector app gives you easy access to the Hilti Fire Protection Design Team from the jobsite, on the road, or in the office to request a new EJ, an EJ Revision, or a Question anytime, anywhere. You can download the app using the appropriate link below.

Hilti Firestop Selector App – Google Play Store

Hilti Firestop Selector App – Apple App Store

If you have any questions, please reach out to our customer service team at 1-800-879-8000 (US) or 1-800-363-4458 (Canada) for assistance.
 
Best regards,
 
Fire Protection Design Team
Hilti North America

curtain wall,IBC 715.4.1

1 comment on this reply
Posted by Kenneth Filarabout 4 years ago
It's the intent that always seems illogical to me here. We have two floors that are nearly completely open to each other; therefore, retarding "the interior spread of fire and hot gases between stories" doesn't seem relevant. Is it just that this section of the Code makes no reference to the two adjacent stories open to each other, and we have to follow through with this seemingly illogical requirement?