Skip to main content

Use of a torque test to determine tension load capacity of installed bolt

Posted by Kenna Chapinalmost 2 years ago
Use of a torque test to determine tension load capacity of installed bolt

We have a contractor who did not get special inspection for Hilti HY270 anchors during installation. They have asked if the anchors can be checked using torque versus a traditional pull test. We do not see any information that notes this as an acceptable test method for testing the tension on the bolts. Does Hilti have any opinion on this.

adhesive,Torque

1 Reply
Posted by Mia Brownellalmost 2 years ago
Hilti Verified

Hi Kenna,

For more information on special inspections, please reference the Special Inspections Guidelines for Post-Installed Anchors - Ask HILTI article. 

If you have any further questions, please reach out to deck@hilti.com

Best,
Mia