Skip to main content

Torque Testing Loads

Posted by Taylor Cardinaleover 1 year ago
Torque Testing Loads

I am trying to specify a load for Torque testing of KB-TZ2 expansion anchors. We need to specify the torque test for carbon steel, stainless and conditions into metal deck and any other possible condition on the project. In the ICC report for the KB-TZ2, values for installation torque are reported. Is the installation torque also the torque value that we should be testing our anchors at on-site? Is there any resource that can give us more information on the torque testing procedure and the target loads that we should be referencing? Also what are all of the different conditions that calls for different test values? Does lightweight concrete have a separate testing value?

Expansion Anchor,testing,Torque

1 Reply
Posted by Mia Brownellover 1 year ago
Hilti Verified

Hi Taylor,

Please click here to access an Ask Hilti article that discusses special inspections guidelines for post-installed anchors. Section 4.3.1 specifically discusses special inspection procedures for post-installed mechanical anchors. 

If you have any further questions, please reach out to hnatechnicalservices@hilti.com.

Best,
Mia

Special Inspection,KB-TZ2