Skip to main content

T rating on CP 680 P

Posted by Elizabeth Beattyabout 2 years ago
T rating on CP 680 P

I am being asked to firestop bare plastic, copper with fiber glass insulated pipe, and bare metal pipe, using firestop device CP 680 P through a 4 1/2” concrete floor over metal decking and to hold a T rating of 2 hrs. Are there any 2 hr T rating Hilti systems that involve just the cp 680 P CID sleeves? Or will I need to have an EJ made up?
I thought these CP 680 sleeves had their own UL Hilti System that covered 2 hr T ratings and F ratings

firestop,system,Cp680p

4 Replies
Posted by Nathaniel Crawfordabout 2 years ago
Hilti Verified

Hello Elizabeth - there are a few different systems you can use to address these conditions. Anything not covered by these systems would need to be an EJ.

  • Bare Plastic - F-A-2092
  • Insulated Metallic - F-A-5018
  • Bare Metallic - F-A-1106


Hilti is proud to announce the launch of our engineering website, the HILTI CONSTRUCTION PLATFORM (HCP). This platform will be the home for all of your Fire Protection Engineering needs, including Engineering Judgment requests. You can find more information on how to access this new platform here: hilti.com/ej (US) or hilti.ca/ej (Canada.). There is also a firestop system selector tool available on HCP to search for other systems.

Regards,
Nate Crawford - Lead FPE


Posted by Elizabeth Beattyabout 2 years ago

In a situation like this one, I was told to use the CP680 P sleeves for all floor penetrations 6" and under in diameter.
After ordering the sleeves and the correct sizes and counts, the CM (Turner Construction CO.) Asks me to provide documentation on the CP680P sleeves carrying a 2 hr T rating for all areas/locations that I am using these cp 680p sleeves.
I was under the impression that these sleeves were meant to carry a 2 hr F and T rating within the sleeve itself and that no other material would be needed or added to fufill the systems UL 2 HR T AND F Ratings.
What devise should have been used to fulfill a 2 HR T rating at the floors for all 3 kinds of penetrants, Plastic pipe, Bare Metal Pipe, and Metallic/copper with 1.5" insulation penetrants.


Posted by Elizabeth Beattyabout 2 years ago

Also for instance,
If I have a 1 1/4" copper pipe with 1.5" pvc/ABS insulation or glass fiber (3" in total, 1.5" on either side totallying 3") this would total 5" in diameter for the pipe and require a 6" CP 680P CID correct? Is there a hilti system that would cover insulated pipe through CP 680 sleeves while also carrying a 2 hr T rating and 2 hr F rating at the floor (4 1/2" concrete over metal decking)?
I also have 4" bare metal pipe passing through 4" cp 680 p sleeves that also require a 2 hr T rating. Wouldnt I need an EJ to fufill this 2 HR T rating requirement for these 2 types of pipes and sizes, insulated, bare metal? Thanks


Posted by Elizabeth Beattyabout 2 years ago

Also, for system FA1106 BARE METAL PIPE through CP680 P
This is requesting FYREWRAP insulation be wrapped around pipe 36" above floor. Ive never used FYREWRAP but I have used Hilti EndoThermic Wrap... Hilti does not offer a system for bare metal pipe through CP 680 P using the Hilti Endo Wrap instead of a different brand? Thanks If an EJ could be created using the endothermic Hilti wrap, Id prefer to use that