Skip to main content

Shear Connectors for concrete overlay.

Posted by Allam Mahmoudover 1 year ago
Shear Connectors for concrete overlay.

What is an economical shear connector to connect a concrete overlay to the top of an existing concrete foundation.
I am currently specifying hairpin dowels anchored to the existing foundation using HIT RE-500 V3.
Is there a more economical solution?
This is a relatively large area, so there is a large number of holes to drill and install the dowels in.

dowels,Overlay,Shear connector

1 Reply
Posted by Matthew Fordover 1 year ago
Hilti Verified

Hi Allam,

If you are looking for an alternative adhesive anchoring system, you may consider using HIT-RE 100. For more information, please reference ESR-3829.

For additional assistance, please reach out to hnatechnicalservices@hilti.com or give us a call at 877-749-6337.

Regards,
Matthew

HIT-RE 100