Skip to main content

Roof Deck Fastening Options

Posted by Raghu Guptaabout 1 year ago
Roof Deck Fastening Options

If the roof deck is outside as in over canopy, which fastener would be better in terms of waterproofing? We have mostly specified welds but if Hilti PAF are waterproofed then we can specify that instead.

Fasteners,Roof Deck Diaphragm

1 Reply
Posted by Sinan Beskokabout 1 year ago
Hilti Verified

Hello Raghu,

Exposure to exterior conditions for Hilti’s decking fasteners (the X-HSN 24 and the X-ENP 19) is discussed in Section 5.8 of ESR-2776. The section mentions the addition of corrosion-resistant paint or sealant for permanently exposed steel deck. As an alternate to applying the corrosion-resistant paint or sealant, the SDK2 is an SAE stainless steel sealing cap with a neoprene seal that can be installed over the X-ENP 19 to provide additional corrosion resistance and achieve a water-resistant seal when properly installed. Additional information can be found on page 158 of the Direct Fastening Technical Guide.

Best,
Sinan

decking,X-HSN 24,X-ENP 19,Water-proofing,Sealing