Skip to main content

RisaConnection to PROFIS Import not working

Posted by John Gunvordahlalmost 4 years ago
RisaConnection to PROFIS Import not working

I am having an issue with the RISAConnection and PROFIS import function. I am able to successfully design the base plates in RISAConnection and it says it has successfully exported the connections to PROFIS, but once I get into PROFIS I do not see the "There is a new RISA update for: ["Project Name"]" on the right side below file import. I am currently running a trial version of PROFIS and RISAConnection to test out the functionality of the software and to decide if this is something my company wants to add into our design process. I do have a subscription for RISA3D and I am within the trial windows for RISAConnection and PROFIS. Help with this issue would be greatly appreciated.

RISA Connection Integration,When I log in to Hilti it doesn't prompt me that I have exported my Risa Connection file.

2 Replies
Posted by Emily almost 4 years ago
Hilti Verified

Hi John,

This instructional video details how to transfer designs and load combinations from RISA Connection to PROFIS Engineering. For information on how to activate the RISA interface in PROFIS Engineering, see this previous
Ask Hilti response. For more information on how to get started with RISA Integrations, see this Software
Demo.

If the issue still persists, please email hnatechnicalservices@hilti.com.

Regards,
Emily


Posted by John Gunvordahlalmost 4 years ago

Additionally, I do have RISA checked under the "Interfaces to structural calculation software" settings.