Skip to main content

Quiz for 'roof deck connections & fasteners...

Posted by Lisa Pogueover 2 years ago
Quiz for 'roof deck connections & fasteners...

The quiz asks about dynamic loads and your quiz does not accept snow load as a dynamic load - as a structural engineer this is an incorrect determination, as the load does change over time: "Dynamic loads are those which can change while the structure is in use. These include live loads and operational loads (e.g. vehicles in a car park or crowds of people on a bridge) as well as environmental influences (wind load, snow load)." Once the snow is done falling, the load becomes static. However, that was NOT specified in the quesiton.

Additionally, asking about efficiency times is frustrating - to say puddle welds take 8-12 sec each and powder actuated fasteners take 1-2 secs each means those mechanical fasteners are 6-8 times faster, which encompasses two of the 4 available answers to the question.

Webinar Quiz,need certificate for webinar I attended.

No replies yet

Be the first to reply to this question!