Skip to main content

Proximity of were anchors

Posted by Matthew Erskineover 3 years ago
Proximity of were anchors

I was wondering how close a Kiwi bolt TZ2 wedge anchor 5/8"x6" and 1/2"x4-1/2" can be installed to one another in untracked concrete?

Hilti Kwik Bolts,Hilti Kwik Bolt TZ2

1 Reply
Posted by Danielle Filerover 3 years ago
Hilti Verified

Hi Matthew,

Anchor spacing is dependent on embedment depth and concrete edge distance. You can reference the technical information for the KB-TZ2 here. The greater of the two spacing requirements should be used, since the 5/8" and 1/2" diameter will have different requirements.

Regards,
Dani

Minimum anchor spacings,KB-TZ2