Skip to main content

Profis Anchor Design with Bearing pads under the Base Plate

Posted by Francisco Alonsoabout 2 years ago
Profis Anchor Design with Bearing pads under the Base Plate

Would be possible to update Profis to consider the option of providing 1/4" to 5/8" thick bearing pads (not grouting) under the base plate of a column or beam landing on a base plate? I think Profis only allows a minimum thickness of grouting under the base plate and this is not helpful for applications using bearing pads that are thinner that the minimum grouting thickness.

use HILTI profis softvare,bearing pad,Anchor with thin bearing pad Offset

1 Reply
Posted by Ashley Couronabout 2 years ago
Hilti Verified

Hi Francisco,

Thank you for reaching out and for the feedback. I have submitted the request to the software team for their review.

Regards,
Ashley

Profis engineering software