Skip to main content

Oversized holes

Posted by  Hadialmost 5 years ago
Oversized holes

There is an application of post installed rebar using re 100 or re 500. Ungortunately the client has made 35 mm dia hole for 20 mm rebar, are there any guidlines by hilti for oversized holes ?

ANCHORS,oversized holes,chemcial anchors

2 Replies
Posted by Ashley Couronalmost 5 years ago
Hilti Verified
Hi Hadi,  Here is the link to the technical data for HIT-RE 500 V3. The technical data includes tested embedment depth ranges, hole depth and nominal drill bit diameter requirements. Here is the link to the technical data for HIT-RE 500 V3 with oversized holes. Additionally, here is the link to the Instructions for Use for HIT-RE 500 V3. Regards, Ashley

1 comment on this reply
Posted by  Hadialmost 5 years ago
Hi Ashley, The link to the technical data is not working, the file is missing.

Posted by Ashley Couronalmost 5 years ago

Hi Hadi,
 
Here is the link to the Instructions for Use for HIT-RE 500 V3.
 
Regards,
Ashley