Skip to main content

On a large circular base plate, all the shear load shown as acting on only 1 anchor

Posted by Toby Polocoserover 3 years ago
On a large circular base plate, all the shear load shown as acting on only 1 anchor

I have a 72" diameter base plate with 16 anchors around the circumference at a diameter of 63". When checking a shear and overturning force, the calc package from Hilti Profis Engineering shows that it is checking the entire shear force against the capacity of only one anchor and it says the anchorage is failing due to the edge condition. Why is it checking all the load against only one anchor when the breakdown of loads, the V table, clearly shows that each anchor gets a portion of the loading?

shear,bad calculation

2 Replies
Posted by Emily over 3 years ago
Hilti Verified

Hi Toby,

Please see page 204 of the PROFIS Engineering design guide for information on how the software calculates concrete breakout failure in shear.

Regards,
Emily

Concrete breakout,shear area of concrete breakout

1 comment on this reply
Posted by Toby Polocoserover 3 years ago
Sorry, but I've read through that description completely and there is still a discrepancy between the report and the value it should be calculating. The report is using Vcb instead of Vcb,g, which the description you provided claims it should be checking. Please take a close look at everything I have submitted. Thank you.

Posted by Emily over 3 years ago
Hilti Verified

Hi Toby,

Please send your .pe file to hnatechnicalservices@hilti.com for further review.

Regards,
Emily