Skip to main content

Multiple Non Metallic Pipe Through Slab 50Pa

Posted by Brian Brittonover 6 years ago
Multiple Non Metallic Pipe Through Slab 50Pa

Hi Matt, I was at your facility last week to the HFSC Level II Workshop. Great facility and fantastic presentations from all your staff. In particular, I really enjoyed "Johnny V's", Matt Winston's and your presentations. I was hoping that I could pick your brain with a firestop question. I know that there are probably no systems for multiple non metallic pipes through concrete slab with 50Pa but I might as well ask the expert anyways. I'm looking to see if Hilti has a system for two 1/2" PEX pipes penetrating a 2" cored hole through concrete slab requiring a two hour rating with 50Pa requirements. I have a hunch what the answer is but thought I'd ask anyways. Any feedback you can provide would be greatly appreciated.

Multiple Pex,50Pa

1 Reply
Posted by Matt Bakerover 6 years ago
Hilti Verified

Hi Brian,

For that particular condition we would need to evaluate if we can provide an EJ based on the 50 Pa requirement. Please see the attached EJ form and let's work together through the FPE team email usfirestopeng@hilti.com

Thanks,
Matt

EJ,50Pa