Skip to main content

Minimum torque for KH-EZ 3/8

Posted by Paul Klarcalmost 2 years ago
Minimum torque for KH-EZ 3/8

Requesting minimum torque for KH-EZ 3/8" X 4" into concrete . researched and found the max torque value ( 40# but need the minimum. this is being questioned by an inspector on a school project

KH-EZ 3/8,minimum torque

1 Reply
Posted by Sinan Beskokalmost 2 years ago
Hilti Verified

Hi Paul,

There is not a range of installation torque for the KH-EZ screw anchor as the installation torque value specified in ESR-3027 and the Instructions For Use in concrete is the value that should be applied. An important note, however, is that the KH-EZ screw anchor is not torque-controlled like expansions anchors. Screw anchors instead rely on keying to develop the capacity. The torque is to ensure the fastened material is properly clamped.

If you have any further questions, please reach out to hnatechnicalservices@hilti.com.

Best,
Sinan

ANCHORS,KH-EZ,Torque,minimum,Screw anchor