Skip to main content

mechanical anchors, exterior cold regions

Posted by KEVIN MILEYover 2 years ago
mechanical anchors, exterior cold regions

Mechanical anchors installed in vertical condition in cold climates subject to freezing.
Is there concern about water seeping into the annular gap between the anchor & concrete?
Specifically we have concerns about potential freeze-thaw damage.
Can the anchors be jacked-up out of the hole?
Freeze-thaw damage to concrete around the hole?

We use larger diameter 3/4" minimum in anchors with primarily continuous tension in such applications. The top of the anchor is exposed and not sealed in any manner.

exterior,Mechanical Fastener,Cold Climate,Freezing Envirnoments

No replies yet

Be the first to reply to this question!