Skip to main content

is Profis capable of designing the Cast in place Cell tower anchor bolts with heavy hex nuts and templates at bottom, if so what diameter of the bolts it can handle.

Posted by Uma Atluriover 3 years ago
is Profis capable of designing the Cast in place Cell tower anchor bolts with heavy hex nuts and templates at bottom, if so what diameter of the bolts it can handle.

Cell towers use these kind of Anchor Bolts(A36, A572, F1554-105) with cast in place, with heavy hex nuts and with a minimum of 5' embedment into concrete. Can we design or Analyze using your Profis with these scenarios? Please advise. if not, do you have any plan to include these in your future software upgrades?

anchor bolts,Anchored to drilled pier foundation

1 Reply
Posted by Ashley Couronover 3 years ago
Hilti Verified

Hi Uma,

There are cast-in place anchoring options in PROFIS Engineering. If they are not showing up, you may have a filter selected that is causing them to be hidden from the anchoring options. If you clear the filters and still do not see them as an option, feel free to email your ".pe" file to hnatechnicalservices@hilti.com.

Regards,
Ashley

Profis engineering software,cast-in place