Posted by Kevinover 3 years ago
Is it acceptable to reuse Kwik Bolt TZ anchors in the original hole?
A steel angle was fastened to a concrete wall with Hilti Kwik Bolt TZ anchors with the steel angle 1 1/2" too low. I am curious if the steel angle can be replaced with a taller angle and reuse the original anchors.
1 Reply
Posted by Ashley Couronover 3 years ago
Hi Kevin,
The KB-TZ anchors cannot be reused. Additionally, if a KB-TZ is removed, the same hole should not be used due to potential damage to the concrete and the original hole.
Regards,
Ashley