Skip to main content

Intumescent Paint - Achieving 3 Hours

Posted by Mateo Aristizabalabout 4 years ago
Intumescent Paint - Achieving 3 Hours

Is it possible to achieve a 3hr fire rating with intumescent paint on a HSS membrane? If so what UL # can be used?

Steel beam fireproofing,light weight concrete,ANSI/UL listed,hollow steel section

1 Reply
Posted by Perla Salcedoabout 4 years ago

Hello Mateo, thank you for your question. To determine if a 3 hour rating is possible we would need to know the HSS size. Please email usspeng@hilti.com with the steel size information to help you determine the mil thickness required for that rating. HSS members reference UL Y634 for Fire Finish 120 CFP SP WB and Y657 for All Weather High Build CFP-SP.

Thank you,

Perla V. Salcedo, MS
Testing and Sales Support Engineer
Hilti North America
Irving Testing and Development Lab: 3701 W. Royal Lane, Suite 100, Irving, TX 75063
E: Perla.Salcedo@hilti.com
W: www.hilti.com


1 comment on this reply
Posted by Mateo Aristizabalabout 4 years ago
Thanks Perla, just to be clear this is a HSS Steel "tube" not "column" as inidicated in UL Y634. I will email the steel size information to the email provided!