Skip to main content

Intumescent coating type in Plenum space of semi-conductor clean room

Posted by Jinsu Baeover 2 years ago
Intumescent coating type in Plenum space of semi-conductor clean room

I am looking for a appropriate intumescent coating (2 hr) types for the plenum space of semi-conductor clean room, and roof structure (trusses) above the plenum. The plenum has more than 20 CFM/CF/minute air flow with temperature/humidity controled. And the roof structure space do not have controled temperature/humidity. It's located in central Texas, so uncontroled space will have 120 °F and 85% humidity. I am looking at epoxy base or solvent base ones. Chemical resistance would be premium - lots of chemicals (solvent, acid, etc.) are used.

2 hr intumescent coating types,semi-conductor clean room,Temperature & humidity controlled and non-controlled spaces

1 Reply
Posted by Chase Hellanover 2 years ago

Hello unfortunately Hilti currently does not have any products that would meet your application. Our steel protection products are designed to protect structural steel and are not able to be used  to protect plenum spaces / roof structures. Please let me know if you have any questions or concerns.

I also have included the Hilti field steel protection specialist who may be able to help as as well.
John Meadows
Steel Protection Specialist 

C: 314-224-9813 | E: john.meadows@hilti.com


Thank you Chase
Sr. Fire Protection Engineer


1 comment on this reply
Posted by Jinsu Baeover 2 years ago
Thank you, Chase.