Skip to main content

Insulated system 15 pvc through concrete / gypsum

Posted by Randy Loveabout 4 years ago
Insulated system 15 pvc through concrete / gypsum

Can you please provide a detail on how to properly fire rate insulated (example 65mm thickness) System 15 PVC, with metal sleeve through concrete and gypsum

insulated plastic,PVC Pipe penetration

1 Reply
Posted by Jose Hernandezabout 4 years ago
Hilti Verified

Hello,

In Canada plastic pipe penetrations are required to be tested with a 50 Pa pressure in the furnace which makes plastic pipes a much bigger challenge when it comes to fire resistance ratings.

We have no testing that would allow for us to address System 15 XFR-PVC with insulation through a gypsum wall or a concrete wall with this 50 Pa rating. The insulation will need to be completely removed from the pipe through the opening in the wall assembly and the firestopping materials that are installed to address the pipe.

I have attached the cUL listing CAJ-2053 which shows how we can address the system 15 XFR-PVC pipe without the insulation. If you would like this same detail in a gypsum wall assembly you will need to submit for an engineering judgement requested through the Hilti Construction Platform (Instructions for signing up below).

--------------------------------------------------------------------------------------------------------------------------------------------------

We can address your application through an Engineering Judgment which will be a custom detail showing your exact application with the firestop components required to maintain the stated ratings.
 
We are proud to announce the launch of the HILTI CONSTRUCTION PLATFORM (HCP), our company’s new engineering service website. This platform will be the home for all of your Fire Protection Design needs. Instead of emailing a PDF form for a request, the platform enables you to create new Engineering Judgment (EJ) requests, submit revisions to previously completed EJs or connect with an FPE on a question. HCP also enables you to track the status of your request.

You can find more information on how to access this new platform here: http://www.hilti.com/ej (US) or http://www.hilti.ca/ej (Canada.) If you have any questions or require assistance navigating the platform, please call Customer Service for help at 1-800-879-8000 (US) or 1-800-363-4458 (Canada.)
 
Along with HCP, Hilti is excited to announce our new mobile app for all your firestop needs: Hilti Firestop Selector. Using the Firestop Selector app gives you easy access to the Hilti Fire Protection Design Team from the jobsite, on the road, or in the office to request a new EJ, an EJ Revision, or a Question anytime, anywhere. You can download the app using the appropriate link below.

Hilti Firestop Selector App – Google Play Store

Hilti Firestop Selector App – Apple App Store

If you have any questions, please reach out to our customer service team at 1-800-879-8000 (US) or 1-800-363-4458 (Canada) for assistance.
 
Best regards,
 
Fire Protection Design Team
Hilti North America

insulation,HCP,Canada,XFR,50 Pa