Skip to main content

How to choose specific anchors for use in PROFIS calculations?

Posted by Chris Lambert10 months ago
How to choose specific anchors for use in PROFIS calculations?

We have a customer who has selected a specific stainless steel threaded rod spec (HAS-R 304 / 316) to be used, and we need to verify it is acceptable with the mounting flange through PROFIS. During the setup for the calculations, it seems impossible to select an appropriate fastener in that family to run the analysis. Is there a method to selecting the exact anchor you wish to test against?

anchor,profis,PART NUMBER

1 Reply
Posted by Mia Brownell10 months ago
Hilti Verified

Hi Chris,

Within the Anchoring to Concrete module in PROFIS Engineering, the anchor can be selected by clicking the "Anchor" tab on the left hand side of the screen (boxed in red below) and the results can be filtered based on your application. If application parameters (i.e. loads, geometry, etc.) are inputted before an anchor is selected, PROFIS will filter out all the anchor options that are not suitable for the application (hence why you may be seeing fewer anchors than normal).



If you have any further questions, please reach out to hnatechnicalservices@hilti.com.

Best,

Mia

anchoring to concrete,profis engineering