Skip to main content

HIT-HY 200 V3 Installation Methods with Threaded Rod

Posted by CHRISTIAN WALDSCHMIDTalmost 3 years ago
HIT-HY 200 V3 Installation Methods with Threaded Rod

Hello, I noticed that in the Product Technical Guide (pg 57), the installation method of diamond core bit with roughening tool was shown to not be acceptable. However, in ESR-4868 (pg 25), diamond core bit with roughening tool is shown to be acceptable as long as the hole is not water filled. Also, Profis shows this to be acceptable under dry hole conditions.

Just to confirm, it is acceptable to use the HIT-HY 200 V3 adhesive with threaded rod with a diamond core drilled hole as long as the roughening tool is used and the hole isn't water filled?

I spoke over the phone with customer service, but I just wanted to confirm to show our contractor.

Thank you,
Christian

roughening tool,HIT-HY 200 V3,HIT-HY 200 V3 HAS Threaded Rod Application

1 Reply
Posted by Ashley Couronalmost 3 years ago
Hilti Verified

Hi Christian,


To confirm, yes, the installation method of using a diamond core bit with roughening tool is acceptable under dry and water saturated concrete conditions per ESR-4868 for Hilti's HIT-HY 200 V3 adhesive anchoring system.

Regards,
Ashley

HIT-HY 200 V3