Skip to main content

HIT-HY 200 V3 Adhesive with HAS Threaded Rod in Core Drilled Holes

Posted by TOM LANGLITZabout 3 years ago
HIT-HY 200 V3 Adhesive with HAS Threaded Rod in Core Drilled Holes

ESR-4868 requires core drilled holes to be roughened with the Hilti TE-YRT roughening tool prior to grouting the threaded rod in the hole. The contractor failed to roughen the surface as required so the anchor has been grouted inside of a smooth hole. Are there reduction factors that can be used to check the anchors as-installed? Are there other options to confirm adequacy of the anchors? These connections are exposed in the final condition so any remediation needs to be architecturally acceptable.

roughening tool,core drilled

1 Reply
Posted by Ashley Couronabout 3 years ago
Hilti Verified

Hi Tom,

If the anchors were not installed per the instructions for use, there are two options that can be considered. You could consider engineering judgement and/or on-site testing to account for variability in performance.

Regards,
Ashley

HIT-HY 200 V3