Posted by Jonathon Comtoisover 2 years ago
Hilti X-U anchor in hollow core plank
Can Hilti X-U fasteners be used in 5,000 psi precast hollow core plank with a minimum thickness of 1.375" at the cores? If so what would the shear capacity be of the anchor, spacing and edge distance requ?
1 Reply
Posted by Ashley Couronover 2 years ago
Hi Jonathan,
Hilti does not have any testing for X-U fasteners installed into precast hollow core plank. The testing that is available for the X-U can be found in Section 3.2.5 of Hilti's Direct Fastening Product Technical Guide.
Regards,
Ashley