Skip to main content

Hilti Post Installed Anchors through cold joint (new concrete over existing concrete)

Posted by Nick Menezesalmost 2 years ago
Hilti Post Installed Anchors through cold joint (new concrete over existing concrete)

I have an existing 9" reinforced slab with a new 9" reinforced slab poured over top. Using Hilti HIT-RE V3 anchor bolt, is it acceptable to install anchor through joint? Due to embedment requirements of tank manufacturer, Anchor will be drilled through entire thickness of new slab and 7 inches into existing slab.

post installed anchor,cold joint

2 Replies
Posted by Hilti Employee13 days ago
Hilti Verified

Hi Quinten,

Thank you for reaching out. Hilti anchor testing is conducted in monolithic slabs only. Thus, Hilti does not have test data available for anchors installed in more than one layer of concrete. Engineering judgment could be considered if the housekeeping pad and supporting slab are sufficiently connected to act as one element. Additional information can be found in the American Concrete Institute (ACI) publication, “Anchoring into Housekeeping Pads,” which was originally published in the Q&A section of the December 2012 issue of Concrete International and can be purchased by clicking here to access ACI online.

Regards,
Kevin

housekeeping,monolithic

Posted by Matthew Fordalmost 2 years ago
Hilti Verified

Hi Nick,

Please refer to this response from a previous question.

Regards,
Matthew

HIT-RE 500 V3,cold joint

1 comment on this reply
Posted by Quinten Sweitzer14 days ago
Could you please provide a response in this thread? The link no longer works.