Skip to main content

Hilti Cast-In-Place Anchors for fall protection

Posted by Stefan Clairalmost 4 years ago
Hilti Cast-In-Place Anchors for fall protection

We use the Hilti Cast-In-Place Anchors on most of our jobsites to reduce overhead work and be more efficient. Once they are installed and concrete is poured, we have to go to the floor below them to install our all-thread. On some of our projects, we are not permitted to drill into the concrete overhead, so we have no means to tie off our fall protection. We are looking for an engineered solution that would allow us to use these cast-in-place anchors as a fall protection anchor. It needs to be able to hold 5,000lbs. Is there a product that you offer (similar to an eyebolt) that would give us this option?

cast-in-place anchors,fall protection

1 Reply
Posted by Emily almost 4 years ago
Hilti Verified

Hi Stefan,

Hilti anchors are not tested for fall protection applications. Typically, customers consider a fall protection system from a manufacturer that specializes in fall protection.

Cheers,
Emily

fall protection anchors