Skip to main content

Finding equivalent Anchor and its strength for the old anchor used

Posted by Samrat Sapkotaover 2 years ago
Finding equivalent Anchor and its strength for the old anchor used

I am working on a design check of anchorage from 1990's where 1-1/4" diameter Hilti HVA Anchors/ HEA resins 304 or 303 SS Thread Rod with 8.25 " embedment in 3000 psi concrete has been used. I wanted to model the same anchorage in Hilti Profis, so do you have the bolts that matches the strength of the previous bolt, also could you provide the strength of those anchor bolts?

Strength,post installed anchor

1 Reply
Posted by Matthew Fordover 2 years ago
Hilti Verified

Hi Samrat,

Unfortunately, discontinued anchors are not available to design with in PROFIS Engineering. The HVU/HVA adhesive anchoring system has been directly replaced by the HVU2 which is available within the software but will have different performance compared to the HVU/HVA.

For additional assistance, please reach out to hnatechnicalservices@hilti.com or give us a call at 877-749-6337.

Regards,
Matthew

HVU,adhesive capsule