Skip to main content

Exterior Wall Assembly EJs

Posted by Dale Yeeover 2 years ago
Exterior Wall Assembly EJs

I have an existing 2-hour rated exterior wall with 2-layers of fire rated gyp on both side and the exterior side also has 1/2" fire treated plywood and cement plaster. I need to upgrade this to a 3-hour rated wall. Can you provide a EJ to achieve the increased rating on the exterior side only?

Engineering Judgments,fire rated exterior wall

1 Reply
Posted by Michael Vuover 2 years ago
Hilti Verified

Hello,

Unfortunately, this goes beyond the scope of what we do at Firestop. We cannot provide guidance on how increase the rating of an assembly, we can only provide a firestop solution after being given the rated assembly. I recommend reaching out to a gypsum manufacturer to see if they are able to help you. Please give us a call at 1-800-879-8000 if you have any further questions.

Thank you,
Michael Vu
Fire Protection Engineering Team
Hilti North America
 
3701 W. Royal Lane, Suite 100 I Irving, TX, 75063P 1-800-879-8000 I F 918-254-1679
E usfirestopeng@hilti.com
www.us.hilti.com/firestop