Skip to main content

Definition of torqued

Posted by BRYCE HANSENover 3 years ago
Definition of torqued

What is the definition of torqued? i.e., how much torque need be applied to consider the anchor torqued?

Single anchor,torqued

1 Reply
Posted by Danielle Filerover 3 years ago
Hilti Verified

Hi Bryce,

I'm not sure I fully understand your question, however the torque requirements vary depending on type and size of anchor. The torque requirements also vary depending on whether it is a torque-controlled anchor such as an expansion anchor, or an adhesive anchor which just has a maximum torque (no minimum torque required). The torque requirements can be found in the instructions for use, which are included in the packaging for every anchor. Additionally, the instructions for use can be found online under the documents section for each anchor. If you have further questions or need assistance with a specific anchor please feel free to reach out to Hilti's engineering team at 877-749-6337.

Regards,
Dani

torque values,installation torque