Skip to main content

CP680 P with a 1 hr T rating

Posted by Elizabeth Beattyabout 2 years ago
CP680 P with a 1 hr T rating

I have attached the projects penetration firestopping requirements.
C.2. states that the T rating 1 HR doesnt apply when inside wall cavities?
I need a cp680 p system for 2" plastic, 3" plastic and 4" plastic all holding at least a 1 HR T rating. I need to also find a system for max insulated 1" copper pipe with 1.5" insulation glass fiber or pvc/
I also need one for a max 4" bare metal floor penetration through floor through a cp680p sleeve that holds a 1 hr T rating as well. Can I get a system for all three of those that also gives me a T rating of 1 HR and follows the forms ive attached? Thanks

Cp680p,1hrtrating

1 Reply
Posted by Chase Hellanabout 2 years ago

Hello, I have attached 3 systems, F-A-5017, F-A-1207 and F-A-2092. FA 5017 only has a 3/4" hr T rating with what you are asking, so that may require an Engineering Judgement (EJ) (see below). F-A-1207 is with endoshield and will provide bare metallic a 1 or 2hr T rating. Finally F-A-2092 is with plastic pipes and will allow for a 2hr T rating. Please be advised the pipe diameter will need to match the correct CP 680; Ie a 4" pipe in a 4" CP 680.
Thank you,
Chase Hellan
Sr. Fire Protection Engineering

We are proud to announce the launch of the HILTI CONSTRUCTION PLATFORM (HCP), our company’s new engineering service website. This platform will be the home for all of your Fire Protection Design needs. Instead of emailing a PDF form for a request, the platform enables you to create new Engineering Judgment (EJ) requests, submit revisions to previously completed EJs or connect with an FPE on a question. HCP also enables you to track the status of your request.

You can find more information on how to access this new platform here: http://www.hilti.com/ej (US) or http://www.hilti.ca/ej (Canada.) If you have any questions or require assistance navigating the platform, please call Customer Service for help at 1-800-879-8000 (US) or 1-800-363-4458 (Canada.)

Along with HCP, Hilti is excited to announce our new mobile app for all your firestop needs: Hilti Firestop Selector. Using the Firestop Selector app gives you easy access to the Hilti Fire Protection Design Team from the jobsite, on the road, or in the office to request a new EJ, an EJ Revision, or a Question anytime, anywhere. You can download the app using the appropriate link below.

Hilti Firestop Selector App – Google Play Store

Hilti Firestop Selector App – Apple App Store

_________________________

Because of the numerous field conditions encountered, it is not always possible to identify a firestop system that has been tested / classified by a nationally recognized independent testing laboratory (such as Underwriters Laboratories, Underwriters Laboratories of Canada, Factory Mutual, Intertek/Omega Point, etc.). In such a case, an Engineering Judgment (“EJ”) or Firestop Custom Detail (“FCD”) may be appropriate. An EJ/FCD represents a firestop solution that would be expected to pass the stated ratings and requirements if tested.
All Hilti EJ’s/FCD’s are designed in accordance with the International Firestop Council (“IFC”) guidelines. These EJ’s/FCD’s are designed by our experienced degreed fire protection technicians using, as the basis for our opinion:
• relevant 3rd-party testing in accordance with ASTM E-84, ASTM E-119, ASTM E-136, ASTM E-814, ASTM E-1966, ASTM E-2307, CAN/ULC-S115-11, UL 263, UL 723, UL 1479, UL 2079, or ASTM E-2837 • wide-ranging related internal testing of our firestop products, and • extensive knowledge and experience of the performance characteristics of Hilti firestop products, and firestopping technology generally.
Pursuant to IFC guidelines, each EJ/FCD is intended for one specific jobsite, since even slight variances from one application to the next can affect system performance.
Best regards,
Fire Protection Design Team
Hilti North America

3701 W. Royal Lane, Suite 100 I Irving, TX, 75063
P 1-800-879-8000
E usfirestopeng@hilti.com
www.us.hilti.com/firestop