Skip to main content

Comparison of two 4-bolt configurations that gives (me) unexpected results.

Posted by Pascal Hayesover 2 years ago
Comparison of two 4-bolt configurations that gives (me) unexpected results.

Please see the attached file with the results from a shelf angle analysis. Both have 4 bolts. The one with two bolts in the tension zone is satisfactory. The one with 4 bolts in the tension zone is not. See my note at the bottom of page 1. For what it's worth, the intent of this thing is to support the end of a 50 cm x 30 cm concrete beam that frames into a 200 mm thick concrete elevator shaft wall. I am trying to reduce bending on the wall and transfer only shear to the wall. I can't say I've ever designed something like this before but this "angle" option seems to be the easiest to analyze. The concrete beam is modeled with a pinned end at this location so I am only transferring shear and no moment. Thank you gentlemen.

Hilti PROFIS,Cone failure,Load Comparison,Tensile bolt forces

1 Reply
Posted by Ashley Couronover 2 years ago
Hilti Verified

Hi Pascal,

For further assistance, please email your ".pe" file to hnatechnicalservices@hilti.com. We will review your file and provide feedback on your questions.

Regards,
Ashley

Profis engineering software