Skip to main content

Coated fire board installed within the lining of a flexablie dry line wall from one side

Posted by Frank Robinsonover 5 years ago
Coated fire board installed within the lining of a flexablie dry line wall from one side

I have a issue on site were we only have access to the compartment wall from one side , Rockwool do a double boarded tested system for this scenario were you install one board seal and then a further board and seal all from one side of the wall, the opening is fully lined out with small services passing through. Do Hilti offer a similar tested system.

One sided application.,1 hour firestop,Penatration seals

1 Reply
Posted by Chase Hellanover 5 years ago
Hilti Verified

Hello if you can provide a picture along with your description to USfirestopeng@hilti.com we can take a look at this and determine if this is something HILTI will be able to provide a solution for (or if we have one).

Thank you,
Chase
Fire Protection Engineer

firestopping,Penetration