Skip to main content

Anchors on top of metal deck/conc fill for seismic

Posted by Daniel Espinoalmost 4 years ago
Anchors on top of metal deck/conc fill for seismic

Hi,

I just need an anchor for shear to be used on top of 2" metal deck with 2 1/2" concrete fill (NW) for seismic. My shear is 1063 lbs with plenty of edge distance but Profis is saying that there are no anchors for this condition. There is no uplift or tension. Am I missing anything? i

concrete-over-metal deck,seismic anchor

1 Reply
Posted by Emily almost 4 years ago
Hilti Verified

Hi Daniel,

It may have to do with the seismic tension type selected. Changing seismic settings may allow anchors to be selected. See this Previous Ask Hilti response for more information on seismic provisions.

Regards,
Emily

seismic provisions,Concrete over metal deck,anchor availability