Skip to main content

Anchoring to the Top of a Concrete Filled Deck?

Posted by Vincent DeVitaalmost 5 years ago
Anchoring to the Top of a Concrete Filled Deck?

I'm designing an anchor to be installed to the top of a concrete filled metal deck. The program does not let me choose the "top" option, only the "flute" options. Can a Hilti KB TZ2 be installed to the top of a concrete filled deck?

steel deck,Top

3 Replies
Posted by Ashley Couronalmost 5 years ago
Hilti Verified

Hi Vincent,
 
Per ESR-4266, the KB-TZ2 can be installed into the top of concrete over metal deck. The option for installation in the top of concrete over metal deck can be found under the Base Material tab in PROFIS Engineering.

Regards,
Ashley


Posted by ROSS KLEINover 3 years ago

The option to do this is grayed out and when I go to select it a red "not allowed" symbol appears.


Posted by Michael Hammontreeover 3 years ago

I am also experiencing this issue. It would be nice if the Hilti rep actually read the initial post and followed up.