Skip to main content

Adhesive anchors to underside of metal deck

Posted by Daniel Huerfanoover 3 years ago
Adhesive anchors to underside of metal deck

I am trying to install a fastener (Most likely an anchor rod) to the underside of metal deck. The purpose is for this anchor to support a swing inside an office space via eye bolts or other type of system that would attach to the adhesive set rod. However, Profits only provides values for mechanical anchors (such as a Kwik Bolt), which prevent me from attaching the system to the anchor directly.

concrete-over-metal deck,adhesive bond capacity

1 Reply
Posted by Emily over 3 years ago
Hilti Verified

Hi Daniel,

Adhesive anchors do not have testing into concrete-over metal deck which is why they are not an option in PROFIS Engineering.



Because your application falls outside the scope of the product’s testing, we have seen engineers use methods like onsite testing to help determine if the connection is acceptable. Ultimately, all design decisions are at the discretion of the Engineer of Record (EOR) on the project.

Regards,
Emily



COMD