PM 50MG‑22
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol
.
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
![]() |
Hilti Li‑ion battery |
![]() |
Hilti charger |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbers in illustrations refer to important work steps or to components important for the work steps. In the text, the corresponding numbers draw attention to these work steps or components, e.g. (3) . |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
This symbol is intended to draw your special attention to certain points for handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
Direct current (DC) |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use |
![]() |
Pendulum locked (laser beam inclined) |
![]() |
Pendulum unlocked (self-leveling system active) |
Sticker on the product
Laser information![]() |
LASER RADIATION! DO NOT LOOK INTO THE LASER BEAM! LASER CLASS 2 PRODUCT. Laser class 2 based on standard IEC60825-1 / EN60825-1:2014 and compliant with CFR 21 § 1040 (Laser Notice 56). |
Product information
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_SYM-Logo_M_M_DEU_Hilti-Logo.jpg)
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationMulti-line laser PM 50MG-22 Generation 01 Serial no.
Declaration of conformity
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_Konform.jpg)
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions, measuring tools
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_SYM-General_M_M_DEU_Gefahr.jpg)
Keep all safety precautions and instructions for future reference.
Work area safety
- Keep your workplace clean and well lit. Cluttered or poorly lit workplaces invite accidents.
- Do not operate the product in explosive atmospheres, such as in the presence of flammable liquids, gases or dust.
- Keep children and other persons clear when the product is in use.
- Use the product only within its specified limits.
- Comply with your national accident prevention regulations.
- Do not expose the product to rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
- Although the product is protected against the entry of moisture, it should be wiped dry before being put away in its transport container.
- Stay alert, watch what you are doing and use common sense when operating a measuring tool. Do not use a measuring tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the measuring tool can result in serious personal injury.
- Avoid unusual body positions. Keep proper footing and balance at all times.
- Wear personal protective equipment. Wearing personal protective equipment reduces the risk of injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- Avoid accidental starting. Make sure that the measuring tool is switched off before connecting it to the battery and before picking it up or carrying it.
- Use the product and accessories in accordance with these instructions and in the way specified for this special type of tool. Take the working conditions and the work to be performed into account. Use of products for applications different from those intended could result in hazardous situations.
- Do not lull yourself into a false sense of security and do not flout the safety rules for measuring tools, even if you are familiar with the measuring tool after using it many times. Carelessness can result in serious injury within a fraction of a second.
- Do not use the measuring tool in the vicinity of medical devices.
- Use the product and accessories only when they are in perfect working order.
- Store measuring tools out of reach of children when not in use. Do not allow persons who are not familiar with the product or these instructions to operate it. Measuring tools are dangerous in the hands of inexperienced persons.
- Measuring tools need care and attention. Check that moving parts operate satisfactorily and do not jam, and make sure that no parts are broken or damaged in such a way that the measuring tool might no longer function correctly. Have damaged parts repaired before using the measuring tool. Many accidents are caused by poorly maintained measuring tools.
- Do not under any circumstances modify or tamper with the product. Changes or modifications not expressly approved by Hilti may restrict the user’s authorization to operate the product.
- Check the accuracy of the measuring tool before using it for important measurements, and if it has been dropped or subjected to other mechanical stresses.
- Due to the measuring principle employed, the results of measurements can be negatively affected by certain ambient conditions. These include, for example, the proximity of devices that produce strong magnetic or electro-magnetic fields, vibrations and temperature changes.
- Rapidly changing measuring conditions can falsify the results.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use. Big differences in temperature can lead to incorrect operation and incorrect results.
- When adapters or accessories are used, make sure they are mounted securely.
- The measuring tool is designed for the tough conditions of jobsite use, but as with other optical and electrical products (e.g. binoculars, spectacles, cameras) it must be handled with care.
- The specified operating and storage temperatures must be observed.
Additional safety instructions for laser measuring tools
- Laser radiation in excess of Class 2 can be emitted if the product is opened without correct procedure being followed. Have the product repaired only by Hilti Service.
- Secure the area in which you will be taking measurements. While setting up the product, make sure that you do not direct the laser beam toward yourself or others. Laser beams should be projected well above or well below eye height.
- Keep the laser exit window clean in order to avoid measurement errors.
- Check the accuracy of the product before use and several times during use.
- Readings taken in the vicinity of reflective objects or surfaces, through panes of glass or similar materials can falsify the result of measurement.
- Mount the product on a suitable holder or bracket or on a tripod, or set it on a smooth, level surface.
- Do not work with surveyor's staffs in the vicinity of high-voltage electricity cables.
- Make sure that no other laser measuring tool that can influence your measurements is in use in the vicinity.
- Do not permit the laser beam to project beyond the controlled area.
Additional safety instructions
- Risk of injury by falling tools and/or accessories. Before starting work, check that the battery and installed accessories are secure.
- To achieve maximum accuracy, project the line onto a vertical, flat surface. To do so, set up the product at 90° to the surface.
Electromagnetic compatibility
Although the product complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference to the product caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions, or if you are unsure. Likewise, Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment).Laser classification for Class 2 laser products
The product corresponds to Laser Class 2 in accordance with IEC ⁄ EN 60825‑1:2014 and in accordance with CFR 21 § 1040 (FDA). This product may be used without need for further protective measures. Nevertheless, as with the sun, do not look directly into the light source. If you do inadvertently look into the laser beam, immediately close your eyes and move your head clear of the laser beam. Do not aim the laser beam at persons.Careful handling and use of batteries
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Use only batteries that are in perfect working order.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
Description
Product overview
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_Uebersicht.jpg)
- Battery
- Battery status indicator
- Battery release button
- Warning sticker
- Laser exit window
- Receiver mode button
- Line mode button
- Selector switch for ON / OFF and lock / unlock pendulum
- Knob for fine adjustment
Intended use
This tool is a self-leveling multi-line laser level that allows a single person to transfer right angles, level horizontally, carry out alignment work and plumb accurately.
The product is designed for mainly indoor use and is no substitute for a rotating laser. For outdoor use make sure that the boundary conditions are the same as for indoor use, or else use a Hilti laser receiver.Possible applications are:
Marking the position of partition walls (at right angles and in the vertical plane).
Checking and transferring right angles.
Aligning components to be installed or sections of a structure in three axes.
Transferring points marked on the floor to the ceiling.
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_Tabelle_Akku.jpg)
For this product, use only the Hilti Nuron Li‑ion batteries of the B 22 series stated in this table.
For these batteries, use only Hilti chargers of the type series stated in this table.
Features
The product has three green 360° laser lines with a range of up to 40 m (131 ft), and five beam intersection points (front, rear, left, right and above). Range depends on the brightness of ambient light.As viewed from the rear, the product has a reference point directed downward on the left-hand front. The rear is the side where the battery is fitted.
The laser lines can be switched on either separately (vertical or horizontal line only) or together. When used with inclination angle, the pendulum for self-leveling is blocked.
Items supplied
Multi-line laser, toolbox, operating instructions, manufacturer’s certificate.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Information displayed during operation
Status |
Meaning |
---|---|
The laser beam blinks twice every 10 seconds (pendulum not locked) or every 2 seconds (pendulum locked). |
The batteries are almost exhausted. |
The laser beam blinks five times and then remains permanently on. |
Activation or deactivation of receiver mode. |
The laser beam blinks very rapidly. |
The tool cannot level itself. |
The laser beam blinks every 5 seconds. |
Inclined line operating mode; the pendulum is locked, so the lines are not leveled. |
Status indicators of the Li‑ion battery
Hilti Nuron Li-ion batteries can indicate state of charge, fault messages and the battery's state of health.Indicators for state of charge and fault messages
Short-press the release button of the battery to get whichever of the following status indications is applicable at the time.State of charge and, if applicable, faults are indicated constantly as long as the connected product is switched on.
Status |
Meaning |
---|---|
Four (4) LEDs show constantly green |
State of charge: 100 % to 71 % |
Three (3) LEDs show constantly green |
State of charge: 70 % to 51 % |
Two (2) LEDs show constantly green |
State of charge: 50 % to 26 % |
One (1) LED shows constantly green |
State of charge: 25 % to 10 % |
One (1) LED slow-flashes green |
State of charge: < 10 % |
One (1) LED quick-flashes green |
The Li-ion battery is completely discharged. Recharge the battery. If the LED again starts quick-flashing after the battery has been charged, consult Hilti Service. |
One (1) LED quick-flashes yellow |
The Li-ion battery or the product in which it is inserted is overloaded, too hot or too cold, or experiencing some other fault. Bring the product and the battery to the recommended working temperature and do not overload the product when it is in use. If the message persists, consult Hilti Service. |
One (1) LED shows yellow |
The Li-ion battery and the product in which it is inserted are not compatible. Consult Hilti Service. |
One (1) LED quick-flashes red |
The Li-ion battery is locked and cannot be used. Consult Hilti Service. |
Indicators showing the battery's state of health
To check the battery's state of health, press the release button and hold it down for longer than three seconds. The system does not detect a potential malfunction of the battery due to misuse, for example battery dropped or pierced, external heat damage, etc.Status |
Meaning |
---|---|
All LEDs show in sequence, followed by one (1) LED showing constantly green. |
The battery can remain in use. |
All LEDs show in sequence, followed by one (1) LED quick-flashing yellow. |
The check to ascertain the battery's state of health did not complete. Repeat the procedure, or consult Hilti Service. |
All LEDs show in sequence, followed by one (1) LED showing constantly red. |
If a connected product can still be used, the remaining battery capacity is below 50 %. If a connected product can no longer be used, the battery has reached the end of its useful life and has to be replaced. Consult Hilti Service. |
Technical data
Product information
Range of the lines and intersection point without laser receiver |
≤ 40 m (≤ 131 ft - 3 in) |
|
Range, lines and intersection point with laser receiver |
2 m … 65 m (6 ft - 7 in … 213 ft - 3 in) |
|
Self-leveling time (typical) |
3 s |
|
Self-leveling range (typical) |
±4.25° |
|
Accuracy |
±3.0 mm in 10 m (±0.12 in in 32 ft - 10 in) |
|
Line width (typical) |
5 m (16.4 in) |
2.5 mm (0.10 in) |
10 m (32.8 in) |
4.0 mm (0.16 in) |
|
Laser class |
Class 2, visible, 510‑530 nm |
|
Battery life (typical, all lines on) |
B 22‑55 |
14 h at 24 ℃ (14 h at 75 ℉) |
B 22‑85 |
24 h at 24 ℃ (24 h at 75 ℉) |
|
Battery life (typical, only horizontal or vertical lines on) |
B 22‑55 |
22 h at 24 ℃ (22 h at 75 ℉) |
B 22‑85 |
32 h at 24 ℃ (32 h at 75 ℉) |
|
Automatic power-off (activated after) |
1 h |
|
Degree of protection (Does not apply for Nuron B 22 battery) |
IP 54 |
|
Tripod thread |
BSW 5/8" | UNC 1/4" |
|
Beam divergence |
0.05 ... 0.08 mrad * 180° |
|
Average output power (PAE = accessible emission laser output power) |
< 2 mW |
|
Wavelength (λ) |
510 nm … 530 nm |
|
Pulse duration (tp) |
< 80 µs |
|
Pulse frequency (f) |
< 12 kHz |
|
Weight in accordance with EPTA procedure 01, without battery |
1.29 kg |
|
Dimensions (Length x width x height) |
140 mm x 128 mm x 180 mm (5.5 in x 5.0 in x 7.1 in) |
|
Operating status indicator |
Laser beams and Nuron B 22 battery status indicator |
|
Operating temperature |
−10 ℃ … 40 ℃ (14 ℉ … 104 ℉) |
|
Storage temperature |
−25 ℃ … 63 ℃ (−13 ℉ … 145 ℉) |
Battery
Battery operating voltage |
21.6 V |
Weight, battery |
See the section headed "Intended use" |
Ambient temperature for operation |
−17 ℃ … 60 ℃ (1 ℉ … 140 ℉) |
Storage temperature |
−20 ℃ … 40 ℃ (−4 ℉ … 104 ℉) |
Battery charging starting temperature |
−10 ℃ … 45 ℃ (14 ℉ … 113 ℉) |
Preparations at the workplace
Observe the safety instructions and warnings in these operating instructions and on the product.Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the product until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the battery release button.
- Remove the battery from the product.
Fall arrest
As drop arrester for this product, use only a combination of the Hilti retaining strap #2293133 and the Hilti tool tether #2261970.- Secure the retaining strap to the installation openings for accessories. Check that it holds securely.
- Secure one carabiner of the tool tether to the retaining strap and secure the second carabiner to a load-bearing structure. Check that both carabiners hold securely.
Operation
Observe the safety instructions and warnings in these operating instructions and on the product.Switching the laser beams on
- Set the selector switch to the
position (ON / unlocked).
- The vertical laser lines are switched on.
- The vertical laser lines are switched on.
- Press the line mode button repeatedly until the desired line mode is set.
- The operating modes change in the following sequence and the sequence repeats itself: vertical lines, vertical side line, horizontal line, vertical and horizontal lines.
- The operating modes change in the following sequence and the sequence repeats itself: vertical lines, vertical side line, horizontal line, vertical and horizontal lines.
Matching two points over distance by fine adjustment
- Position the device with the lower plumbing beam centered on the reference cross on the ground.
- Turn the knob for fine adjustment until the vertical laser beam is aligned with the second, remote control point.
Setting the laser beam for the "Inclined line" function
- Set the selector switch to the
position (ON / locked).
- Press the line mode button repeatedly until the desired line mode is set.
Activating or deactivating laser receiver mode
- To activate the receiver mode, press the receiver mode button. The laser beam flashes five times as confirmation.
- Press the receiver mode button again to deactivate the receiver mode.
Switching the laser beams off
- Set the selector switch to the OFF position.
- The laser beam is switched off and the pendulum is locked.
- The laser beam is switched off and the pendulum is locked.
- The laser beam is switched off automatically when the battery is low.
Examples of applications
Transferring heights
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_02.jpg)
Setting up drywall track for a partition wall
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_03.jpg)
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_04.jpg)
Vertical alignment of pipes
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_05.jpg)
Aligning heating units
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_06.jpg)
Aligning door and window frames
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_07.jpg)
Care and maintenance
Care of the product- Blow dust off the glass of the laser exit windows. Do not touch the glass surfaces with your fingers.
- Carefully remove stubborn dirt.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use a dry, clean cloth to clean the contacts of the product.
- Never use a battery with clogged air vents. Clean the air vents carefully using a dry, soft brush.
- Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain).
If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service. - Keep the battery free of extraneous oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry cloth. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Do not touch the contacts of the battery and do not remove the factory-applied grease from the contacts. - Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
- After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
Checking
Checking the plumb point
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_08.jpg)
- In a high room (for example in a stairwell with a height of 10 m), make a mark (a cross) on the floor.
- Place the tool on an even, level surface.
- Switch the tool on and unlock the pendulum.
- Position the tool so that the lower plumb beam coincides with the center of the cross marked on the floor.
- Mark the top point of intersection of the laser lines on the ceiling.
- Pivot the tool through 90°.
- Mark the top point of intersection of the laser lines on the ceiling.
- Repeat the procedure after pivoting the tool through 180° and 270°.
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_FORMELR1.jpg)
- Calculate the value R.
- The value R should be less than 3 mm (corresponds to 3 mm at 10 m).
- The value R should be less than 1/8".
- The value R should be less than 3 mm (corresponds to 3 mm at 10 m).
Checking the leveling of the laser beam
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_09.jpg)
- The distance between the walls must be at least 10 m.
- Place the tool on an even, level surface approx. 20 cm from the wall (A) with the point of intersection of the laser lines directed toward the wall (A).
- Mark the point of intersection of the laser lines with a cross (1) on wall (A) and with a cross (2) on wall (B).
- Place the tool on an even, level surface approx. 20 cm from wall (B) and carefully aim the point of intersection of the laser lines at cross (1) on wall (A).
- Use the adjustable feet to adjust the height of the point of intersection of the laser lines so that the point of intersection coincides exactly with the mark (2) on the wall (B). In doing so, make sure that the bubble level remains centered.
- Mark the point of intersection of the laser lines again with a cross (3) on the wall (A).
- Measure the offset D between the crosses (1) and (3) on the wall (A) (RL = room length).
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_FORMELR2.jpg)
- Calculate the value R.
- The value R should be less than 3 mm.
- The value R should be less than 1/8".
- The value R should be less than 3 mm.
Checking perpendicularity (horizontal)
- Position the tool so that the lower plumb beam coincides with the center of a reference cross marked in the middle of a room at a distance of about 5 m from the walls.
- Mark all 4 points of intersection on the four walls.
- Rotate the tool through 90° and make sure that the center of the point of intersection coincides with the first reference point (A).
- Mark each new point of intersection and measure each offset (R1, R2, R3, R4 [mm]).
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_FORMELR3.jpg)
- Calculate the offset R (RL = room length).
- The value R should be less than 3 mm or 1/8".
- The value R should be less than 3 mm or 1/8".
Checking the accuracy of the vertical line
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_PM_50MG_10.jpg)
- Position the tool at a height of 2 m (pos.1).
- Switch the tool on.
- Position the first target plate T1 (vertical) at a distance of 2.5 meters from the tool at the same height (2 meters), so that the vertical laser beam strikes the plate. Mark this position.
- Then place the second target plate T2 at a position 2 meters below the first target plate, so that the vertical laser beam strikes the plate. Mark this position.
- Mark position 2 at the opposite side of the test setup (mirror image) on the laser line on the floor at a distance of 5 meters from the tool.
- Now place the tool on the previously marked position (pos. 2) on the floor.
- Align the laser beam so that it strikes the target plate T1 and the position marked on it.
- Mark the new position on target plate T2.
- Read the distance D between the two marks on target plate T2.
Hilti Measuring Systems Service
Hilti Measuring Systems Service checks the scanning tool and, if deviations from the specified accuracy are found, recalibrates it and rechecks to ensure conformity with specifications. The service certificate provides written confirmation of conformity with specifications at the time of the test. The following is recommended:- Choose a test/inspection interval that matches usage of the device.
- Have the product checked by Hilti Measuring Systems Service after exceptionally heavy use or subjection to unusual conditions or stress, before important work or at least once a year.
Transport and storage
Transport of cordless power tools and batteries- Remove the battery/batteries.
- Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Prior to each use and before and after prolonged transport, check the product and the batteries for damage.
- Store the product and the batteries in a cool and dry place. Comply with the temperature limits stated in the technical data.
- Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
- Never leave batteries in direct sunlight, on sources of heat, or behind glass.
- Store the product and batteries where they cannot be accessed by children or unauthorized persons.
- Prior to each use and before and after prolonged storage, check the product and the batteries for damage.
Troubleshooting
If a problem occurs, always observe the status indicator of the battery. See the section headed Status indicators of the Li‑ion battery .If the trouble you are experiencing is not listed in this table or you are unable to rectify the problem by yourself, contact Hilti Service.
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
LEDs of the battery show nothing |
Battery faulty. |
|
The battery runs down more quickly than usual. |
Very low ambient temperature. |
|
Battery does not engage with an audible click. |
The retaining lug on the battery is dirty. |
|
The product or battery gets very hot. |
Electrical fault. |
|
Disposal
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_SYM-General_M_M_DEU_Recycling_f.jpg)
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
FCC statement (applicable in US)/IC statement (applicable in Canada)
However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by taking the following measures:- Re-orient or relocate the receiving antenna.
- Increase the separation between the equipment and receiver.
- Connect the equipment to a power outlet on a circuit different from that to which the receiver is connected.
- Consult the dealer or an experienced TV/radio technician for assistance.
Operation is subject to the following two conditions:
- This device shall cause no harmful interference.
- This device must accept any interference received, including interference that may cause undesired operation.
Further information
RoHS (Restriction of Hazardous Substances)![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_ROHS-China.jpg)
![Image alternative](https://files-techDocs.hilti.com/2394965/H2_BILD-Objekt_System_PM_50MG-22_DEU_ROHS-Taiwan.jpg)
Hilti Li-ion batteries
Instructions for safety and useThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-ion cells joined together. These batteries are to be used in Hilti power tools exclusively. Use only genuine Hilti batteries!DescriptionHilti batteries have cell-management and cell-protection systems.
The batteries are composed of cells that contain lithium-ion storage materials capable of providing high specific energy density. Li-ion cells have a minimal memory effect, but they are very susceptible to external impact, deep discharge, and high temperatures.
The products approved for use with Hilti batteries can be found in your Hilti Store or at: www.hilti.group
Safety
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Follow the instructions in the section headed What to do in case of a battery fire .
- Always contact Hilti when a battery is damaged.
- Never use a battery that is leaking fluid.
- Avoid direct eye and/or skin contact with fluid leaking from a battery. Always wear protective gloves and eye protection when undertaking tasks involving battery fluid.
- Use a chemical spill cleanup kit to remove leaked battery fluid. Comply with the locally applicable cleanup regulations for battery fluid.
- To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then seal the lid air-tight and store the container away from flammable gases, liquids or objects.
- Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
- Watch for abnormal battery behavior, such as faulty charging, unusually long charging times, noticeable power loss, unusual LED activity, or leaking fluids. These are signs of an internal problem.
- If you suspect an internal battery problem, contact Hilti Service.
- A battery that no longer works, cannot be recharged or leaks fluid has to be disposed of correctly. See the section headed Maintenance and disposal .
- Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
- Leave the room immediately in case of intense smoke emission.
- Consult a doctor in case of any skin or respiratory irritation.
- Alert the fire service before you start tackling the fire.
- Use only water to tackle a battery fire and keep as far from the fire as effective extinguishing permits. Powder fire extinguishers and fire blankets are ineffective with Li-ion batteries. Fire in nearby materials can be extinguished with appropriate extinguishing agents.
- Do not try to move large quantities of burning batteries. Instead, isolate the batteries by removing unaffected materials from the immediate vicinity.
- Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
- Leave the battery in the bucket for at least 24 hours until it has cooled down completely.
- See the section headed What to do in case of damaged batteries .
- Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
- Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
- Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
- Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Never transport batteries in bulk form (loose, unprotected). During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
- Keep the battery free of oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry rag.
- Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully using a dry, soft brush.
- Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
- If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
- See the section headed What to do in case of damaged batteries .
- Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
- Do not dispose of batteries as household waste.
- Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.