B 3600
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The product supports near-field communication (NFC) technology compatible with iOS and Android platforms. |
![]() |
Li-ion battery |
![]() |
Never use the battery as a striking tool. |
![]() |
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. |
![]() |
Protection class II (double-insulated) |
![]() |
Transport mode |
![]() |
Standby mode |
![]() |
Operational mode |
Product information
![Image alternative](https://files-techDocs.hilti.com/2345499/H2_SYM-Logo_M_M_DEU_Hilti-Logo.jpg)
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationPortable energy system B 3600 Generation 01 Serial no.
Declaration of conformity
![Image alternative](https://files-techDocs.hilti.com/2345499/H2_BILD-Objekt_System_B_3600_DEU_Konform.jpg)
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Use the product and accessories only when they are in perfect working order.
- Never tamper with or modify the product or accessories in any way. Do not attempt to open the product.
- Do not touch the electrical contacts with your fingers, tools, jewelry, or other electrically conductive objects.
- Do not short-circuit the outputs of the product.
- Close the protective caps of the connections whenever the connections are not being used.
- Do not disassemble, squash or incinerate the product and do not subject it to temperatures over 80 °C.
- Never expose the product to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Keep the product away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Do not use or store the product in explosive environments.
- Use the product only within its specified limits.
- Treat the product with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Make sure that the product stands securely when it is being used. Set the product down only on a non-slip surface. Avoid allowing the product to project over an edge.
- Make sure that the connected consumer has a supply cord of adequate length; it is not permissible for the supply cord to be under strain.
- Do not use or attempt to charge the product if it has suffered an impact or is damaged in any other way. Check the product regularly for signs of damage.
- Do not stand on the product (do not use it as a substitute for a ladder).
- Do not transport the product by crane or with hoists.
- Comply with your locally applicable regulations for the safe use of electrical consumers.
- Do not connect a faulty consumer to the product.
- Do not connect generators to the outputs of the product.
- Charge the product only with the charging cord supplied.
- Make sure that product and consumer are both switched off before you connect the consumer. Always switch the consumer off after use.
- Do not use the product to power life-supporting medical devices.
- If the product is too hot to touch, it may be defective. Put the product in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow it to cool down. If the product is still too hot to touch after an hour, it is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
Description
Product overview
![Image alternative](https://files-techDocs.hilti.com/2345499/H2_BILD-Objekt_System_B_3600_DEU_Uebersicht.jpg)
- Frames
- Grip
- Rotary switch
- AC output
- LED indicator
- AC charging input
- Fuse cap
Intended use
The product described is a portable energy system. It is designed for powering corded consumers.
Items supplied
Portable energy system, charging cord, operating instructionsOther system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
LED indicators
The Hilti B 3600 energy system can indicate the state of charge and fault messages.If fault messages are detected the LEDs show or flash in accordance with the current state of charge.
Status |
Meaning |
---|---|
Eight (8) LEDs show constantly green |
State of charge: 100 % to 88 % |
Seven (7) LEDs show constantly green. |
State of charge: 87 % to 76 % |
Six (6) LEDs show constantly green. |
State of charge: 75 % to 63 % |
Five (5) LEDs show constantly green. |
State of charge: 62 % to 50 % |
Four (4) LEDs show constantly green |
State of charge: 49 % to 37 % |
Three (3) LEDs show constantly green |
State of charge: 36 % to 25 % |
Two (2) LEDs show constantly green |
State of charge: 24 % to 12 % |
One (1) LED shows constantly green |
State of charge: 12 % to 1 % |
One (1) LED flashes green (charging cord not connected). |
The Li-ion battery is completely discharged. Charge the battery. |
No LEDs show. |
The portable energy system is switched off. Switch it on. If no LEDs light up after the system has been switched on, consult Hilti Service. |
The LED corresponding to the current state of charge flashes green (while charging is in progress). |
The Li-ion battery is being charged. |
One or more LEDs show constantly yellow. |
A current spike occurred and the AC outputs were deactivated. Unplug all consumers. Turn the rotary switch to the position for standby mode ![]() ![]() If the message persists, consult Hilti Service. |
One or more LEDs flash yellow. |
The energy system is outside the permissible temperature range. Operation or charging has been interrupted. Unplug the consumer or the charging cord from the energy system and switch the energy system to standby mode ![]() If the message persists, consult Hilti Service. |
One (1) LED quick-flashes red |
A system fault has occurred. Disconnect the consumer or the charging cord, switch the energy system to transport mode ![]() |
Rotary switch
The rotary switch has the following three positions:![]() |
Transport |
In transport mode all connections are inactive and the energy system is switched off. |
![]() |
Standby / charging operation |
In standby mode the AC outputs are de-energized, the AC charging input is active. The LEDs do not show. |
![]() |
Operation |
In operational mode the AC outputs are active, a consumer can be connected and operated. The LEDs indicate the state of charge or fault messages. |
Technical data
High voltage |
|
---|---|
Output voltage |
220 V … 240 V / 50‑60 Hz |
Rated output power |
3,600 W / 16 A |
Peak output power for max. 120 seconds |
7,200 W / 32 A |
Energy available |
2.1 kWh |
Charging power |
1,000 W / 4 A |
Degree of protection |
IP 54+ |
Weight |
19.8 kg (43.7 lb) |
Dimensions (length x width x height) |
420 mm x 210 mm x 420 mm (16.5 in x 8.3 in x 16.5 in) |
Ambient temperature for operation |
−17 ℃ … 60 ℃ (1 ℉ … 140 ℉) |
Storage temperature |
−20 ℃ … 40 ℃ (−4 ℉ … 104 ℉) |
Battery charging starting temperature |
0 ℃ … 45 ℃ (32 ℉ … 113 ℉) |
Operation
Observe the safety instructions and warnings in this documentation and on the product.Charging
- Turn the rotary switch to the position for standby mode
.
- Connect the charging cord supplied with the product to the AC charging input and turn the bayonet connector clockwise until it latches.
- Connect the charging cord to a power outlet.
- The LEDs that show green indicate the current state of charge.
- If the energy storage battery is fully charged, all the LEDs show green for 10 seconds. The state of charge indicator then goes out.
- The LEDs that show green indicate the current state of charge.
- After charging, disconnect the charging cord and switch the energy system to transport mode
.
Operation
![Image alternative](https://files-techDocs.hilti.com/2345499/H2_BILD-Objekt_System_B_3600_DEU_Anschluesse.jpg)
- Turn the rotary switch to the position for operational mode
. The energy system is activated and the LEDs flash.
- If one or more LEDs subsequently show green, this indicates that the energy system is ready for operation.
- If one LED flashes green after the start sequence, this indicates that the energy system is completely discharged. Charge the battery.
- If no LEDs show after the start sequence, there is a fault in the system. Consult Hilti Service.
- If one or more LEDs subsequently show green, this indicates that the energy system is ready for operation.
- Connect a consumer to the AC output.
- Comply with the following instructions for powering more than one consumer off the energy system:
- If a consumer is powered off a vacuum cleaner connected to the energy system, the consumer has to be connected to the vacuum cleaner via a portable residual current device.
- For connecting two consumers, Hilti offers a splitter with integral portable residual current device.
- If multi-outlet power strips are used, each connected consumer has to be protected by a portable residual current device of its own.
- If a consumer is powered off a vacuum cleaner connected to the energy system, the consumer has to be connected to the vacuum cleaner via a portable residual current device.
- During operation, the LEDs indicate the current state of charge.
- To interrupt use of the energy system, turn the rotary switch to the position for standby mode
.
- To switch the energy system off completely, turn the rotary switch to the position for transport mode
.
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use a dry, clean cloth to clean the contacts of the product.
- Never expose the product to high levels of moisture (e.g. by being dipped in water or left in the rain).
If the product has been soaked by moisture, treat it in the same way as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
- After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
Changing fuse
- Unscrew the fuse cap.
- Remove the fuse. Insert a new fuse.
Materials Fine-wire fuse
T5A L 250V; 5 mm × 20 mm - Re-install the fuse cap.
Transport and storage
Transport- Transport the product only when it is in transport mode
.
- During transport, the product should be protected from excessive shock and vibration. Comply with the locally applicable regulations for transporting batteries.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Prior to each use and before and after prolonged transport, check the product for damage.
- It is not permissible to transport the product in an aircraft. Consult airline personnel if applicable.
- Store the product in a cool and dry place. Comply with the temperature limits stated in the technical data.
- Store the product only when it is in transport mode
.
- Do not keep the product in storage for a long period of time with the battery discharged. This could lead to deep discharge. Charge the product every three months at the latest.
- Never leave the product in direct sunlight, on sources of heat, or behind glass.
- Store the product where it cannot be accessed by children or unauthorized persons.
- Prior to each use and before and after prolonged storage, check the product for damage.
Troubleshooting
If a problem occurs, always observe the energy system's LED indicators. See the section headed LED indicators .If the trouble you are experiencing is not listed in this table or you are unable to rectify the problem by yourself, contact Hilti Service.
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
A connected consumer does not work or does not operate at full power. |
Plug not plugged in correctly |
|
The energy system is not in operational mode. |
|
|
Battery discharged |
|
|
Consumer's power consumption too high |
|
Disposal
![Image alternative](https://files-techDocs.hilti.com/2345499/H2_SYM-Hinweis_M_M_DEU_Recycling_f.jpg)
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
China RoHS (Restriction of Hazardous Substances)![Image alternative](https://files-techDocs.hilti.com/2345499/H2_BILD-Objekt_M_M_DEU_China-ROHS_cordless.jpg)
Hilti Li-ion batteries
Instructions for Use and OperationThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-Ion cells joined together. These batteries are to be used in Hilti power tools exclusively. When using Hilti power tools, use Hilti original battery packs!Hilti batteries are state of the art and are equipped with cell management and cell protection systems.
DescriptionThe batteries are composed of cells that contain lithium-ion storage materials that are capable providing high specific energy density. Unlike NiMH and NiCd batteries, Li-ion batteries have a minimal memory effect, but they are extremely susceptible to external impact, deep discharge, and high temperatures. See Safety WARNING
Find our battery-powered products at your Hilti Store or at:
www.hilti.group | USA: www.hilti.com
Safety
- Batteries must not be modified or tampered with!
- Never use recycled or repaired batteries conducted by non-Hilti companies.
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. Examine your batteries regularly for signs of damage, such as shredding, cuts or punctures.
- Never use the battery or a battery-operated power tool as a hammer.
- Avoid eye or skin contact with leaking liquids!
- See What to do in case of damaged batteries
- Damaged batteries can leak fluid which may moisten adjacent objects. Clean these objects with warm soapy water and replace the damaged batteries.
- See What to do in case of damaged batteries
- Never expose batteries to elevated temperature, sparking, or an open flame because the battery may explode.
- Do not touch the battery poles with your fingers, tools, jewelry, or other metallic objects because this may cause a short circuit, electrical shock, burns or explosions.
- Keep batteries away from rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
- Only use chargers and power tools approved for the specific battery type. Read and follow the instructions in the respective user manuals.
- Do not store or use the battery in explosion-prone environments containing combustible liquids or gases. An unexpected battery malfunction can cause an explosion under those conditions.
- If a Hilti battery is found to be damaged, contact your Hilti service partner.
- If a battery is leaking, use safety goggles and gloves to avoid direct eye or skin contact.
- To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then, close the lid air-tight and store the container away from flammable gases, liquids, or objects.
- Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
- Use a chemical spill cleanup kit to remove leaked battery fluid.
- Watch for abnormal battery behavior, such as faulty charging or unusually long charging times, noticeable power loss, unusual charger LED activity, or leaking fluids. These are signs of an internal problem.
- If you suspect an internal battery problem, contact your Hilti service partner.
- Should the battery be in operational or no longer chargeable or leaking fluid, dispose of it as described above.
- See What to do in case of damaged batteries .
- Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
- Leave the room immediately in case of intense smoke emission.
- Consult a doctor in case of any skin or respiratory irritation.
- Battery fires should be extinguished with water. Powder fire extinguishers and fire blankets are ineffective with Li-Ion batteries. Fires started by a lithium-ion battery in nearby materials can be extinguished with any appropriate extinguishing agent.
- Do not try to move large quantities of damaged, burning, or leaking batteries. Instead, remove surrounding materials and isolate the batteries. If the scale of the fire is larger than can be extinguished with available methods, contact the nearest firefighting authority.
- Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
- Wait for the battery to cool down completely.
- See What to do in case of damaged batteries .
- Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
- Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
- Do not store batteries on the charger. Separate battery from charger after use.
- Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
- Batteries should not be sent through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Do not transport batteries in bulk, loosely packaged. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit.
- Keep the battery free of oil and grease. If the battery is exposed to oil or grease, remove the contamination with a clean dry rag.
- Never use a battery with clogged venting slots. Clean the venting slots carefully with a soft brush to prevent debris from entering the battery.
- Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
- If the battery becomes dirty, clean it with a soft brush or clean, dry rag.
- If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
- See What to do in case of damaged batteries
- Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
- Do not dispose of batteries as household waste.
- Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.