PS 85
Original operating instructions
Information about the operating instructions
About these operating instructions
- Read these operating instructions before the product is used or operated for the first time. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in these operating instructions and on the product.
- Always keep the operating instructions with the product and make sure that the product is accompanied by these operating instructions only, when the product is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
![]() |
Hilti Li‑ion battery |
![]() |
Hilti charger |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
SD card |
![]() |
USB |
![]() |
The tool supports near-field communication (NFC) technology compatible with iOS and Android platforms. |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
![]() |
Li-ion battery |
![]() |
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationWall scanner PS 85 Generation 01 Serial no.
Declaration of conformity

The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions, measuring tools

Keep all safety precautions and instructions for future reference.
Work area safety
- Keep your workplace clean and well lit. Cluttered or poorly lit workplaces invite accidents.
- Do not operate the product in explosive atmospheres, such as in the presence of flammable liquids, gases or dust.
- Keep children and other persons clear when the product is in use.
- Use the product only within its specified limits.
- Comply with your national accident prevention regulations.
- Do not expose the product to rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
- Wipe the product dry before stowing it in the transport container.
- Stay alert, watch what you are doing and use common sense when operating a measuring tool. Do not use a measuring tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the measuring tool can result in serious personal injury.
- Avoid unusual body positions. Keep proper footing and balance at all times.
- Wear personal protective equipment. Wearing personal protective equipment reduces the risk of injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- Avoid accidental starting. Make sure that the measuring tool is switched off before connecting it to the battery and before picking it up or carrying it.
- Use the product and accessories in accordance with these instructions and in the way specified for this special type of tool. Take the working conditions and the work to be performed into account. Use of products for applications different from those intended could result in hazardous situations.
- Do not lull yourself into a false sense of security and do not flout the safety rules for measuring tools, even if you are familiar with the measuring tool after using it many times. Carelessness can result in serious injury within a fraction of a second.
- Do not use the measuring tool in the vicinity of medical devices.
- Use the product and accessories only when they are in perfect working order.
- Store measuring tools out of reach of children when not in use. Do not allow persons who are not familiar with the product or these instructions to operate it. Measuring tools are dangerous in the hands of inexperienced persons.
- Measuring tools need care and attention. Check that moving parts operate satisfactorily and do not jam, and make sure that no parts are broken or damaged in such a way that the measuring tool might no longer function correctly. Have damaged parts repaired before using the measuring tool. Many accidents are caused by poorly maintained measuring tools.
- Do not under any circumstances modify or tamper with the product. Changes or modifications not expressly approved by Hilti may restrict the user’s authorization to operate the product.
- Check the accuracy of the measuring tool before using it for important measurements, and if it has been dropped or subjected to other mechanical stresses.
- Due to the measuring principle employed, the results of measurements can be negatively affected by certain ambient conditions. These include, for example, the proximity of devices that produce strong magnetic or electro-magnetic fields, vibrations and temperature changes.
- Rapidly changing measuring conditions can falsify the results.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use. Big differences in temperature can lead to incorrect operation and incorrect results.
- When adapters or accessories are used, make sure they are mounted securely.
- The measuring tool is designed for the tough conditions of jobsite use, but as with other optical and electrical products (e.g. binoculars, spectacles, cameras) it must be handled with care.
- The specified operating and storage temperatures must be observed.
Additional safety instructions
Personal safety- Keep the measuring tool well away from all implants.
- Comply with the national accident prevention regulations.
- Do not use the measuring tool to examine humans or animals.
- Operation of the device in the proximity of expectant mothers or persons with a cardiac pacemaker is not permissible.
- Remove the battery prior to storage.
- Prior to use, always check the measuring tool's presettings and the settings you have made yourself.
- After switching on and while using the product, always pay attention to the information and warnings that appear on the display.
- Keep the underside of the scanner and the wheels clean as these parts can have an influence on measuring accuracy.
- Do not affix stickers or adhesive labels to the sensor area at the back of the measuring tool. Metal plates / labels, in particular, will affect measuring results.
- While measuring is in progress, always keep all 4 wheels in contact with the surface being scanned. Do not pass over steps or edges.
- While scanning is in progress, to avoid influencing the scan hold the measuring tool only by the grip provided for the purpose.
- While scanning is in progress, do not wear gloves and ensure an adequate earth/ground connection. An inadequate earth/ground connection can impair material detection (including detection of electrically live lines).
- Always move the measuring tool back and forth with a perfectly steady action.
- Do not drill at positions where the measuring tool has detected the presence of an object. Take the diameter of the drill bit into account and always allow an adequate safety factor.
- Do not use the measuring tool to detect critical objects such as load-bearing structural elements, high-tension lines, gas or steam lines, high-pressure lines and similar objects.
- Never rely on the measuring tool alone. Verify the results of measurements by cross-checking with other sources of information and by taking control measurements and, if necessary, by drilling pilot holes.
- Make sure that the wrist strap is securely attached. Prior to each use, always check the attachment point of the wrist strap for possible damage.
- Risk of injury by falling tools and/or accessories. Use only the wrist strap supplied.
- Carry the measuring tool only by the grip provided for the purpose. Keep the grip clean, dry and free from oil and grease.
- Keep the display clean and easily readable. Wipe the display only with a clean, non-scratch cloth.
- Due to the measuring principle employed, the results of measurements can be negatively affected by certain ambient conditions. These include, e.g. proximity to devices that generate powerful magnetic or electromagnetic fields, dampness, construction materials containing metal, aluminum foil-backed insulation, multiple layers, materials with cavities or electrically conductive wall coverings or tiles. Accordingly, other sources of information (e.g. plans of the building) should also be consulted before beginning drilling, sawing or grinding in the area scanned.
- When scanning is in progress, avoid the vicinity of devices (such as cellphones, for example) that emit strong electric, magnetic or electro-magnetic fields. On all devices capable of producing emissions that can impair measurement, deactivate the relevant functions if possible, or switch the devices off.
- Do not operate the measuring tool in the vicinity of military installations, airports, radio astronomy facilities or in aircraft unless prior permission has been obtained.
- Check the accuracy of the measuring tool if it has been dropped or subjected to other mechanical stresses. If the measuring tool is damaged, have it repaired by a Hilti service center.
- The specified operating and storage temperatures must be observed.
Careful handling and use of batteries
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Use only batteries that are in perfect working order.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
Careful handling and use of button-cell batteries
- Never swallow button-cell batteries. Severe internal caustic burns or death can result within 2 hours of swallowing a button-cell battery.
- Make sure that button-cell batteries are inaccessible to children. Consult a physician immediately if there is any suspicion that a button-cell battery has been swallowed or inserted into a body orifice.
- When replacing the button-cell battery, make sure that the correct procedure is followed. There is a risk of explosion.
- Use only the button-cell batteries stated in these operating instructions. Do not use any other button-cell batteries or other power supply.
- Do not attempt to recharge button-cell batteries and do not short-circuit button-cell batteries. The button-cell battery can develop a leak, explode, catch fire and injure persons.
- Remove and dispose of discharged button-cell batteries correctly. Discharged button-cell batteries can develop leaks and so damage the product or injure persons.
- Do not allow the button-cell battery to overheat and do not throw it into a fire. The button-cell battery can develop a leak, explode, catch fire and injure persons.
- Do not damage button-cell batteries and do not attempt to take button-cell batteries apart. The button-cell battery can develop a leak, explode, catch fire and injure persons.
- Do not bring a damaged button-cell battery into contact with water. In the presence of water, escaping lithium can produce hydrogen and so lead to a fire or an explosion, or cause injury to persons.
Description
Product overview

- Wheel
- Top marking notch
- Display
- Left/right marking notches
- Control panel
- Grip
- Screw, button-cell battery holder
- Button-cell battery holder
- Battery release button
- Battery
- Battery state of charge indicator
- Slot, micro-SD card
- USB port, type C
- Sensor area
- Eye
- Left function button
- Arrow buttons
- Start/stop button
- Right function button
- Screenshot button
- On/off button
Intended use
The product described is a wall scanner. It is designed to detect objects such as ferrous metals (reinforcing bars), non-ferrous metals (copper, aluminum), wooden beams, plastic pipes, lines and electric cables in dry materials.Device operation is limited to those engaged professionally in the building and construction trades.

- For this product, use only Hilti lithium‑ion batteries of the B 12 series. For this product, Hilti recommends the use of the batteries stated in this table.
- For these batteries, use only Hilti chargers of the type series stated here.
Items supplied
Wall scanner, USB cable, operating instructionsOther system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Overview of measuring modes
The measuring tool supports the following measuring modes:- Object detection for detecting objects in walls, floors and ceilings.
- Leak detection for detecting leaks.
- Distance measurement for measuring distances.
Technical data
Maximum detection depth in dry concrete |
200 mm (7.9 in) |
|
Detection depth for absolutely reliable results in dry concrete |
metal objects |
≤ 85 mm (≤ 3.3 in) |
other objects |
≤ 80 mm (≤ 3.1 in) |
|
Detection depth, wooden beams in drywall partitions |
38 mm (1.5 in) |
|
Detection depth, metal objects in early-age concrete |
60 mm (2.4 in) |
|
Detection depth, objects in other supported wall types |
80 mm (3.1 in) |
|
Accuracy of displayed object depth (plus application-specific deviation) |
in dry concrete |
±5 mm (±0.2 in) |
in early-age concrete |
±10 mm (±0.4 in) |
|
Measuring accuracy to center of object |
±5 mm (±0.2 in) |
|
Minimum distance between two neighboring objects |
40 mm (1.6 in) |
|
Measuring accuracy, distance measurement |
±10 mm / 1 m (±0.4 in / 3 ft) |
|
Frequency, radar sensor |
1.8 GHz … 5.7 GHz |
|
Maximum transmitting power, radar sensor |
0.00001 mW |
|
Frequency, inductive sensor |
48 kHz … 52 kHz |
|
Maximum magnetic field strength (at 10 m) |
20 dBµA/m |
|
Maximum site elevation above datum |
2,000 m (6,561 ft - 10 in) |
|
Maximum relative humidity |
90 % |
|
Maximum relative humidity for detecting electrically live objects |
50 % |
|
Degree of dirtying in accordance with IEC 61010-1 |
2 |
|
Typical battery life with B 12/2.6 battery |
≈ 6 h |
|
Button-cell battery |
CR2032 (3 V lithium battery) |
|
Button-cell battery life |
approx. 36 months |
|
Degree of protection |
IP 5X |
|
Dimensions (length x width x height), without battery |
264 mm x 115 mm x 100 mm (10.4 in x 4.5 in x 3.9 in) |
|
Weight in accordance with EPTA-Procedure 01, without battery |
0.57 kg (1.26 lb) |
|
Ambient temperature for operation |
−10 ℃ … 50 ℃ (14 ℉ … 122 ℉) |
|
Storage temperature |
−20 ℃ … 70 ℃ (−4 ℉ … 158 ℉) |
Battery
Battery operating voltage |
10.8 V |
Ambient temperature for operation |
−17 ℃ … 60 ℃ (1 ℉ … 140 ℉) |
Storage temperature |
−20 ℃ … 40 ℃ (−4 ℉ … 104 ℉) |
Battery charging starting temperature |
−10 ℃ … 45 ℃ (14 ℉ … 113 ℉) |
Operation
Observe the safety instructions and warnings in this documentation and on the product.Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the product until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the battery release button.
- Remove the battery from the product.
Attaching wrist strap
- Pull the narrow loop of the wrist strap through the eyelet in the underside of the product.
- Pass the broad loop through the narrow loop and pull the wrist strap tight.
Switching measuring tool on/off
- To switch the measuring tool on, press the on/off button or the start/stop button.
- Outside the operating temperature range, a fault message is displayed and the measuring tool automatically switches off. Allow the measuring tool to cool down or warm up, as appropriate, and then switch it on again.
- Outside the operating temperature range, a fault message is displayed and the measuring tool automatically switches off. Allow the measuring tool to cool down or warm up, as appropriate, and then switch it on again.
- To switch the measuring tool off, press the on/off button.
Menu
Navigating in menu
The functions assigned to the left and right function buttons vary, depending on which display view is active. The assigned function is indicated by a symbol appearing on the display directly above the corresponding function button.- To open the menu, press the left function button.
- To scroll through a menu, press the up or down arrow button.
- To confirm your choice of a menu option, press the start/stop button.
- To move back up to the next higher menu level, press the left function button.
- To exit the menu, press the right function button (not available in the "Gallery" submenu).
Menu items
Gallery You can retrieve images saved in the tool's internal memory, or you can delete them by pressing the right function button below the wastebasket symbol.Measuring mode Set the measuring mode you want to use. The measuring tool switches directly to the desired mode as soon as you make your selection. In "Object detection" mode you can also select the most suitable wall type for the planned measurement as well as the view, which determines how the results of measurement are displayed on screen.
Tool settings
- Measuring tape: Switch the measuring tape on and off for the measuring modes "Object detection" (except Spot view) and "Leak detection". You can use the measuring tape to measure the center-to-center distance between two objects, for example. Press the right function button to zero the measuring tape.
- Screen brightness : Set the brightness of the display lighting.
- Audio : Switch the acoustic signal on or off. When the function is switched on, an acoustic signal sounds every time a button is pressed and for each object detected underneath the sensor area.
- Start settings : Choose the settings (e.g. wall type, view, measuring tape) that are activated by default when the measuring tool is switched on. You have the choice of using the settings active when the tool was last switched off, or a personalized basic setting (corresponds to the current settings selected in the main menu).
- Switch off after ... : Select the time after which the measuring tool will switch off automatically if it is not used.
- Language : Select the display language.
- Date & time : Set the date and time for saving images and select the date and time formats. When date and time are no longer saved the button-cell battery has to be changed (see the section headed "Inserting/changing button-cell battery" (see Figure D), Page 31).
- Unit of measure : Select the unit of measure to be used in displaying measurements. (Not available in all markets.)
- Default settings : You can reset all menu options to their ex-works default settings. At the same time, all images saved in the tool's internal memory are irretrievably deleted.
Context-sensitive information and help
Whenever the question-mark symbol appears on the display above the right function button, pressing the right function button will call up context-sensitive information and help. This option is available whenever you change the wall type or the view, in all measuring modes of object detection and in leak detection.Saving / transferring results of measurement
Saving results of measurement as image
A panorama screenshot function is available in Object view. You can use it to save the results of measurement (including the object depth for each object shown on the display) as an image for documentation and subsequent analysis.- Measure the desired area in the usual way.
- Then press the "Screenshot" button.
- If there a micro-SD card installed in the slot, the images are saved to the card. Otherwise, the images are saved to the measuring tool's internal memory and can be exported via the USB interface.
- If there a micro-SD card installed in the slot, the images are saved to the card. Otherwise, the images are saved to the measuring tool's internal memory and can be exported via the USB interface.
Data transfer via USB interface
The USB interface is for data transfer only. Batteries or other devices cannot be recharged via this port.- Open the cover over the USB port.
- With the measuring tool switched off, use the USB cable to establish the connection between the USB port on the tool and your PC.
- Switch the measuring tool on.
- Open the file browser on your PC and select "Hilti PS 85 " as the drive. The files saved in the measuring tool's internal memory can be copied, moved to your PC, or deleted.
- As soon as you have completed the desired procedure, disconnect the drive in the standard way.
- Then switch the measuring tool off at the on/off switch.
- Disconnect the USB cable and close the cover over the USB port to protect against dirt and spray.
Data transfer by micro-SD card
If there is a micro-SD card inserted in the measuring tool, images are automatically saved to the card and not to the measuring tool's internal memory.- Open the cover over the slot for the micro-SD card.
- Press the micro-SD card slightly into the measuring tool until the card unlatches.
- Remove the micro-SD card from the slot and connect it to your PC. The files saved on the card can be copied, moved to your PC, or deleted.
- When you are finished, re-insert the micro-SD card into the slot. Make sure you insert the card right way round. Push the micro-SD card in until it engages.
- Close the cover of the slot to protect against dust and spray.
Software update
You can update the software of the measuring tool when necessary.The newest software version can be downloaded from here: Downloading
- If the software version is newer than the version installed on your product, download the update file.
- Load the update file on to the micro-SD card.
- Insert the micro-SD card into the measuring tool.
- Switch the measuring tool on.
- If a new update file that was not installed beforehand is found, the update process starts automatically.
- You can follow the progress of the update process on the display. This process can take several minutes to complete.
- When the update procedure completes, the measuring tool reboots automatically.
- Hilti recommends subsequently deleting the update file from the micro-SD card.
"Object detection" measuring mode
Working principle
The measuring tool is used to examine the base material in the sensor area. If there are objects set one above the other in the wall, the object closest to the surface is shown on the display.In "Object detection" mode you can also select the most suitable wall type for the planned measurement as well as the view, which determines how the results of measurement are displayed on screen.
Detectable objects
Objects that differ from the wall material are detected.- Plastic pipes (e.g. water-filled plastic pipes at least 10 mm in diameter, empty pipes at least 20 mm in diameter in solid surrounding material)
- Electric cables (irrespective of whether the cables are live or not)
- Three-phase power cables (e.g. for kitchen cooker)
- Low-voltage lines (e.g. for doorbell, telephone, LAN, smart-home wiring)
- Metal pipes, bars, beams of all kinds (e.g. steel, copper, aluminum)
- Reinforcing bars
- Wooden beams
- Cavities
Special measurement cases
-
Due to the principle employed, certain adverse circumstances can have a negative effect on the result:
- Multi-layer wall make-ups.
- Empty plastic pipes and wooden beams in cavities and drywall partitions.
- Objects running at an angle in the wall.
- Metal surfaces and damp areas; under certain circumstances (e.g. high water content), might be presented on the display as objects in a wall. Bear in mind that concrete has to cure for several months to reach its fully dry state.
- Cavities in a wall; might be presented on the display as objects.
- Proximity to devices that produce strong magnetic or electro-magnetic fields, such as cellphone base stations or electricity generators.
Wall types
Changing wall typeTo obtain the best possible results, always set the appropriate wall type. Measuring depth depends on wall type; the maximum is 85 mm (3.3 in).- Press the left or right arrow button until the wall type you want to use appears on the display.
- Press the start/stop button to confirm your selection of wall type.
Wall type "Concrete"Wall type "Concrete" is suitable for applications in dry concrete. Plastic and metal objects and electrical lines and other lines are shown on the display. Empty plastic pipes less than 2 cm (0.8 in) in diameter might not show up on the display. When you select the wall type you can also set the maximum measuring depth in the range from 8 cm (3.1 in) to 20 cm (7.9 in).
Wall type "Drywall"Wall type “Drywall” is suitable for detecting wooden beams, metal framing and electrical lines and other lines in drywall partitions (wood, gypsum board, etc.). Filled plastic pipes and wooden beams appear identical on the display. Empty plastic pipes are not detected. If you identify many objects close to the surface (0‑2 mm (0‑0.08 in) below the surface), try working with a surface overlay (e.g. a sheet of perspex 1 cm (0.4 in) thick).
Wall type "Vertical coring brick"Wall type "Vertical coring brick" is eminently suitable for applications in vertical coring bricks. Vertical coring bricks are bricks with many small cavities, generally running vertically. Metal objects and electrical lines and other lines and water-filled plastic pipes are shown on the display. Cavities or empty plastic pipes might not show up on the display.
Wall type "Horizontal coring brick"Wall type "Horizontal coring brick" is eminently suitable for applications in horizontal coring bricks. Horizontal coring bricks are bricks with a small number of large cavities, generally running horizontally. Shallow-covered metal objects, electrical lines and other lines and water-filled plastic pipes at a maximum measuring depth of 2 cm are shown on the display. Cavities or empty plastic pipes might not show up on the display. To improve the result, additionally scan horizontal coring brick with the "Vertical coring brick" wall type. Be prepared to distinguish between plausible and implausible objects (ghost objects).
Wall type "Early-age concrete"Wall type "Early-age concrete" is eminently suitable for applications in concrete that has not yet cured to the fully hardened and dry state. Metal objects, plastic and metal pipes and electric lines are shown on the display. It is not possible to differentiate between electrically live and non-live lines. The maximum detection depth is 6 cm (2.4 in). Bear in mind that concrete has to cure for several months to reach its fully hardened and dry state.
View
Changing view- Repeatedly press the up or down arrow button until the view you want to use is shown.
- Press the start/stop button to confirm your selection of the view.
Spot view

Whenever possible, even in Spot view you should move the measuring tool over the surface in order to obtain the best possible results. If the measuring tool is not moved its ability to pinpoint objects is restricted, particularly with regard to plastic pipes and wooden beams.
Measurement displayIf no object is found, only the outside circle appears on the display and it shows green.
If there is an object in the vicinity, the outside circle shows red. As the measuring tool approaches an object the number of concentric circles shown on the display increases. The number of circles diminishes as the measuring tool moves away from an object.
If the signal is strong enough, orientation arrows appear on the display. To pinpoint the center of the object, move the measuring tool in the direction indicated by the orientation arrows. Over the center of the object the reading peaks and if the signal is strong enough centering crosshairs appear on the display. The color coding for material property is the same as in Object view.
Even if the orientation arrows and the centering crosshairs do not appear, there is still the possibility of an object being present in the immediate vicinity.
Object view

Measuring operation
- Place the measuring tool on the surface to be scanned and move it in the required direction. The results of measurement appear on the display after the tool has been moved at least approximately 10 cm.
- Always move the measuring tool in a straight line, applying light pressure so that the wheels are in firm contact with the surface of the wall.
- To obtain optimum results, move the measuring tool slowly over the entire area to be examined and observe the results obtained as you draw the measuring tool back. The scan should be at least 40 cm in length.
- You can start a new measurement at any time by pressing the start/stop button.
- If you lift the measuring tool off the wall while a measurement is in progress, the most recent result remains visible on the display. Measurement restarts when contact with the wall is re-established, or when movement of the measuring tool resumes.
- For particularly sensitive measurements, use Spot view with the appropriate wall type.

A single pass in one direction along the track to be examined suffices to locate objects. If you want to pinpoint and precision-mark a detected object, draw the measuring tool back along the same track in the reverse direction.
You can ascertain the path of a detected object in the wall by running a succession of passes with the measuring tool along adjacent tracks.
Measurement displayIf no object was detected in the sensor area, the broken lines and the center line are completely green. A detected object appears between the two broken lines on the display and the two broken lines and the center line are partly or completely red.
The depth scale on the right shows the depth of the detected object's top edge below the surface.
The image of the objects shown on the display can differ from the actual properties of the objects. In particular, very thin objects appear to be thicker than they actually are. Larger-diameter cylindrical objects (e.g. plastic pipes or water pipes) can appear narrower than they actually are.
Color coding of material propertyDepending on the nature and the depth of the object detected, it is possible to identify material properties.
They are indicated by color-coding, as follows:
Orange |
Electrically live object |
Blue |
magnetic / ferrous metal (e.g. reinforcing bar) |
Turquoise |
Non-magnetic metal (e.g. copper pipe) |
White |
Non-metal (e.g. wood, plastic) |
Gray |
Material property unknown |
- Move the measuring tool to the detected object you want to mark.
- Position the measuring tool so that the object is centered relative to the center line on the display.
- Apply one mark at each marking notch for top, right and left.
- The point of intersection for the marks you applied coincides with the center of the object.
- Alternatively, position the measuring tool so that the object is centered relative to either of the two broken lines on the display.
- The object is now centered below the corresponding outside edge of the measuring tool.
- Draw a line along this outside edge on the surface of the material and on this line mark a cross at the position of the corresponding side marking notch.
- This coincides with the center of the object.
Signal view 2D

Signal view 2D can be used to pinpoint close-spaced objects and arrive at a better estimation of complicated material make-ups. Even objects with a weak echo and objects underlying other objects can be detected under certain circumstances. See the notes on the measuring operation in Object view.
See the notes on the measuring operation in Object view .
Signal view

"Leak detection" measuring mode
The relative material moisture content of the surface is shown in this measuring mode. Consequently, it is suitable for locating the place of maximum material moisture content and thus indicating a possible leak. Different materials on the surface, shallow objects underneath the surface and inhomogeneity in the base material (joints, for example) can falsify the results."Distance measurement" measuring mode
This measuring mode enables you to measure distances between objects.The reference point for measurement is always the top marking notch. Measurement is possible only straight ahead in the direction of travel of the wheels. The distance from the starting point is measured continuously. The measured value shown on the display corresponds to the distance from the starting point of the current measurement. It is not the total distance traveled. The measured value counts down when you roll the measuring tool back toward the starting point.
If the measuring tool returns implausible distance values measure a defined distance, for example 1 m (3 ft). If the distance reading is not within tolerance (see the section headed "Technical data"), consult Hilti Service.
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Carefully clean the air vents, if present, with a dry, soft brush.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use a dry, clean cloth to clean the contacts of the product.
- Never use a battery with clogged air vents. Clean the air vents carefully using a dry, soft brush.
- Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain).
If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service. - Keep the battery free of extraneous oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry cloth. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Do not touch the contacts of the battery and do not remove the factory-applied grease from the contacts. - Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
- After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
Changing button-cell battery
The measuring tool has a button-cell battery to enable it to save the date and time. The button-cell battery has to be changed when it is discharged.
- Remove the screw of the button-cell battery holder.
- Ease the button-cell battery holder out of its slot (using a suitable tool if necessary).
- Remove the empty button-cell battery and insert a new button-cell battery. Make sure that polarity is correct. The positive pole of the button-cell battery must be facing up.
- Re-insert the button-cell battery holder into its slot. Make sure that the button-cell battery holder is inserted correctly and fully, as otherwise protection against dust and spray is not ensured.
- Re-install the screw of the button-cell battery holder and tighten it until hand-tight.
Transport and storage of cordless tools and batteries
Transport- Remove the battery/batteries.
- Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Prior to each use and before and after prolonged transport, check the product and the batteries for damage.
- Store the product and the batteries in a cool and dry place. Comply with the temperature limits stated in the technical data.
- Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
- Never leave batteries in direct sunlight, on sources of heat, or behind glass.
- Store the product and batteries where they cannot be accessed by children or unauthorized persons.
- Prior to each use and before and after prolonged storage, check the product and the batteries for damage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
Product cannot be switched on. |
Battery is discharged |
|
Battery not fully inserted. |
|
|
Battery does not engage with an audible click. |
Retaining lugs on the battery are dirty. |
|
Entry by means of control panel not possible |
Control panel defective |
|
Wheels not running smoothly |
Wheels dusty or dirty |
|
Product cannot be connected to a PC. |
Product is not detected by the PC. |
|
USB cable faulty. |
|
|
USB port on the product faulty. |
|
|
The micro-SD card is not working. |
The micro-SD card is not detected. |
|
The micro-SD card is not readable. |
|
FCC statement (applicable in US) / IC statement (applicable in Canada)
This equipment has been tested and found to comply with the limits for a class B digital device, pursuant to part 15 of the FCC rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause interference to radio communications.However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by taking the following measures:
- Re-orient or relocate the receiving antenna.
- Increase the separation between the equipment and receiver.
- Connect the equipment to a power outlet on a circuit different from that to which the receiver is connected.
- Consult the dealer or an experienced TV/radio technician for assistance.
Operation is subject to the following two conditions:
- This device shall cause no harmful interference.
- This device must accept any interference received, including interference that may cause undesired operation.
Coordination requirements
- UWB imaging systems require coordination through the FCC before the equipment may be used. The operator shall comply with any constraints on equipment usage resulting from this coordination.
- The users of UWB imaging devices shall supply operational areas to the FCC Office of Engineering and Technology, which shall coordinate this information with the Federal Government through the National Telecommunications and Information Administration. The information provided by the UWB operator shall include the name, address and other pertinent contact information of the user, the desired geographical area(s) of operation, and the FCC ID number and other nomenclature of the UWB device. If the imaging device is intended to be used for mobile applications, the geographical area(s) of operation may be the state(s) or county(ies) in which the equipment will be operated. The operator of an imaging system used for fixed operation shall supply a specific geographical location or the address at which the equipment will be operated. This material shall be submitted to Frequency Coordination Branch, OET, Federal Communications Commission, at the address of the FCC's main office indicated in 47 CFR 0.401(a), ATTN: UWB Coordination.
- The manufacturers, or their authorized sales agents, must inform purchasers and users of their systems of the requirement to undertake detailed coordination of operational areas with the FCC prior to the equipment being operated.
- Users of authorized, coordinated UWB systems may transfer them to other qualified users and to different locations upon coordination of change of ownership or location to the FCC and coordination with existing authorized operations.
- The FCC/NTIA coordination report shall identify those geographical areas within which the operation of an imaging system requires additional coordination or within which the operation of an imaging system is prohibited. If additional coordination is required for operation within specific geographical areas, a local coordination contact will be provided. Except for operation within these designated areas, once the information requested on the UWB imaging system is submitted to the FCC no additional coordination with the FCC is required provided the reported areas of operation do not change. If the area of operation changes, updated information shall be submitted to the FCC following the procedure in paragraph 2) of this section.
- The coordination of routine UWB operations shall not take longer than 15 business days from the receipt of the coordination request by NTIA. Special temporary operations may be handled with an expedited turn-around time when circumstances warrant. The operation of UWB systems in emergency situations involving the safety of life or property may occur without coordination provided a notification procedure, similar to that contained in § 2.405(a) through (e) of this chapter, is followed by the UWB equipment user.
Hilti, Inc.
7250 Dallas Parkway, Suite 1000
US-Plano, TX 75024
www.hilti.com
For users in Canada: This radar imaging device shall be operated only where directed toward the floor or wall, and where it is in contact with or at a distance of 20 cm from the floor or wall surface. This radar imaging device shall be operated only by law enforcement agencies, scientific research institutes, commercial mining companies, construction companies, and emergency rescue or fire-fighting organizations.
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
Accessories, system products and more information about your product can all be found here.China RoHS (Restriction of Hazardous Substances)

Hilti Li-ion batteries
Instructions for safety and useThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-ion cells joined together. These batteries are to be used in Hilti power tools exclusively. Use only genuine Hilti batteries!Description Hilti batteries have cell-management and cell-protection systems.
The batteries are composed of cells that contain lithium-ion storage materials capable of providing high specific energy density. Li-ion cells have a minimal memory effect, but they are very susceptible to external impact, deep discharge, and high temperatures.
The products approved for use with Hilti batteries can be found in your Hilti Store or at: www.hilti.group
Safety
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Follow the instructions in the section headed What to do in case of a battery fire .
- Always contact Hilti when a battery is damaged.
- Never use a battery that is leaking fluid.
- Avoid direct eye and/or skin contact with fluid leaking from a battery. Always wear protective gloves and eye protection when undertaking tasks involving battery fluid.
- Use a chemical spill cleanup kit to remove leaked battery fluid. Comply with the locally applicable cleanup regulations for battery fluid.
- To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then seal the lid air-tight and store the container away from flammable gases, liquids or objects.
- Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
- Watch for abnormal battery behavior, such as faulty charging, unusually long charging times, noticeable power loss, unusual LED activity, or leaking fluids. These are signs of an internal problem.
- If you suspect an internal battery problem, contact Hilti Service.
- A battery that no longer works, cannot be recharged or leaks fluid has to be disposed of correctly. See the section headed Maintenance and disposal .
- Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
- Leave the room immediately in case of intense smoke emission.
- Consult a doctor in case of any skin or respiratory irritation.
- Alert the fire service before you start tackling the fire.
- Use only water to tackle a battery fire and keep as far from the fire as effective extinguishing permits. Powder fire extinguishers and fire blankets are ineffective with Li-ion batteries. Fire in nearby materials can be extinguished with appropriate extinguishing agents.
- Do not try to move large quantities of burning batteries. Instead, isolate the batteries by removing unaffected materials from the immediate vicinity.
- Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
- Leave the battery in the bucket for at least 24 hours until it has cooled down completely.
- See the section headed What to do in case of damaged batteries .
- Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
- Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
- Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
- Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Never transport batteries in bulk form (loose, unprotected). During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
- Keep the battery free of oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry rag.
- Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully using a dry, soft brush.
- Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
- If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
- See the section headed What to do in case of damaged batteries .
- Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
- Do not dispose of batteries as household waste.
- Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.