IC-BLE
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol
.
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationBluetooth module Set: IC-BLE
Receiver module: IC-RC
Remote control: IC-RMGeneration 01 Serial no.
Declaration of conformity

The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions
Read all safety instructions and other instructions. Keep all safety instructions and other instructions for future reference.- Stay alert, watch what you are doing and use common sense when working with the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product can result in serious personal injury.
- Maintain power tools and accessories carefully. Check that moving parts operate satisfactorily and do not jam, and whether any parts are broken or so damaged that the correct operation of the power tool is adversely affected. If parts are damaged, have the parts repaired before using of the tool. Many accidents are caused by poorly maintained power tools.
- Do not expose the product to rain or moisture. Water entering an electric device will increase the risk of electric shock.
- Have the product repaired only by qualified specialists using only genuine Hilti spare parts. The safety of the module can thus be maintained.
- Keep the product out of reach of children.
Product-specific safety instructions
- Check the contents of the packaging. Make sure that nothing is damaged and that the contents are complete. If you notice defects or shortcomings that could impair the operability of the product, have them rectified by qualified personnel.
- Make sure that the product is correctly installed and secured.
Additional safety instructions
- When attaching to a power tool, make sure that grips and other gripping surfaces are not obstructed and that you can still hold the power tool securely.
- Do not attach the remote control unit to rotating parts of power tools and do not attach it to parts of the body, such as a hand or an arm.
- Although the product complies with the strict requirements of the valid directives, Hilti cannot entirely rule out the possibility of the product causing interference due to powerful electromagnetic radiation. This can lead to incorrect operation. Similarly, Hilti cannot exclude the possibility of interference with other electrical devices (e.g. aircraft navigation devices).
Careful handling and use of button-cell batteries
- Never swallow button-cell batteries. Severe internal caustic burns or death can result within 2 hours of swallowing a button-cell battery.
- Make sure that button-cell batteries are inaccessible to children. Call a poison control center to obtain information on treatment if there is any suspicion that a button-cell battery has been swallowed or inserted into a body orifice.
- Use only the button-cell batteries stated in these operating instructions. Do not use any other button-cell batteries or other power supply.
- Do not attempt to recharge non-rechargeable button-cell batteries. The button-cell battery can develop a leak, explode, catch fire and injure persons.
- Do not force-discharge, charge, disassemble or incinerate the button-cell battery. Do not heat the button-cell battery to a temperature above the maximum temperature stated by the manufacturer. Otherwise there is a risk of injury by degassing, leakage or explosion leading to chemical burns.
- Remove discharged button-cell batteries and recycle or dispose of them immediately in accordance with your local regulations. Keep button-cell batteries out of reach of children. Do NOT dispose of button-cell batteries in household waste and do not incinerate them. Discharged button-cell batteries can develop leaks and so damage the product or injure persons.
- Even discharged button-cell batteries can lead to serious injuries or death. Do not treat discharged button-cell batteries with less care than new batteries.
- Do not bring a damaged button-cell battery into contact with water. In the presence of water, escaping lithium can produce hydrogen and so lead to a fire or an explosion, or cause injury to persons.
Description
Product overview

- Hole for securing screw
- LED indicator
- Bluetooth operating button
- ON/OFF operating button
- LED indicator
- Hook for attachment
- Rubber band for attachment (for attachment to suction hose or power tool)
Intended use
The product described is a Bluetooth receiver module with remote control unit that can be retrofitted to Hilti vacuum cleaners. It is designed to enable wireless on/off control of the vacuum cleaner.
The remote control unit is designed for mounting on a suction hose.
Items supplied
Wireless remote control, receiver module, securing screw (2 of), rubber band for attachment, operating instructionsBluetooth®
The Bluetooth ® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc and any use of such marks by Hilti Corporation is under license.Bluetooth is a wireless data transfer system by which the two Bluetooth-enabled products can communicate with each other over a short distance.
The Hilti Bluetooth module comes paired ex-works to the accompanying remote control unit and automatically establishes the connection when switched on.
BLE-Mute function
The BLE-Mute function temporarily interrupts wireless communication between remote control unit and the receiver module installed on the vacuum cleaner. Activate this mode for transport in aircraft, for example, and for working in facilities such as hospitals.→To activate the BLE-Mute function: Press the ON/OFF operating button and hold it down for 10 seconds.
→To deactivate the BLE-Mute function: Press the ON/OFF operating button and hold it down for 3 seconds.
Signals issued by LED indicator
Both remote control unit and receiver module have an LED indicator that can issue signals indicative of various operating states.The following LED signals can occur:
LED signal |
Meaning |
---|---|
Remote control unit or receiver module: LED does not light up |
Option A: BLE-Mute function is activated. Option B: Button-cell battery state of charge is too low or the receiver module is not correctly installed in the vacuum cleaner. |
Receiver module: LED pulsates (approx. 2-second interval) |
Remote control unit and receiver module are paired and functioning correctly. This state is the normal operating mode. |
Remote control unit or receiver module: LED quick-flashes |
Pairing mode is active. Remote control unit and receiver module are paired ex-works. The signal indicating normal operating mode appears directly on initial start-up. |
Technical data
Product properties
IC-RC |
IC-RM |
|
---|---|---|
Rated voltage |
3.3 V |
3.3 V |
Rated current |
50 mA |
20 mA |
Battery |
·/· |
CR2032 |
Dimensions (L × W × H) |
62 mm × 43 mm × 14 mm |
40 mm × 37 mm × 21 mm |
Operating temperature |
−15 ℃ … 50 ℃ |
−15 ℃ … 50 ℃ |
Storage temperature |
−20 ℃ … 70 ℃ |
−20 ℃ … 70 ℃ |
Signal range (can vary greatly depending on surrounding conditions) |
30 m |
30 m |
Bluetooth
Communication standard |
Bluetooth® 5 |
Frequency |
2,404 GHz … 2,480 GHz |
Maximum emitted transmission power |
4 dBm |
Operation
Installing receiver module

- Remove the 2 securing screws from the blanking cover on the vacuum cleaner.
- Remove the blanking cover.
- Plug the connector into the port.
- Note the coding of the plug-in connection.
- The connector is engaged.
- Note the coding of the plug-in connection.
- Insert the receiver module into the mount.
- Secure the receiver module with the 2 securing screws.
- Hold the remote control unit in position on the suction hose.
- Fix the remote control unit firmly in position with the rubber band for attachment.
Pairing remote control unit and receiver module
The remote control unit and receiver module in a set are paired ex-works. You can pair two products manually, for example when you replace or retrofit either of the two components. Pairing mode is also activated whenever you deactivate the BLE-Mute mode.- On each of the two products to be paired (remote control unit and receiver module), press the operating button and hold both buttons down for 3 seconds.
- The LED indicator (on remote control unit and receiver module) flashes.
- The LED indicator (on remote control unit and receiver module) flashes.
- Wait until the pairing procedure has completed.
- Pairing has completed as soon as the LED indicator (on the receiver module) starts to pulsate.
- Pairing has completed as soon as the LED indicator (on the receiver module) starts to pulsate.
Using remote control unit
The remote control unit enables on/off control of the vacuum cleaner at a distance. The rubber band for attachment enables you to attach the remote control unit to the suction hose or a power tool. Make sure that you do not obstruct gripping surfaces or safety devices.- Set the vacuum cleaner to Bluetooth operation.
- Follow the instructions in the operating instructions for the vacuum cleaner.
- Follow the instructions in the operating instructions for the vacuum cleaner.
- To switch on or off, press the ON/OFF operating button.
Changing battery (remote control unit)
- Open the cover of the battery compartment cover with a suitable instrument (e.g. coin).
- Remove the discharged battery.
- Insert the new battery, with the + pole facing up, into the battery compartment.
- Battery type: CR2032 button cell
- Battery type: CR2032 button cell
- Close the battery compartment with the cover.
Care and maintenance
Care- Carefully remove stubborn dirt from the tool.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as they can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage
Transport- Do not transport this product with an accessory tool installed.
- Make sure that the equipment is held securely throughout all transport operations.
- After transporting, always check all visible parts and controls for signs of damage and make sure that they all function correctly.
- Always store this product with the electric supply cable unplugged from the electricity supply.
- Store this product in a dry place, where it cannot be accessed by children or unauthorized persons.
- After a long period of storage, always check all visible parts and controls for signs of damage and make sure that they all function correctly.
Troubleshooting
Check for a fault affecting the vacuum cleaner and consult the troubleshooting section in the operating instructions of the vacuum cleaner.If the trouble you are experiencing is not listed in this table or you are unable to rectify the problem by yourself, please contact Hilti Service.
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
LED does not light up when the operating button is pressed |
Button-cell battery discharged |
|
Remote control unit faulty |
|
|
LED does not light up (control switch set to AUTO ) |
Cable of the receiver module not correctly plugged into the vacuum cleaner |
|
Receiver module not correctly installed |
||
Receiver module faulty |
|
|
Vacuum cleaner does not start and/or does not react to inputs via the remote control unit |
Button-cell battery discharged |
|
No connection between receiver module and remote control unit |
|
|
Pairing procedure was aborted or failed |
||
Source of trouble is in the vacuum cleaner |
|
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information

FCC statement (applicable in US) / IC statement (applicable in Canada)
This device is in compliance with paragraph 15 of the FCC rules and the RSS‑210 specifications of ISED.Operation is subject to the following two conditions:
- This device shall cause no harmful interference.
- This device must accept any interference received, including interference that may cause undesired operation.