BX-S
BX‑SH B3
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol
. - Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The tool supports near-field communication (NFC) technology compatible with iOS and Android platforms. |
On the product
Laser information![]() |
Laser class 1 based on standard IEC / EN 60825-1:2014 and corresponding to CFR 21 § 1040 (Laser Notice 56). |
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationLaser
HolderBX-S
BX-SH B3Generation 01 Serial no.
Declaration of conformity
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions
WARNING! Read all safety precautions and other instructions. This product can present hazards if handled incorrectly. Failure to comply with the safety instructions and other instructions can result in damage to the product and/or serious injury.
Keep all safety precautions and instructions for future reference.
Work area safety
- Keep your workplace clean and well lit. Cluttered or poorly lit workplaces invite accidents.
- Do not operate the product in explosive atmospheres, such as in the presence of flammable liquids, gases or dust.
- Keep children and other persons clear when the product is in use.
- Use the product only within its specified limits.
- Comply with your national accident prevention regulations.
- Do not expose the product to rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
- Wipe the product dry before stowing it in the transport container.
- Stay alert, watch what you are doing and use common sense when operating the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product can result in serious personal injury.
- Avoid unusual body positions. Keep proper footing and balance at all times.
- Wear personal protective equipment. Wearing personal protective equipment reduces the risk of injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- Avoid accidental starting. Make sure that the product is switched off before inserting batteries and before picking it up or carrying it.
- Use the product and accessories in accordance with these instructions and in the way specified for this special type of tool. Take the working conditions and the work to be performed into account. Use of products for applications different from those intended could result in hazardous situations.
- Do not allow yourself to be lulled into a false sense of security and do not flout the safety rules, even if you are familiar with the product after using it many times. Caress handling could cause serious injury within fractions of a second.
- Do not use the product in proximity to medical devices.
- Use the product and accessories only when they are in perfect working order.
- Store products out of reach of children when not in use. Do not allow persons who are not familiar with the product or these instructions to operate it. The product is dangerous if used by inexperienced persons.
- Maintain the product carefully. Check that moving parts operate satisfactorily and do not jam, and make sure that no parts are broken or damaged in such a way that the product might no longer function correctly. Have damaged parts repaired before using the product. Many accidents are caused by poorly maintained products.
- Do not under any circumstances modify or tamper with the product. Changes or modifications not expressly approved by Hilti may restrict the user’s authorization to operate the product.
- Check the accuracy of the product before using it for important measurements, and if it has been dropped or subjected to other mechanical stresses.
- Due to the measuring principle employed, the results of measurements can be negatively affected by certain ambient conditions. These include, for example, the proximity of devices that produce strong magnetic or electro-magnetic fields, vibrations and temperature changes.
- Rapidly changing measuring conditions can falsify the results.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use. Big differences in temperature can lead to incorrect operation and incorrect results.
- When adapters or accessories are used, make sure they are mounted securely.
- The product is designed for the tough conditions of jobsite use, but as with other optical and electrical products (e.g. binoculars, spectacles, cameras) it must be handled with care.
- The specified operating and storage temperatures must be observed.
Additional safety instructions
- Laser radiation in excess of Class 1 can be emitted if the product is opened without correct procedure being followed. Have the product repaired only by Hilti Service.
- Never aim the product against the sun or other powerful light sources.
- Do not aim the laser at other persons and do not aim it at bare skin at close range.
- Switch the product off when it is not in use.
- Do not use the product in very bright conditions. The arc cast by the laser must remain visible. Darken or shade the working area if necessary.
- Check the accuracy of the product if it has been dropped or subjected to other mechanical stresses.
- Keep the laser aperture clean to avoid measurement errors.
- Comply with national health and safety requirements.
Electromagnetic compatibility
Although the product complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference to the product caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions, or if you are unsure. Likewise, Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment).Careful handling and use of batteries
- Remove the batteries from the product if it is to remain unused for a lengthy period of time. Batteries can corrode and self-discharge during prolonged storage.
- Make sure that batteries are inaccessible to children.
- Do not mix old and new batteries. Always replace all batteries at the same time. Do not mix batteries of different makes or types.
- Do not use damaged batteries.
- Use only the battery type intended for this product. Use of other batteries may create a risk of injury and fire.
- When changing batteries, make sure that polarity is correct. There is a risk of explosion.
- Do not allow batteries to overheat and do not expose them to fire. Batteries can explode and release toxic substances.
- Do not attempt to charge non-rechargeable batteries.
- Do not solder batteries into the product.
- Do not discharge batteries by short-circuiting. Batteries can develop a leak, explode, catch fire and injure persons.
- Do not damage batteries and do not attempt to take batteries apart. Batteries can develop a leak, explode, catch fire and injure persons.
Description
Product overview
- Laser exit window
- Selector ring
- On/off button
- Release button
- Securing screw
- Holder
Intended use
The product described is a laser. It is designed exclusively for use with the BX 3 cordless fastening tool. When mounted on its BX‑SH B3 (01) holder and with a certain distance preset, the laser enables speedy pinpointing of the position where the next fastener is to be driven.
The product is intended for indoor use.Items supplied
Laser, 3x AA batteries (not in all markets), operating instructionsOther system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
"Battery state of charge low" indicator
If the battery state of charge drops below 10 %, the laser diode emits a certain sequence of flashes:| Time of occurrence |
Light signal |
|---|---|
| Just after being switched on |
Flashes 5× |
| In operation |
Flashes 5× (every 5 minutes) |
Technical data
| Projected radiuses |
300 mm, 400 mm, 500 mm, 600 mm, 800 mm (11.81 in, 15.75 in, 19.69 in, 23.62 in, 31.50 in) |
| Accuracy (Fastening tool not pressed against surface) |
-15% ... +5% |
| Laser class |
1 |
| Automatic power-off |
≈ 6 min |
| Battery life |
at +20 °C (+68 °F): 15 h (typical) |
| Power source |
3× AA battery (1.5 V) |
| Voltage range |
2.7 V … 5 V |
| Maximum average power output (p) |
≤ 600 mW |
| Weight including batteries |
266 g (9.38 oz) |
| Weight with holder and including batteries |
354 g (12.49 oz) |
| Dimensions, laser (length × width × height) |
103.6 mm × 70.1 mm × 76.4 mm (4.079 in × 2.760 in × 3.008 in) |
| Dimensions, holder (length × width × height) |
85.4 mm × 100.7 mm × 137.3 mm (3.362 in × 3.965 in × 5.406 in) |
| Maximum humidity without condensation |
85% |
| Ambient temperature for operation |
0 ℃ … 50 ℃ (32.0 ℉ … 122.0 ℉) |
| Storage temperature |
−15 ℃ … 70 ℃ (5.0 ℉ … 158.0 ℉) |
Operation
Observe the safety instructions and warnings in this documentation and on the product.Operating the appliance for the first time
The BX-S is delivered with batteries pre-installed (not in all markets). In preparation for operation you must first remove the strip of insulating film that protects the batteries against premature discharge.- Open the lid of the battery compartment.
- Remove the insulating film.
- Position the lid lugs first on the battery compartment and close the lid. The lid snaps closed with an audible click.
Please change batteries
- Open the lid of the battery compartment.
- Insert three AA batteries into the battery compartment.
- Make sure that polarity is correct.
- Make sure that polarity is correct.
- Position the lid lugs first on the battery compartment and close the lid. The lid snaps closed with an audible click.
Installing holder
- Open the securing screw.
- Slip the holder round the fastening tool.
- Tighten the securing screw.
- Check correct installation.
- The slots in the holder must be in exact alignment with the air vents of the fastening tool.
- The slots in the holder must be in exact alignment with the air vents of the fastening tool.
Installing/removing laser
- Install the holder.
- Position the laser with the front retaining lug on the holder.
- Then press the laser with the rear retaining lug on to the holder, so that it engages with an audible click.
- Check that both retaining lugs of the laser are securely engaged in the holder.
- To remove, press the release button on the laser and disengage it from the holder.
Using laser
- Press the on/off button to switch the laser beam on.
- Turn the selector knob to the desired distance.
- Drive a fastener (see the operating instructions for the fastening tool).
- To drive the next fastener, advance the fastening tool on the working surface to where the laser arc is over the exact center of the fastener driven beforehand.
- Drive the next fastener.
- Continue repeating steps 3 to 5 until there are no more fasteners you want to drive.
- Press the on/off button to switch the laser off.
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Blow dust off the laser exit window. Do not touch the laser exit window with your fingers.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
- After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
Checking accuracy
- Mark a point (with a cross) on a level surface.
- Correctly install the laser on the fastening tool.
- Position the fastening tool with the muzzle centered on the cross marked beforehand.
- Switch the laser on and set it to a distance presetting of 300 mm.
- Apply three more marks on the projected laser circle to the right, left and above the initial mark.
- Switch the laser off and lay the fastening tool aside.
- Now measure the distances between the initial mark and each of the three new marks.
- The deviation of each point should not be more than -15 % to +5 % of 300 mm.
- If deviation is outside this tolerance, consult Hilti Service.
- The deviation of each point should not be more than -15 % to +5 % of 300 mm.
- Repeat steps 4 to 7 for all other radius settings (400 mm, 500 mm, 600 mm and 800 mm).
Transport and storage
Transport- Prior to each use and before and after prolonged transport, check the product for damage.
- Store the product and the batteries in a cool and dry place. Comply with the temperature limits stated in the technical data.
- Never leave the product or batteries in direct sunlight, on sources of heat, or behind glass.
- Store the product and batteries where they cannot be accessed by children or unauthorized persons.
- Prior to each use and before and after prolonged storage, check the product for damage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.| Trouble or fault |
Possible cause |
Action to be taken |
|---|---|---|
| Laser does not work. |
The batteries are exhausted. |
|
| The batteries are inserted incorrectly. |
||
| Strip of insulating film not removed prior to initial use. |
||
| The temperature is outside the permissible range. |
|
|
| On/off button or laser faulty. |
|
|
| Incorrect measured results |
Dirt or foreign matter between holder and fastening tool or between holder and laser |
|
| Holder not correctly installed on fastening tool or laser not correctly installed on holder |
|
|
| Laser diode faulty or knocked out of alignment by an impact |
|
|
| Fastening tool not held perpendicular to the surface. |
|
Disposal
Most of the materials from which Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.
In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.