Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
Protection class II (double-insulated)
Only use in enclosed spaces
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms.
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .
Li-ion battery
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards.
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Radio
R 6-22
Generation
01
Serial no.
Safety
General safety instructions
ATTENTION! Read all instructions. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
Keep these instructions in a handy yet secure place.
Workplace
Ensure that the workplace is well lit.
Do not tamper with or attempt to make alterations to the appliance.
The appliance is not intended for wall mounting.
Keep your work area clean and well lit. Cluttered or poorly lit work areas invite accidents.
Personal safety
This product is not intended for use by persons (including children) with physical, sensory or mental disabilities or persons lacking the appropriate experience and/or knowledge. These persons must receive instruction in safe handling of the appliance and must be supervised throughout their use of the appliance by a responsible person.
Explain to children that they are not allowed to play with the appliance.
Children over 8 years of age must receive instruction in safe handling of the appliance and must be supervised throughout their use of the appliance by a responsible person.
Do not wear jewelry such as rings or chains. Jewelry could cause a short circuit resulting in personal injury in the form of burns.
Avoid touching the contacts.
Battery use and care
Observe the special guidelines applicable to the transport, storage and use of Li-ion batteries.
Do not expose batteries to high temperatures, direct sunlight or fire.
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your HiltiService .
If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact HiltiService .
Service
Have the appliance serviced by a qualified repair person using only genuine Hilti spare parts. The safety of the appliance can thus be maintained.
Battery use and care
Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
Use only batteries that are in perfect working order.
Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
Do not under any circumstances modify or tamper with batteries!
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
Never use recycled or repaired batteries.
Never use the battery or a battery-operated power tool as a striking tool.
Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
Do not use or store the battery in explosive environments.
If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
The product described is a cordless jobsite radio. It is designed for playing music as a radio receiver or from various other devices that can be either paired with the product via Bluetooth or connected to it by an AUX cable.
The product is designed for a jobsite environment. Do not expose the product to moisture such as running water, for example.
Use the product only indoors.
For this product, use only Hilti lithium‑ion batteries of the B 22 series. For this product, Hilti recommends the use of the batteries stated in this table.
For these batteries, use only Hilti chargers of the type series listed here.
Other system products approved for use with this product can be found at your local
Hilti Store or at:
www.hilti.group
Bluetooth
This product is equipped with Bluetooth (optional).
Bluetooth is a wireless data transfer system by which the two Bluetooth-enabled products can communicate with each other over a short distance.
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
If the release button is pressed with a battery inserted in the product, subsequently check that the battery is correctly re-engaged and secure.
State of charge and, if applicable, faults are indicated constantly as long as the connected product is switched on.
Status
Meaning
Four (4) LEDs show constantly green
State of charge: 100 % to 71 %
Three (3) LEDs show constantly green
State of charge: 70 % to 51 %
Two (2) LEDs show constantly green
State of charge: 50 % to 26 %
One (1) LED shows constantly green
State of charge: 25 % to 10 %
One (1) LED slow-flashes green
State of charge: < 10 %
One (1) LED quick-flashes green
The Li-ion battery is completely discharged. Recharge the battery. If the LED again starts quick-flashing after the battery has been charged, consult Hilti Service.
One (1) LED quick-flashes yellow
The Li-ion battery or the product in which it is inserted is overloaded, too hot or too cold, or experiencing some other fault. Bring the product and the battery to the recommended working temperature and do not overload the product when it is in use. If the message persists, consult Hilti Service.
One (1) LED shows yellow
The Li-ion battery and the product in which it is inserted are not compatible. Consult Hilti Service.
One (1) LED quick-flashes red
The Li-ion battery is locked and cannot be used. Consult Hilti Service.
Indicators showing the battery's state of health
To check the battery's state of health, press the release button and hold it down for longer than three seconds. The system does not detect a potential malfunction of the battery due to misuse, for example battery dropped or pierced, external heat damage, etc.
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
If a connected product can still be used, the remaining battery capacity is below 50 %. If a connected product can no longer be used, the battery has reached the end of its useful life and has to be replaced. Consult Hilti Service.
The AM frequency band has been selected as the audio source.
The FM frequency band has been selected as the audio source.
AUX has been selected as the audio source.
Indicates the battery state of charge. A bar stands for 25 %.
The Bluetooth symbol indicates whether the appliance is connected to a player. If the Bluetooth symbol lights continuously, a player is connected. If the Bluetooth symbol flashes, the appliance is searching for a player with which it can connect.
The pairing symbol indicates that the appliance is searching for a Bluetooth device with which it has already been paired. The pairing symbol flashes while searching is in progress.
Indicates the volume settings.
Indicates the bass settings.
Indicates the treble settings.
Indicates stereo playback. Stereo playback is activated automatically when signal reception is good enough.
Indicates the memory slot of the station.
Indicates the time. Symbols flash in setup mode.
Cradle for mobile devices
Via Bluetooth or AUX, the radio can play audio from external mobile devices (such as smartphones or tablet computers). The mobile devices can be cradled securely on the radio.
Technical data
Product properties
Power input
160 W
Battery operating voltage
22 V
Battery pack
Li-Ion
Weight (Without battery)
5.1 kg
AM frequency range
526.5 kHz …1,606.5 kHz
FM frequency range
87.5 MHz …108 MHz
DAB / DAB+
174 MHz …240 MHz
USB output voltage
5.0 V / 2.1 A
Ambient temperature
−17 ℃ …40 ℃
Battery
Battery operating voltage
21.6 V
Weight, battery
See the section headed "Intended use"
Ambient temperature for operation
−17 ℃ …60 ℃ (1 ℉ …140 ℉)
Storage temperature
−20 ℃ …40 ℃ (−4 ℉ …104 ℉)
Battery charging starting temperature
−10 ℃ …45 ℃ (14 ℉ …113 ℉)
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
Inserting the back-up batteries
It is not possible to save settings unless the batteries are correctly installed.
Make sure that battery polarity is correct.
Remove the cover from the battery compartment.
Insert the 2 AAA batteries supplied with the appliance into the battery compartment.
Install the cover on the battery compartment.
Switching the appliance on / off
Press the Power button.
Operation
Observe the safety instructions and warnings in this documentation and on the product.
Establishing a Bluetooth connection
If you are prompted for a code, enter the code 0000.
Press the Bluetooth button.
To initially pair the radio manually, press the Bluetooth button and hold it down for 2 seconds.
The Bluetooth symbol flashes.
Select the Hilti radio on the mobile device.
The devices have been successfully paired when the Bluetooth and pairing symbols both show continuously in the display.
If the radio has already been paired to the mobile device, press the Bluetooth button.
Pairing starts automatically and the pairing symbol on the screen starts to flash.
The radio searches for a signal for a maximum of 3 minutes.
The pairing symbol appears on the display to indicate that the devices are paired.
The Bluetooth symbol appears in the display to indicate that the radio has found a paired mobile device.
If you have a second radio, you can synchronize the two radios and listen to music in stereo.
Radio (A) is connected to your mobile device. This radio is the master.
Switch radio (B) on.
On radio (B) , press the Bluetooth button.
On master radio (A) , press the Preset button (an acoustic signal sounds to confirm that the connection has been established).
Shortly after, music will start playing in stereo on the two radios.
Making an NFC connection
Activate the NFC function on your mobile device (if it supports NFC).
Hold you mobile device close to the NFC interface of the radio. This is on the right-hand side and is indicated by the NFC symbol.
You must accept the NFC connection on your mobile device when the connection is established for the first time.
Setting the audio source
Press the mode button to select the audio source: AM, FM, AUX or Bluetooth.
Press the mode button.
Select the desired audio source. You can choose between AM, FM, AUX and Bluetooth.
Searching for and saving stations
Quickly turn the knob a short distance to start the automatic station search.
Use the knob to select a frequency.
Press the 'Preset' button.
Press the knob to save this frequency.
Positioning the antenna
Swivel the antenna to the position at which reception is clearest.
Adjusting the volume
Turn the power button clockwise to increase the volume.
Turn the power button counterclockwise to reduce the volume.
Equalizer settings
This allows you to make adjustments to the bass and treble settings.
Press the equalizer button (EQ) .
Use the knob to select either bass or treble for adjustment.
Use the knob to change your settings.
Audio playback from a mobile device via Bluetooth
For good audio quality, set the volume of the external device to very high. Further adjustment of the volume should then be made using the controls on the appliance.
Establish a Bluetooth connection between the mobile device and the radio.
Select the play mode (Bluetooth).
Press the Start/Pause button on your mobile device or press the knob to start or pause audio playback.
Use the arrow buttons on the mobile device or turn the knob to change tracks and to start.
Audio playback from an external device via AUX
For good audio quality, set the volume of the external device to very high. Further adjustment of the volume should then be made using the controls on the appliance.
Select the play mode (AUX or Bluetooth).
Press the start/pause button on your mobile device to start or pause audio playback.
Use the arrow buttons on the external device to change tracks and to start.
USB charging function
The USB connector provides charging power only. Data transfer is not possible.
Use a USB cable to connect your mobile device to the USB port of the radio.
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
Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain). If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service.
Keep the battery free of extraneous oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry cloth. Do not use cleaning agents containing silicone as these can attack the plastic parts. Do not touch the contacts of the battery and do not remove the factory-applied grease from the contacts.
Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Maintenance
Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by
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
Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
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
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, contact
Hilti Service.
Malfunction
Possible cause
Action to be taken
Radio does not switch on.
Battery discharged
Charge the battery or insert a new battery.
Battery defective
Check the battery by pressing the two buttons at the sides. If the LEDs light up the radio might be defective. If the LEDs do not light up the battery is defective.
Contact Hilti Service.
Radio defective
Contact Hilti Service.
Border of the battery symbol flashes, no segment of the state of charge indicator filled (the indicator assumes this state for a short time before the appliance switches itself off).
Battery too hot
Wait until the battery cools down.
Battery too cold
Wait until the battery warms up.
Battery defective
Check the battery by pressing the two buttons at the sides. If the LEDs light up the radio might be defective. If the LEDs do not light up the battery is defective.
Contact Hilti Service.
Settings such as clock time are no longer saved in memory.
Batteries discharged
Replace the back-up batteries.
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
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Most of the materials from which
Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti sales representative for further information.
Do not dispose of power tools, electronic equipment or batteries as household waste!
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.
FCC statement (applicable in US) / IC statement (applicable in Canada)
This device has been tested and found to comply with the limits for a class A digital device, pursuant to part 15 of the FCC rules. These limits are intended to ensure adequate protection against electromagnetic interference when the device is operated in areas used for commercial purposes. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause interference to radio communications. The user must bear costs incurred due to interference that operation of this device in residential areas can cause.
This device is in compliance with paragraph 15 of the FCC rules and the RSS‑210 specifications of ISED.
Operation is subject to the following two conditions:
This device shall cause no harmful interference.
This device must accept any interference received, including interference that may cause undesired operation.
Changes or modifications not expressly approved by
Hilti may restrict the user’s authorization to operate the equipment.
Further information
China RoHS (Restriction of Hazardous Substances)This table is valid for the China market.
Taiwan RoHS (Restriction of Hazardous Substances)This table is valid for the Taiwan market.
Hilti Li-ion batteries
Instructions for Use and OperationThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-Ion cells joined together. These batteries are to be used in Hilti power tools exclusively. When using Hilti power tools, use
Hilti original battery packs!
Hilti batteries are state of the art and are equipped with cell management and cell protection systems.
DescriptionThe batteries are composed of cells that contain lithium-ion storage materials that are capable providing high specific energy density. Unlike NiMH and NiCd batteries, Li-ion batteries have a minimal memory effect, but they are extremely susceptible to external impact, deep discharge, and high temperatures. See
Safety WARNING Find our battery-powered products at your
Hilti Store or at:
www.hilti.group | USA:
www.hilti.com Safety
Batteries must not be modified or tampered with!
Never use recycled or repaired batteries conducted by non-Hilti companies.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. Examine your batteries regularly for signs of damage, such as shredding, cuts or punctures.
Never use the battery or a battery-operated power tool as a hammer.
Avoid eye or skin contact with leaking liquids!
See What to do in case of damaged batteries
Damaged batteries can leak fluid which may moisten adjacent objects. Clean these objects with warm soapy water and replace the damaged batteries.
See What to do in case of damaged batteries
Never expose batteries to elevated temperature, sparking, or an open flame because the battery may explode.
Do not touch the battery poles with your fingers, tools, jewelry, or other metallic objects because this may cause a short circuit, electrical shock, burns or explosions.
Keep batteries away from rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
Only use chargers and power tools approved for the specific battery type. Read and follow the instructions in the respective user manuals.
Do not store or use the battery in explosion-prone environments containing combustible liquids or gases. An unexpected battery malfunction can cause an explosion under those conditions.
What to do in case of damaged batteries
If a Hilti battery is found to be damaged, contact your Hilti service partner.
If a battery is leaking, use safety goggles and gloves to avoid direct eye or skin contact.
To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then, close the lid air-tight and store the container away from flammable gases, liquids, or objects.
Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
Use a chemical spill cleanup kit to remove leaked battery fluid.
What to do in case of dysfunctional batteries
Watch for abnormal battery behavior, such as faulty charging or unusually long charging times, noticeable power loss, unusual charger LED activity, or leaking fluids. These are signs of an internal problem.
If you suspect an internal battery problem, contact your Hilti service partner.
Should the battery be in operational or no longer chargeable or leaking fluid, dispose of it as described above.
See What to do in case of damaged batteries .
What to do in case of a battery fire
WARNING
Battery fire hazard! A burning battery releases hazardous and potentially explosive liquids and fumes that can lead to corrosion injuries, burns or explosions.
Wear your personal protective equipment when you tackle a battery fire.
Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
Leave the room immediately in case of intense smoke emission.
Consult a doctor in case of any skin or respiratory irritation.
Battery fires should be extinguished with water. Powder fire extinguishers and fire blankets are ineffective with Li-Ion batteries. Fires started by a lithium-ion battery in nearby materials can be extinguished with any appropriate extinguishing agent.
Do not try to move large quantities of damaged, burning, or leaking batteries. Instead, remove surrounding materials and isolate the batteries. If the scale of the fire is larger than can be extinguished with available methods, contact the nearest firefighting authority.
In the case of a single burning battery,:
Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
Wait for the battery to cool down completely.
See What to do in case of damaged batteries .
Shipping and storage
Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
Do not store batteries on the charger. Separate battery from charger after use.
Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
Batteries should not be sent through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
Do not transport batteries in bulk, loosely packaged. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit.
Maintenance and disposal
Keep the battery free of oil and grease. If the battery is exposed to oil or grease, remove the contamination with a clean dry rag.
Never use a battery with clogged venting slots. Clean the venting slots carefully with a soft brush to prevent debris from entering the battery.
Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
If the battery becomes dirty, clean it with a soft brush or clean, dry rag.
If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
See What to do in case of damaged batteries
Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
Do not dispose of batteries as household waste.
Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.