Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
National waste-materials management system
“Off” position
Continuous dispensing
Measured dispensing 5...70 ml
Measured dispensing 1...14
Discard function
Repeat function
Direct current (DC)
The product supports near-field communication (NFC) technology compatible with iOS and Android platforms.
Li-ion battery
Never use the battery as a striking tool.
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way.
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards.
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Type:
HDE 500-22
Generation:
02
Serial number:
Safety
General power tool safety warnings
WARNINGRead all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference. The term "power tool" in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
Keep work area clean and well lit. Cluttered or dark areas invite accidents.
Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a power tool.Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
Dress properly. Do not wear loose clothing or jewellery. Keep your hair and clothing away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
Power tool use and care
Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
Battery tool use and care
Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
Do not use a battery pack or tool that is damaged or modified. Damaged or modified batteries may exhibit unpredictable behaviour resulting in fire, explosion or risk of injury.
Do not expose a battery pack or tool to fire or excessive temperature. Exposure to fire or temperature above 130° C (265 °F) may cause explosion.
Follow all charging instructions and do not charge the battery pack or tool outside the temperature range specified in the instructions. Charging improperly or at temperatures outside the specified range may damage the battery and increase the risk of fire.
Service
Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
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
Wear eye protection and protective gloves when changing accessories.
Prior to use, read and comply with the safety data sheet for the product, the instructions on the packaging and the instructions for use of the foil pack.
Begin injecting the compound until it is in the immediate working area.
Never point the product toward yourself or other persons.
Never leave the product unattended.
Do not use the product if parts are damaged or if operating controls do not function faultlessly. Have the product repaired by Hilti Service.
Safety at the workplace
Keep the workplace tidy. Objects which could cause injury should be removed from the working area.
Wear non-skid shoes.
Take the influences of the surrounding area into account. Do not use the product where there is a risk of fire or explosion.
Do not use defective/worn cartridges.
Battery use and care
Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
Use only batteries that are in perfect working order.
Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
Do not under any circumstances modify or tamper with batteries!
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
Never use recycled or repaired batteries.
Never use the battery or a battery-operated power tool as a striking tool.
Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
Do not use or store the battery in explosive environments.
If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
Front locating lug for installation of the foil pack holder / cartridge
Cradle for the foil pack holder / cartridge
Rear locating lug for installation of the foil pack holder / cartridge
Tool LED
Dispensing mode selector switch
Parallel piston rods with grip
Release button
Grip
Battery
Battery status indicator
Battery release button
Installation opening for accessories
Trigger
Foil pack
Foil pack holder, black
Foil pack holder, red
Cartridge
Intended use
The dispenser is designed to dispense the contents of Hilti foil packs and cartridges in a controlled operation. The HDE 500‑22 cordless dispenser is designed exclusively for use with Hilti 330 ml or 500 ml foil packs and 580 ml cartridges.
The dispenser can be used with either a foil pack holder or a cartridge:
For this product, use only Hilti Nuron lithium-ion batteries of the B 22 series. For optimum performance, Hilti recommends the batteries stated in this table for this product.
For these batteries, use only Hilti chargers of the type series stated in this table.
Items supplied
Dispenser, operating instructions
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
If the release button is pressed with a battery inserted in the product, subsequently check that the battery is correctly re-engaged and secure.
State of charge and, if applicable, faults are indicated constantly as long as the connected product is switched on.
Status
Meaning
Four (4) LEDs show constantly green
State of charge: 100 % to 71 %
Three (3) LEDs show constantly green
State of charge: 70 % to 51 %
Two (2) LEDs show constantly green
State of charge: 50 % to 26 %
One (1) LED shows constantly green
State of charge: 25 % to 10 %
One (1) LED slow-flashes green
State of charge: < 10 %
One (1) LED quick-flashes green
The Li-ion battery is completely discharged. Recharge the battery. If the LED again starts quick-flashing after the battery has been charged, consult Hilti Service.
One (1) LED quick-flashes yellow
The Li-ion battery or the product in which it is inserted is overloaded, too hot or too cold, or experiencing some other fault. Bring the product and the battery to the recommended working temperature and do not overload the product when it is in use. If the message persists, consult Hilti Service.
One (1) LED shows yellow
The Li-ion battery and the product in which it is inserted are not compatible. Consult Hilti Service.
One (1) LED quick-flashes red
The Li-ion battery is locked and cannot be used. Consult Hilti Service.
Indicators showing the battery's state of health
To check the battery's state of health, press the release button and hold it down for longer than three seconds. The system does not detect a potential malfunction of the battery due to misuse, for example battery dropped or pierced, external heat damage, etc.
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
If a connected product can still be used, the remaining battery capacity is below 50 %. If a connected product can no longer be used, the battery has reached the end of its useful life and has to be replaced. Consult Hilti Service.
Tool LED for dispensing operation
Status
Dispensing-wheel setting/symbol
Meaning
LED shows green
Discard function Repeat function Measured dispensing
Discarding/dispensing completed successfully.
LED shows red
Discard function Repeat function Measured dispensing
Discarding/dispensing aborted. Discarding/dispensing volume not fully ejected.
LED flashes red
Discard function Repeat function Measured dispensing
The volume left in the pack is not sufficient for the next dispensing operation or repeat of the previous dispensing operation as set by means of the dispensing wheel, or for the discharge function.
Technical data
HDE 500‑22
Weight without battery
1.9 kg (4.2 lb)
Rated voltage
21.6 V
Storage temperature
−40 ℃ …85 ℃ (−40 ℉ …185 ℉)
Ambient temperature for operation
−17 ℃ …60 ℃ (1 ℉ …140 ℉)
Battery
Battery operating voltage
21.6 V
Weight, battery
See the section headed "Intended use"
Ambient temperature for operation
−17 ℃ …60 ℃ (1 ℉ …140 ℉)
Storage temperature
−20 ℃ …40 ℃ (−4 ℉ …104 ℉)
Battery charging starting temperature
−10 ℃ …45 ℃ (14 ℉ …113 ℉)
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
Do not secure a tool tether to the belt hook. Do not use a belt hook to lift the product.
Comply with the national regulations for working at heights.
As drop arrester for this product, use the
Hilti tool tether #2261970 or #2261971.
Secure the carabiner to a load-bearing structure. Check that the carabiner holds securely.
Depending on which type of Hilti tool tether is used, secure either the second carabiner or the loop to the product as shown in the illustration. Check that it holds securely.
Comply with the operating instructions of the
Hilti tool tether.
Inserting the foil pack holder and foil pack
CAUTION
Trap hazard Hands can be trapped if care is not exercised when swiveling the foil pack holder closed.
Keep your hands clear of the cradle area when swiveling the foil pack holder into position.
CAUTION
Risk of injury Chemicals hazard.
Check the foil pack holder for damage and soiling. Both pistons must move smoothly and easily in both directions over the full length of their travel in the foil pack holder. Replace the foil pack holder if it is damaged and/or badly soiled.
Press the release button.
Pull the piston rod back as far as they will go.
Fit the front end of the foil pack holder into the front locating lug.
Pull the foil pack holder on to the rear locating lug and swivel the foil pack holder up.
Screw the static mixer (mixing nozzle) onto the foil pack.
Push the foil pack into the foil pack holder.
Swivel the foil pack holder into the dispenser.
Inserting the cartridge
Press the release button.
Pull the piston rod back as far as they will go.
Fit the front end of the cartridge into the front locating lug.
Pull the cartridge on to the rear locating lug and swivel the cartridge up.
Screw the static mixer (mixing nozzle) onto the foil pack.
Swivel the cartridge into the dispenser.
Discarding initially dispensed mortar
WARNING
Risk of injury Chemicals hazard.
Never point the dispenser toward yourself or other persons. Begin dispensing mortar only after the mixing nozzle has been screwed on. Incorrect use can lead to injury.
You must discard the initially dispensed volume of mortar every time the static mixer (mixing nozzle) is changed.
The initially dispensed mortar is not suitable for use.
Manually discarding the initial quantity of mortar
Set the dispensing mode selector switch to .
Squeeze the trigger until the mixing nozzle is completely full.
Set the dispensing mode selector switch to the appropriate volume of mortar for discarding .
Discard the amount of mortar stated in the instructions for the foil pack.
Discard the initially dispensed volume of mortar.
Initial quantity of mortar dispensed with discard function
The benefit of the discard function is that you can set the quantity of mortar to be discarded.
Before starting, check that the battery still has enough power for you to use the discard function.
Set the dispensing mode selector switch to .
Squeeze the trigger until the mixing nozzle is completely full.
Turn the dispensing wheel to the discard function and keep the trigger squeezed until the dispenser automatically stops the discard function.
If the required discard quantity was correctly dispensed, the tool LED shows green.
Otherwise, the tool LED shows red. If this happens, repeat the procedure for discarding the mortar.
Failure to repeat the procedure for discarding mortar can lead to mixing disruptions and reduced load values.
The mixing nozzle must be filled all the way to the tip before ejection of the mortar required for discarding commences. Otherwise, the discarded quantity is not sufficient.
Use only the mixing nozzle supplied when discarding the initially ejected mortar. Do not use an extension tube.
Operation
Observe the safety instructions and warnings in this documentation and on the product.
Injecting mortar
For each new foil pack and each new cartridge and if the mortar has hardened inside the mixing nozzle, always use a new static mixer (mixing nozzle).
Press the trigger.
Inject the mortar.
Repeat function
The repeat function allows you to repeat dispensing with the measured quantity of mortar last dispensed, regardless of the dispensing mode (continuous dispensing / measured dispensing).
Turn the dispensing wheel to the repeat symbol and keep the trigger squeezed until the dispenser automatically stops dispensing.
If the volume was correctly dispensed, the tool LED shows green.
If the intended volume was not fully dispensed because dispensing was aborted, the tool LED shows red.
After grouting each drillhole, always check that there is enough mortar in the drillhole.
Observe the grouting volume of mortar stated in the instructions for the foil pack.
Completion of aborted dispensing operation
If the dispensing operation was aborted prematurely by:
release of the trigger before the end of the dispensing operation
not enough mortar for the dispensing operation left in the foil pack/cartridge
battery discharged
the tool LED shows red.
You can complete an interrupted dispensing operation by double-clicking and holding down the trigger.
The green tool LED shows to indicate correct completion of the dispensing operation.
After changing foil pack/cartridge and discarding the initially dispensed volume of mortar by means of the discard function, before double-clicking the trigger you must reset the dispensing wheel to the dispensing volume originally desired.
This function is available for all positions on the dispensing mode selector switch, except the positions for continuous dispensing and discard function.
After grouting each drillhole, always check that there is enough mortar in the drillhole.
Observe the grouting volume of mortar stated in the instructions for the foil pack/cartridge.
Removing the foil pack holder and foil pack
Set the dispensing mode selector switch to .
Press the release button.
Pull the piston rod back as far as they will go.
Swivel the foil pack holder up.
Remove the foil pack.
Press the tab on the foil pack holder.
Press the foil pack holder down at the rear locating lug.
Pull the foil pack holder down from the front locating lug.
Removing the cartridge
Set the dispensing mode selector switch to .
Press the release button.
Pull the piston rod back as far as they will go.
Swivel the cartridge upwards.
Press the cartridge down at the rear locating lug.
Pull the cartridge down from the front locating lug.
Care and maintenance
WARNING
Risk of injury with battery inserted !
Always remove the battery before carrying out care and maintenance tasks!
Care of the product
Carefully remove stubborn dirt from the tool. Keep the tool LED clean at all times.
Carefully clean the ventilation slots, if present, with a dry brush.
Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Oil the piston rods when necessary.
Care of the Li‑ion batteries
Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully using a dry, soft brush.
Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain). If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service.
Keep the battery free of oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry rag. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Maintenance
Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local
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
Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
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
Transport and storage of dispensers
For transporting and storing the tool, set the dispensing mode selector switch to .
Troubleshooting
If a problem occurs, always observe the charge-status and fault indicator of the battery. See the section headed
Status indicators of the Li‑ion battery .
If the trouble you are experiencing is not listed in this table or you are unable to rectify the problem by yourself, contact
Hilti Service.
Trouble or fault
Possible cause
Action to be taken
Product does not work.
The battery is not fully inserted.
Push the battery in until it engages with an audible click.
Battery is discharged.
Change the battery.
Dispensing mode selector switch set to
Select the desired dispensing volume.
Product prematurely aborts dispensing operation
The overload cut-out is activated; mortar in the mixing nozzle has hardened
Replace the static mixer (mixing nozzle).
The overload cut-out is activated; The dispensing pressure required is too high for the product.
Increase the foil pack temperature.
Foil pack empty
Replace the empty foil pack.
The battery does not engage with an audible click.
The retaining lug on the battery is dirty.
Clean the retaining lug and push the battery in until it engages. If the problem persists, consult Hilti Service.
The product or battery gets very hot.
The product is overloaded (application limits exceeded).
Pay attention to the power and performance rating of the product before using it, i.e check its suitability for the job on hand. See “Technical data” section.
Electrical fault
Switch the product off immediately, remove the battery, keep it under observation, allow it to cool down and contact Hilti Service.
The foil pack holder cannot be swiveled into the product.
The foil pack is not pushed fully into the holder.
Push the foil pack into the foil pack holder as far as it will go.
Piston rods not pulled back fully
Press the release button and pull the piston rods all the way back.
The foil pack holder does not engage with an audible click
The retaining lugs are dirty
Clean the retaining lugs.
The retaining lugs are defective
Insert a different foil pack holder. Contact Hilti Service if the problem persists.
No mortar is dispensed from the mixing nozzle
Mortar in the mixing nozzle has hardened
Unscrew the mixing nozzle containing the hardened mortar and fit a new mixing nozzle.
Dispensing switch set to repeat function, but dispensing quantity not defined beforehand.
Define a dispensing quantity before you use the repeat function.
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
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Most of the materials from which
Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
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
Instructions for safety and useThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-ion cells joined together. These batteries are to be used in Hilti power tools exclusively. Use only genuine
Hilti batteries!
DescriptionHilti batteries have cell-management and cell-protection systems.
The batteries are composed of cells that contain lithium-ion storage materials capable of providing high specific energy density. Li-ion cells have a minimal memory effect, but they are very susceptible to external impact, deep discharge, and high temperatures.
The products approved for use with
Hilti batteries can be found in your
Hilti Store or at:
www.hilti.group Safety
Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
Do not under any circumstances modify or tamper with batteries!
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
Never use recycled or repaired batteries.
Never use the battery or a battery-operated power tool as a striking tool.
Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
Do not use or store the battery in explosive environments.
If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Follow the instructions in the section headed What to do in case of a battery fire .
What to do in case of damaged batteries
Always contact Hilti when a battery is damaged.
Never use a battery that is leaking fluid.
Avoid direct eye and/or skin contact with fluid leaking from a battery. Always wear protective gloves and eye protection when undertaking tasks involving battery fluid.
Use a chemical spill cleanup kit to remove leaked battery fluid. Comply with the locally applicable cleanup regulations for battery fluid.
To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then seal the lid air-tight and store the container away from flammable gases, liquids or objects.
Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
What to do in case of dysfunctional batteries
Watch for abnormal battery behavior, such as faulty charging, unusually long charging times, noticeable power loss, unusual LED activity, or leaking fluids. These are signs of an internal problem.
If you suspect an internal battery problem, contact Hilti Service.
A battery that no longer works, cannot be recharged or leaks fluid has to be disposed of correctly. See the section headed Maintenance and disposal .
What to do in case of a battery fire
WARNING
Battery fire hazard! A burning battery releases hazardous and potentially explosive liquids and fumes that can lead to corrosion injuries, burns or explosions.
Wear your personal protective equipment when you tackle a battery fire.
Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
Leave the room immediately in case of intense smoke emission.
Consult a doctor in case of any skin or respiratory irritation.
Alert the fire service before you start tackling the fire.
Use only water to tackle a battery fire and keep as far from the fire as effective extinguishing permits. Powder fire extinguishers and fire blankets are ineffective with Li-ion batteries. Fire in nearby materials can be extinguished with appropriate extinguishing agents.
Do not try to move large quantities of burning batteries. Instead, isolate the batteries by removing unaffected materials from the immediate vicinity.
In the case of a battery that does not cool down, or a smoking or burning battery:
Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
Leave the battery in the bucket for at least 24 hours until it has cooled down completely.
See the section headed What to do in case of damaged batteries .
Shipping and storage
Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
Never transport batteries in bulk form (loose, unprotected). During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
Maintenance and disposal
Keep the battery free of oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry rag.
Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully using a dry, soft brush.
Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
See the section headed What to do in case of damaged batteries .
Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Comply with the locally applicable regulations for transporting damaged batteries!
Do not dispose of batteries as household waste.
Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.