The controls on the fastening tool are as follows:
 |
Release button for selector ring for driving energy The button unlocks the selector ring for driving energy or is used for removal of the exhaust gas piston return unit.
|
 |
Release button for fastener guide (A) The button unlocks the fastener guide so that the fastener guide can be changed or the fastening tool cleaned.
|
The product described is a fastening tool for driving nails, studs and fasteners into steel.
Use the product only in combination with the equipment designed for use with the fastening tool. Fastener guides, pistons and fasteners must be compatible with one another.
Use the product only with spare parts and accessories from
Hilti and with cartridges and fasteners from
Hilti , or other suitable cartridges and fasteners.
The Bluetooth
® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc and any use of such marks by
Hilti Corporation is under license.
Bluetooth is a wireless data transfer system by which the two Bluetooth-enabled products can communicate with each other over a short distance.
This product has a Bluetooth Low Energy module. The module enables communication and data transfers between smart phones and
Hilti gateway. The module is used for checking the status of the product and can submit data attributes such as location of the receiving device, runtime, total application count, application count during interval and timestamp of transfer.
Information about the connectivity functions offered can be found in the respective
Hilti application (app).
Data transmission via Bluetooth
The data transmission interval can vary, depending on the available power source of the product. The signal range can vary greatly depending on external conditions, including the receiving device used. The Bluetooth range can be significantly less inside closed rooms and through metallic barriers (e g. walls, shelving units, cases, etc.). Depending on ambient conditions, several transmission intervals may be required before the product is detected.
If the product is not detected, check the following:
• Is the distance to the mobile terminal device too great?
→ Reduce the distance between the mobile terminal device and the product.
Installing and setting up the app
In order to be able to use the connectivity functions, you first have to install the respective
Hilti app.
(1.) Download the app from the corresponding app store (Apple App Store, Google Play Store).
You will require a user account on the corresponding app store to do this.
(2.) When you start the app for the first time, either log in with your account or register.
(3.) The display of your mobile terminal device will show you all the subsequent steps required to connect the product to the mobile device.
In addition, be sure to study all the notes on operation in the app. This will give you a better overview of how the connection is made and how the functions are used.
WARNING
Risk of injury by unexpected explosion! Use of cartridges that do not meet the minimum safety requirements can lead to a build-up of unburned powder. A sudden explosion and severe injuries to the operator and bystanders can result.
- Use only cartridges that meet the minimum safety requirements of your local statutory regulations!
- Adhere to the maintenance intervals as stated and have the fastening tool cleaned regularly by Hilti-Service !
Use only the
Hilti DX cartridges listed in this table, or other suitable cartridges that are compliant with the minimum safety requirements:
- It is a requirement for EFTA countries that the cartridges must be CE-compliant and must bear the CE mark of compliance.
- It is a requirement for the United Kingdom that the cartridges must be UKCA-compliant and must bear the UKCA mark of compliance.
- It is a requirement for the USA that the cartridges must be compliant with the stipulations set out in ANSI A10.3-2020.
- It is a requirement for the non-European member states of the C.I.P. that the cartridges must have C.I.P. approval for the DX fastening tool used.
- It is a requirement for the remaining countries that the cartridges must have passed the firing-residues test in accordance with EN 16264 and must have a manufacturer's declaration to this effect.
Cartridges
Ordering designation
|
Color
|
Power level
|
DX 6 cartridge
|
titanium-gray
|
strong
|
DX 6 cartridge
|
black
|
extra-strong
|
You must always observe certain minimum distances and spacing when driving fasteners. They can differ, depending on the product.
Comply with the instructions for use in the operating instructions of the fastener used, in the
Hilti
Direct Fastening Technology Manual or the corresponding local
Hilti 'Technical Guide to Fastening Technology'.
Fastening to steelAlways observe the following minimum distances and spacing when fastening to steel:
- The minimum distance from the edge of the base material to the fastener must be at least 15 mm.
- The minimum center-to-center distance between two fasteners is 20 mm.
- The base material must have a thickness of at least 6 mm.