Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property.
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
Read the operating instructions.
Button symbols
The buttons on the product are as follows:
Distance button
Functions button
Add button
Subtract button
Bluetooth button
Memory | Timer button
Reference button
On | Delete | Off button
Display icons (functions)
The icons that can appear on the product's display are as follows:
Measuring area
Measure volumes
Pythagoras (2-point)
Pythagoras (3-point)
Layout function
Display icons (general symbols)
The icons that can appear on the product's display are as follows:
Battery state of charge
Bluetooth
Add distances
Subtract distances
Reference
Timer
Data storage
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration issued by the certification department can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
There is a label bearing the serial number on the bottom of the battery compartment.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Laser range meter
PD-I
Generation
02
Serial no.
Laser information on the product
Designation and explanation
Class 2 laser. Do not stare into the beam. Do not direct the beam toward other persons or toward areas in which other persons, who are not involved in the work with lasers, may be present.
Laser classification for Class 2 laser products
The device complies with Laser Class 2 in accordance with IEC 60825-1:2014 /EN 60825-1:2014. These devices can be used without further protective measures.
Data for classification
Wavelength
620 nm … 690 nm
Maximum radiant output power for classification
≤ 1 mW
Pulse duration
≥ 400
Pulse repetition frequency
320 MHz
Beam divergence
0.16 mrad x 0.6 mrad
CAUTION
Risk of injury! Do not direct the laser beam toward persons.
Never look directly into the source of the laser beam. In the event of direct eye contact, close your eyes and move your head out of the path of the laser beam.
Safety
Safety instructions
General safety measures
Check the product for damage before use. Have damage repaired by Hilti Service.
Check the accuracy of the product if it has been dropped or subjected to other mechanical stresses.
Although the product is designed for the tough conditions of jobsite use, like other measuring instruments it should be treated with care.
When not in use, products must be stored in a dry, high place or locked away out of reach of children.
The product is not intended for use by children.
Comply with national health and safety requirements.
Basic safety precautions
In addition to the information relevant to safety given in each of the sections of these operating instructions, the following points must be strictly observed at all times. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
Keep all safety instructions and other instructions for future reference.
Stay alert, watch what you are doing and use common sense when operating the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product can result in serious personal injury.
Do not render safety devices ineffective and do not remove information and warning notices.
Laser radiation in excess of Class 2 can be emitted if the product is opened without correct procedure being followed. Have the product repaired by Hilti Service only.
Do not tamper with or attempt to make alterations to the product.
Before starting to use the product, always make sure that it is full working order.
Readings taken through panes of glass or similar materials can falsify the result of measurement.
People passing through the laser beam or other quick changes in measuring conditions can falsify the result of measurement.
Never aim the product against the sun or other powerful light sources.
Take the influences of the surrounding area into account. Do not use the device where there is a risk of fire or explosion.
Follow the directions for operation, care and maintenance in the operating instructions.
Working safely with laser tools
Laser Class 2/Class II tools may be operated only by appropriately trained persons.
Laser beams should not be projected at eye height.
Precautions must be taken to ensure that the laser beam does not unintentionally strike highly reflective surfaces.
Precautions must be taken to ensure that persons do not stare directly into the beam.
The laser beam must not be allowed to project beyond the controlled area.
Switch the laser tool off when it is not in use.
Store laser tools, when not in use, in places to which unauthorized persons have no access.
Proper arrangement of the workplace
Avoid unusual postures when working on ladders. Maintain firm footing and balance at all times.
Secure the site where you are taking measurements and when using the product do not direct the laser beam toward other persons or toward yourself.
When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use.
Use the product only within its specified limits.
Keep the laser aperture clean to avoid measurement errors.
Comply with the national accident prevention regulations.
Electromagnetic compatibility
Although the product complies with the strict requirements of the applicable directives,
Hilti cannot entirely rule out the possibility of interference to the product caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions, or if you are unsure. Likewise,
Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment). The product complies with the requirements of class A; the possibility of interference in a residential environment cannot be excluded.
Only for Korea: This laser range meter is suitable for commercial and industrial use and for the electromagnetic radiation encountered in this field (Class A). The user must be aware of this and shall not use this laser range meter in residential environments.
Description
Product overview
Display
Distance button
Functions button
Bluetooth button
Memory | Timer button
On | Delete | Off button
Reference button
Subtract button
Add button
Spike
Battery-compartment cover
Intended use
The product described is a laser range meter. It is designed for single measurements and for continuous measurement of distances.
Distances can be measured to any stationary target, i.e. concrete, stone, wood, plastic, paper, etc. The use of prisms or other highly reflective targets is not permitted and can falsify the results.
The product is approved for use with batteries of type AAA.
Bluetooth®
This product has Bluetooth.
Bluetooth is a wireless data transfer with which two Bluetooth-enabled devices can communicate with each other over a short distance.
Hilti products ship ex-works with Bluetooth deactivated.
The
Bluetooth® wordmark and the logo are registered trademarks and the property of
Bluetooth SIG, Inc. and
Hilti has been granted a license to use these trademarks.
Switching Bluetooth on or offPress the
button and hold it down for 2 seconds.
Items supplied
Laser range meter, belt pouch, wrist strap, 2x AAA battery (1.5 V), "Quick Start" guide, safety instructions, manufacturer's certificate, declaration of conformity
Other system products approved for use with this product can be found at your local
Hilti Store or at:
www.hilti.group .
Technical data
Product properties
Dimensions (L x W x H)
4.9 in x 1.8 in x 1.0 in (125 mm x 46 mm x 26 mm)
Weight (including batteries)
3.9 oz (111 g)
Length (spike)
2.6 in (65 mm)
Smallest displayed unit
0.004 in (0.1 mm)
Protection class in accordance with IEC 60529
IP 54
Operating temperature
14 ℉ … 122 ℉ (−10 ℃ … 50 ℃)
Storage temperature
−13 ℉ … 158 ℉ (−25 ℃ … 70 ℃)
Laser properties
Laser type
635 nm | < 1 mW
Laser class in accordance with EN 60825-1:2014
Laser class 2
Range (ideal conditions)
0 ft - 2.0 in … 328 ft (0.05 m … 100 m)
Accuracy (ideal conditions) ±
0.06 in (1.5 mm)
Battery time
Battery time (measurements)
≈ 10,000
Automatic switch-off (laser)
after 90 seconds
Automatic switch-off (product)
after 180 seconds
Bluetooth Smart
Version
v4.0
Range
< 32 ft - 10 in (< 10 m)
Before use
Inserting the batteries
Do not use damaged batteries.
Make sure that battery polarity is correct.
Change the batteries as soon as the
indicator lights up, and always change the batteries as a pair.
Flip the contact spike forward.
Open the battery compartment.
Insert the batteries.
Close the battery compartment and flip the contact spike back to the closed position.
Switching the laser range meter on or off
CAUTION
Risk of injury! Do not direct the laser beam toward persons.
Never look directly into the source of the laser beam. In the event of direct eye contact, close your eyes and move your head out of the path of the laser beam.
Press the button to switch the laser range meter on.
Press the button and hold it down for 2 seconds to switch the laser range meter off.
Undo
Take a measurement.
Press the button.
The last measurement is undone.
Pressing the
button again takes you directly back to the "Measure distance" function.
Basic settings
Setting the reference
The "Reference" setting influences whether the length of the product is taken into account in measurement. You can select either of two references:
• Top edge of the laser range meter (product length is excluded)
• Bottom edge of the laser range meter (product length is included)
The default setting is
bottom edge of the laser range meter.
Press the button and hold it down for 2 seconds to toggle the reference setting.
The reference is changed.
The reference is reset to the default setting when you switch the device off.
Setting the unit of measure
The unit of measure cycles through the following:
The default unit of measure can vary, depending on the country.
Simultaneously press the and buttons and hold them down for 2 seconds.
The unit of measure is changed.
Repeat step 1 until the unit of measure you want is set.
The setting you select is saved as the new default setting.
Switching the acoustic signal on or off
Simultaneously press the and buttons and hold them down for 2 seconds.
The setting you select is saved as the new default setting.
Using the contact spike
The contact spike makes the laser range meter easier to aim when you are targeting a fixed position.
Measurements from awkward area are easier, for example when you have to measure a diagonal from a corner.
Flip the contact spike open through 90°.
The contact spike can be used as an end stop.
Flip the contact spike open through 180°.
The reference is changed automatically.
Measuring using a target plate
Use the target plate to measure distance under the following unfavorable conditions:
The wall is not sufficiently reflective due to the type of surface.
The target point is not on a surface.
The distance to be measured is too long.
The light conditions are unfavorable (bright sunshine).
When measuring with a target plate, add 2 mm (1/16 in) to the measured distance.
Operation
Overview of the functions
Press the
button to cycle through the main functions.
The "Measure distance" function is selected by default every time the device is switched on.
You can switch from every main function directly to the "Measure distance" function by pressing the
button.
If a measurement has already been taken, press the
button twice.
To repeat a function (Area, Volume, Pythagoras or Layout function), press the
button after the regular measurement procedure finishes.
The laser switches off automatically:
• When a single measurement has been carried out.
• When 90 seconds pass without a measurement being carried out.
• When you switch from a main function directly to the "Measure distance" function.
Short-press the
button to switch the laser on.
Aim the laser at a target point.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Previous measurement
• Measured distance
For more single measurements, switch the laser on and repeat the procedure.
Measuring area
Aim the laser at a target point for the room length.
Press the button.
Aim the laser at a target point for the room width.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Measured lengths
• Calculated result
Press button
and hold it down for 2 seconds to view the room perimeter.
Measuring wall areas (decorator function)
Aim the laser at a target point for the room length.
Repeat steps 1 to 3 until you have measured all the wall lengths.
Aim the laser at a target point for the room height.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Room perimeter
• Room height
• Wall area (decorator area)
Measuring volume
Aim the laser at a target point for the room length.
Press the button.
Aim the laser at a target point for the room width.
Press the button.
Aim the laser at a target point for the room height.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Room width
• Room height
• Calculated volume
Press button
and hold it down for 2 seconds to view the room perimeter and the wall area.
Measure Pythagoras (2-point)
Aim the laser at the first target point.
Press the button.
Aim the laser as the second target point at right angles to the target distance.
You can improve the result by activating the "Min/Max" function.
Press the
button and hold it down for 2 seconds to activate.
Measure the wall vertically until the length has been measured at exactly a right angle.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Measured lengths
• Calculated result
Measure Pythagoras (3-point)
Aim the laser at the first target point.
Press the button.
Aim the laser as the second target point at right angles to the target distance.
You can improve the result by activating the "Min/Max" function.
Press the
button and hold it down for 2 seconds to activate.
Measure the wall vertically until the length has been measured at exactly a right angle.
Press the button.
Aim the laser at the third target point.
Press the button.
Measurement has been completed.
The following values are shown on the display:
• Second length
• Third length
• Calculated result
Using the Layout function
Use the and buttons to set the distance between the layout points.
Press the button to confirm the value.
Take the measurement by passing the laser range meter along the layout baseline.
The following values are shown on the display:
• Distance between the nearest layout point and the wall
• Distance from the nearest layout point
An acoustic signal sounds inside a range of 10 cm from the nearest layout point.
A different acoustic signal sounds when the layout point is reached (display shows
0.000 ).
A minus sign (-) in front of the value indicates that you have to move away from the wall.
Press the button to end measurement.
Special functions
Adding or subtracting measurements
You can use the "Add/Subtract" function to add or subtract the measured values of different functions.
The following functions are compatible:
• Measure distance
• Measuring area
• Measure volumes
• Pythagoras (2-point)
• Pythagoras (3-point)
Use one of the compatible functions.
Press the button if you want to add a new measured value or press the button if you want to subtract.
Take another measurement.
If you are using the "Measure distance" function, the result appears automatically. If you are using the Area, Volume or Pythagoras function, you have to press the
button after completing the regular process of measurement.
The following values are shown on the display:
• Previous measurements
• Sum of/difference between measurements
Retrieving or deleting data from data memory
The product can save a maximum of 10 measured values in its data memory.
Every subsequent measurement automatically deletes the oldest measured value.
Press the button.
The 10 most recent measured values are displayed.
Use the or buttons to browse through the measured values in memory.
Alternatively, repeatedly press the
button.
Simultaneously press the and buttons and hold them down for 2 seconds to delete the measured values saved in the device's data memory.
All measured values are deleted from the device's data memory.
Taking a continuous measurement (min/max)
Press the button and hold it down for 2 seconds to start measuring.
The following values are shown on the display:
• Maximum value
• Minimum value
• Current measured value
Press the button to stop measuring.
The following values are shown on the display:
• Maximum value
• Minimum value
• Last measured value
Taking delayed measurement (timer function)
Delayed measurement (timer function) enables precision measurements over long distances.
Measurement takes place automatically when a countdown time out. This rules out slight movement of the laser range meter such as can occur when a button is pressed, for example.
The timer function can be used in all the main functions.
The default is 5 seconds.
Press the button and hold it down for 2 seconds.
Use the and buttons to set the timer.
Press the button to confirm the value.
The countdown starts.
Using Bluetooth Smart
Bluetooth Smart enables you to transmit measured values to a mobile device using an app.
You need an app from an official
Hilti partner in order to use the function. Before using Bluetooth Smart, install an appropriate app on you mobile device.
You can find the apps of official
Hilti partners by scanning the following QR code:
qr.hilti.com/r9121031
Press the button and hold it down for 2 seconds to switch Bluetooth on.
Establish a connection between the mobile device and the laser range meter.
Fault codes
Press the
or
button to hide a fault code.
If a fault code not listed here appears, switch the product off and then on again.
Contact
Hilti Service if the fault code re-appears.
Malfunction
Possible cause
Action to be taken
204
Calculation error
Take the measurement again.
220
General hardware fault.
Contact Hilti Service.
240
Fault in data transmission
Connect the product and try again.
252
Product has overheated.
Allow the product to cool down.
Comply with the specified operating and storage temperatures.
253
The product is too cold.
Warm up to the product.
Comply with the specified operating and storage temperatures.
255
Incoming signal too weak, measurement takes too long.
Change the target surface (e.g. white paper).
256
Incoming signal too high
Change the target surface (e.g. white paper).
257
Target surface too bright
Darken the target surface.
trc
Distance was less than the minimum measurable distance.
Measure within the laser range meter's stated measuring range (minimum 0.05 m).
Distance was greater than the maximum measurable distance.
Measure within the laser range meter's stated measuring range (maximum 100 m).
Care, transport and storage
Cleaning
Do not touch the lens with the fingers.
Clean the lens by blowing off dust or by wiping with a clean, soft cloth.
Use only pure alcohol or water for cleaning.
Do not dip the laser range meter into water.
Transport
The batteries must be insulated or removed from the product before it is shipped or sent by mail.
Use the Hilti packaging or packaging of equivalent quality for transporting or shipping your equipment.
Storage and drying
Do not put the product into storage when wet. Allow it to dry before putting it away.
Observe the temperature limits given in the Technical Data section which are applicable to storage or transport of the equipment.
Check the accuracy of the equipment before it is used after a long period of storage or transportation.
Disposal
WARNING
Risk of injury. Hazards presented by improper disposal.
Improper disposal of the equipment may have the following consequences: The burning of plastic components generates toxic fumes which may present a health hazard. Batteries may explode if damaged or exposed to very high temperatures, causing poisoning, burns, acid burns or environmental pollution. Careless disposal may permit unauthorized and improper use of the equipment. This may result in serious personal injury, injury to third parties and pollution of the environment.
Most of the materials from which
Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
Disposal of electric tools or appliances together with household waste is not permissible.
FCC statement / ISED statement
This product has been tested and found to comply with the limits for a class B digital device, pursuant to part 15 of the FCC rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. These products generate, use and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause interference to radio communications.
There is no guarantee that interference will not occur in a particular installation. If this product does cause harmful interference to radio or television reception, which can be determined by turning the product off and on, the user is encouraged to try to correct the interference by taking the following measures:
Re-orient or move the receiving antenna.
Increase the distance between the product and receiver.
Connect the product to a power outlet on a circuit different from that to which the receiver is connected.
Consult your dealer or an experienced TV/radio technician for assistance.
Changes or modifications not expressly approved by
Hilti may restrict the user’s right to operate the product.
This product complies with the requirements set out in Paragraph 15 of the FCC rules and in RSS 210 of IC.
Operation of the product is subject to the following conditions:
This product should cause no harmful interference.
This product must accept any interference received, including interference that may cause undesired operation.
FCC statement on RF radiationThe RF radiation of the product described is below the limits for portable devices stipulated by the FCC in accordance with KDB 447498.
Statement on RF radiationThe radio frequencies emitted by the product described are below the limits for portable devices imposed by Health Canada's Safety Code 6. The distance between the RF emitter and the user and/or uninvolved third parties is less than 20 cm.
Japanese Radio Law compliance
This device is granted persuant to the Japanese Radio Law (電波法).
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.