Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:
DANGER
DANGER !
Draws attention to imminent danger that will lead to serious personal injury or fatality.
WARNING
WARNING !
Draws attention to a potential threat of danger that can lead to serious injury or fatality.
CAUTION
CAUTION !
Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property.
Symbols in the documentation
The following symbols are used in this document:
Read the operating instructions before use.
Instructions for use and other useful information
Dealing with recyclable materials
Do not dispose of electric equipment and batteries as household waste
Symbols in the illustrations
The following symbols are used in illustrations:
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section
This symbol is intended to draw special attention to certain points when handling the product.
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:
General mandatory sign
Wear eye protection
Wear ear protection
Wear a hard hat
Return waste material for recycling
Highlighting of designations and markings
Designations and markings are indicated as follows:
‚ ‛
Description of marked operating controls on the fastening tool
« »
Markings on the fastening tool
Product information
Hilti products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
In the table below, enter the designation and serial number from the type identification plate.
Always quote this information when you contact a Hilti representative or Hilti Service to make an inquiry about the product. Product information
Product information
Fastening tool, gas-actuated
GX-IE GX-IE XL
Generation:
01
Serial number:
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration issued by the certification department can be found at the end of this documentation.
The technical documentation is filed and stored here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
Safety instructions
These safety instructions apply for fastening tools with and without magazine.
Working safely with the fastening tool
Pressing the nosepiece of the fastening tool against a part of the body may lead to serious injury due to inadvertent actuation and release of a fastener. Never press the nosepiece of the tool against your hand or any other part of the body.
When inserting/loading application-specific fasteners (e.g. washers, clips or clamps, etc.) in/on the fastener guide there is a risk of serious injury due to inadvertent actuation of the tool resulting in discharge of a fastener. When inserting/loading an application-specific type of fastener, never press a hand or any other part of the body against the fastener guide.
Never point the fastening tool towards yourself or any other person.
Keep your arms flexed when operating the tool (do not straighten the arms).
When pulling back the nail pusher, always take care to ensure that it engages.
When disengaging the nail pusher, do not release it and allow it to jump forward. Guide it forward slowly. There is a risk of pinching the fingers.
Do not attempt to drive fasteners into materials that are too hard , such as welded steel or cast steel. Attempting to drive fasteners into these materials may lead to malfunctions, incorrectly driven fasteners or breakage of fasteners.
Do not attempt to drive fasteners into materials that are too soft , such as wood or drywall/gypsum board. Attempting to drive fasteners into these materials may lead to malfunctions and fasteners being driven incorrectly or driven right through the material.
Do not attempt to drive fasteners into materials that are too brittle , such as glass or tiles. Attempting to drive fasteners into these materials may lead to malfunctions, fasteners being driven incorrectly and may cause the material to shatter.
Before driving fasteners, check that there is no risk of injuring persons or of damaging objects present behind or below the working surface.
Pull the safety trigger only when the fastening tool is pressed against the working surface in such a way that the fastener guide is pushed into the tool as far as it will go.
Always wear gloves if you have to carry out maintenance work on the fastening tool while it is still hot.
If fasteners are driven at a high rate or if the tool used for a long period, surfaces of the tool beyond the grip areas may get hot. Wear protective gloves to avoid burning injuries.
If the fastening tool overheats, remove the gas can and allow the tool to cool down. Do not exceed the specified maximum fastener driving rate.
Driving fasteners may cause flying fragments or result in parts of the nail strip material being forcibly ejected from the tool. Flying fragments present a risk of injury to the body and eyes. Wear eye protection, ear protection and a hard hat. Depending on the application and type of fastening tool in use, wearing personal protective equipment such as a dust mask, non-slip safety footwear, hard hat and ear protection reduces the risk of injury. Other persons in the vicinity must also wear eye protection and a hard hat.
Wear suitable ear protection ( see noise information in the technical data section). Fasteners are driven through ignition of a gas/air mixture. The resulting noise exposure may cause damage to the hearing. Other persons in the vicinity should also wear suitable hearing protection.
When driving a fastener, always hold the fastening tool securely and at right angles to the supporting material. This helps to avoid deflection of the fastener by the supporting material.
Never drive a second fastener at the same location. This may lead to breakage or jamming of fasteners.
Always remove the gas can and battery and empty the magazine before changing the magazine and before undertaking cleaning, servicing or maintenance work, in preparation for storage or transport and before leaving the fastening tool unattended.
To ensure that the fastening tool functions faultlessly and as intended, always check the tool and accessories for possible damage before use. Check that moving parts function faultlessly, without sticking, and that no parts are damaged. In order to ensure faultless operation of the fastening tool, all parts must be fitted correctly and must meet the necessary requirements. Damaged protective devices or other parts must be properly repaired or replaced by Hilti Service unless otherwise stated in the operating instructions.
Have the fastening tool repaired only by trained and qualified specialists using genuine Hilti spare parts. This will ensure that the safety of the fastening tool is maintained.
Tampering with or modification of the fastening tool is not permissible.
Do not use the fastening tool where there is a risk of fire or explosion.
Take influences of the surrounding area into account. Do not expose the fastening tool to rain or snow and do not use it in damp or wet conditions.
Use the fastening tool only in well-ventilated working areas.
Select the correct combination of fastener guide and fastener. The wrong combination may result in damage to the tool and in reduced fastening quality.
Always observe the application guidelines.
Hazards presented by electricity
Before beginning work, check the working area (e.g. using a metal detector) to ensure that no concealed electric cables or gas and water pipes are present.
Hold the fastening tool only by the insulated grip when working in areas where fasteners may be driven inadvertently into concealed electric cables. Contact with a live electric cable may cause metal parts of the fastening tool also to become live, leading to a risk of electric shock.
Use and care of battery-powered tools
Check that the tool is switched off before inserting the battery. Inserting a battery into an electric tool that is switched on can lead to accidents.
Do not expose batteries to high temperatures, the direct heat of the sun, and keep them away from fire. There is a risk of explosion.
Do not disassemble, squash or incinerate batteries and do not subject them to temperatures over 80°C. This presents a risk of fire, explosion or injury through contact with caustic substances.
Avoid ingress of moisture. Ingress of moisture may cause a short circuit, resulting in burning injuries or fire.
Use only batteries of the type approved for use with the applicable tool. Use of other batteries or use of the batteries for purposes for which they are not intended presents a risk of fire and explosion.
Observe the special guidelines applicable to the transport, storage and use of Li-ion batteries.
Remove the battery from the tool before transport or storage.
Avoid short circuiting the battery terminals. Check that the contacts on the battery and on the tool are free from foreign objects before inserting the battery into the tool. Short circuiting the battery terminals presents a risk of fire, explosion and chemical burns.
Do not continue to use or attempt to charge damaged batteries (e.g. batteries with cracks, broken parts, bent or pushed-in / pulled-out contacts).
A battery that is too hot to hold may be defective. Allow the battery to cool down in a place where there is no risk of causing a fire. Check that there are no flammable materials nearby. Contact Hilti Service.
Instructions for handling the propellant gas
Observe the instructions printed on the gas can and in the accompanying information.
Escaping gas is harmful to the lungs, skin and eyes. Keep your face and eyes away from the gas can compartment for up to about 10 seconds after removing the gas can.
Do not operate the gas can valve manually.
If a person has inhaled gas, take the person into the open air or into a well-ventilated area and place the person in a comfortable position. Consult a doctor if necessary.
Call a doctor if the person is unconscious. Bring the person into a well-ventilated area and place the person in the stable recovery position (i.e. lying on the side). If the person is not breathing, administer artificial respiration and, if necessary, supply oxygen.
After eye contact with gas, rinse the open eyes thoroughly under running water for several minutes.
After skin contact with gas, wash the contact area carefully with soap and warm water. Subsequently apply a skin cream.
General instructions concerning personal safety
Take care to adopt an ergonomic body position. Work from a safe stance and take care to stay in balance at all times. This will allow you to control the fastening tool better, even in unexpected situations.
Keep other people away from the working area, especially children.
Description
Product overview
Fastener guide
Fastener guide release slider
Belt hook
Safety trigger
Cooling air slots
Gas can compartment
Battery release button
Battery state of charge indicator
Gas can status indicator button
Gas can status indicator
Battery
Intended use
The product described is a gas-actuated fastening tool. It is for driving suitable fasteners into concrete and other materials suitable for use of the direct fastening technique.
The fastening tool, gas can, battery and fasteners form a technical unit. This means that trouble-free fastening with this fastening tool can be ensured only when it is used together with the fasteners, gas cans and batteries specially manufactured for it by
Hilti . The fastening and application recommendations made by
Hilti apply only when these conditions are observed.
The fastening tool is for hand-held use only.
Use only Hilti Li‑ion batteries of the B 12 series with this product.
Use only Hilti battery chargers of the C 4/12-50 series for charging these batteries.
Items supplied
Gas-actuated fastening tool with fastener guide, 2 batteries, charger, toolbox and operating instructions.
Other system products approved for use with this product can be found at your local
Hilti Center or online at:
www.hilti.com
Fastener guide
The fastener guide holds the insulation plug and in the driving process it directs the fastener to the desired position in the material.
Fastener guide release slider
In the
EJECT position, the slider releases the fastener guide for removal.
Status
Meaning
EJECT
Fastener guide release
Belt hook
The belt hook can be extended in three stages.
Status
Meaning
Position 1
Position for attaching to a waist belt
Position 2
Position for attaching to ladders, scaffolds, platforms, etc.
Position 3
Belt hook removed
Gas can
Observe the safety instructions provided with the gas can!
In order to operate the fastening tool, the gas can must be inserted in the gas can compartment.
The gas can status can be read from the LED display after pressing the
GAS button.
The gas can must be removed before breaks between working, before maintenance and before transporting or storing the fastening tool.
Indication of gas can status
After pressing the
GAS button, the LED display indicates the status of the gas can.
Status
Meaning
All four LEDs light green.
The level is between 100 % and 75 %.
Three LEDs light green.
The level is between 75 % and 50 %.
Two LEDs light green.
The level is between 50 % and 25 %.
One LED lights green.
The level is between 25 % and 10 %.
One LED blinks green.
Level is below 10 %. Replacement of the gas can is recommended.
The gas can is empty or is malfunctioning. Replacement of the gas can is recommended.
Even when the level is indicated as “empty”, the gas can, for technical reasons, still contains a little gas.
One LED blinks red.
No gas can or the wrong type of gas can is present in the fastening tool.
Indication of battery charge status
After pressing a battery release button, the display shows the status of the battery and the fastening tool.
Status
Meaning
All four LEDs light green.
Charge status is 75 % to 100 %.
Three LEDs light green.
Charge status is 50 % to 75 %.
Two LEDs light green.
Charge status is 25 % to 50 %.
One LED lights green.
Charge status is 10 % to 25 %.
One LED blinks green.
Charge status is below 10 %.
The fastening tool is overloaded or overheated and thus not ready for operation.
Technical data
Fastening tool
Weight (empty) GX 2-IE
3.3 kg (7.3 lb)
Weight (empty) GX 2-IE-XL
3.4 kg (7.5 lb)
Tool length for GX 2-IE
500 mm (19.7 in)
Tool length for GX 2-IE-XL
550 mm (21.7 in)
Application temperature, ambient temperature
−10 ℃ … 45 ℃ (14 ℉ … 113 ℉)
Maximum fastener length
39 mm (1.5 in)
Maximum fastener length for GX 2-IE-XL
200 mm (7.9 in)
Fastener diameter
60 mm (2.4 in)
3.90 mm (0.154 in)
Compression stroke
20 mm (0.8 in)
Maximum fastener driving frequency (Fasteners per hour)
800
Loading the fastening tool
Equipment required for driving fasteners
The fasteners are pushed manually on to the fastener guide.
Inserting the gas can
If you are using a new gas can, remove the transport safety device.
Open the gas can compartment cover.
Push the gas can (with metering valve fitted) into the red adapter in the gas can compartment.
Close the gas can compartment cover.
Inserting the battery
Check that the contacts on the battery and on the fastening tool are undamaged and free from foreign objects.
Fit the battery and make sure that it is heard to engage.
Once the battery has been fitted, the charge status LEDs light for a short time.
CAUTION
A falling battery presents a hazard. If the battery is not secured correctly it may drop out and fall while the work is in progress.
Check that the battery is seated securely.
Check that the battery is securely seated in the fastening tool.
Driving fasteners
WARNING
Risk of injury due to accidental actuation! The uncontrolled driving of a fastener can cause serious injury
Never press the nosepiece of the tool against your hand or any other part of the body.
Never pull back the magazine, fastener guide or fastener by hand.
Penetrate the insulating material with the fastener that is on the fastener guide.
Press the fastening tool against the working surface as far as it will go (until fully compressed).
Make sure that the fastener guide is perpendicular to the working surface and is seated against the insulation.
Pull the safety trigger to drive a fastener.
It is not possible to drive a fastener if the fastening tool and the fastener are not pressed fully against the working surface.
Lift the fastening tool completely away from the working surface after driving a fastener.
When you finish work or are going to leave the fastening tool unattended, remove the gas can ( ) and the battery ( ).
Unloading the fastening tool
Removing the battery
Press the release button and pull the battery out of the fastening tool.
Removing the gas can
Open the gas can compartment.
Remove the gas can.
Close the gas can compartment.
Optional operating steps
Removing the transport safety device from a new gas can
Lift the transport safety device, containing the metering valve, away from the gas can.
Remove the metering valve from the transport safety device.
Fit the metering valve onto the gas can, with the foremost of the two grooves on the lip of the can.
Press the metering valve firmly onto the gas can, bringing the rearmost groove towards the lip of the can, until the metering valve is heard to snap into place over the lip and it then lies flush with the can.
Checking the status of the gas can
After inserting the battery, press the GAS button without pressing the fastening tool against the working surface.
Read the gas can status from the display.
Removing the fastener guide
Remove the battery.
Remove the gas can.
Move the fastener guide release slider to the EJECT position.
Remove the fastener guide.
Inserting the fastener guide
Remove the gas can.
Remove the battery.
Push the fastener guide release slider in the direction indicated by the arrow to the EJECT position and hold it there.
The fastener guide can be inserted only when the slider is held in the
EJECT position.
Slide the fastener guide into the slot in the nose of the fastening tool until it engages with an audible click.
Check that the fastener guide is seated correctly.
Remedying possible malfunctions
Removing foreign objects from the area of the fastener guide
Remove the battery.
Remove the gas can.
Remove the fastener guide.
Remove all foreign objects from the area of the fastener guide.
Insert the fastener guide.
Care and maintenance
Caring for the fastening tool
Clean the fastening tool regularly with a cloth.
Keep the grip areas free from oil and grease.
Do not use spray equipment, pressure jet washers or running water for cleaning.
Do not use cleaning agents containing silicone.
Do not use sprays or similar lubricating and cleaning agents.
Never operate the fastening tool if the cooling air slots are blocked.
Cleaning the fastening tool
The fastening tool must be cleaned and serviced regularly. We recommend that a cleaning service is carried out, at the latest, after driving 25,000 fasteners.
Clean the fastening tool, or have it cleaned, if malfunctions such as misfiring occur increasingly.
For cleaning, use the cleaning set (available as an accessory) and observe the illustrated cleaning instructions enclosed with it.
Maintenance
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local Hilti Center or online at: www.hilti.group .
Check all external parts of the fastening tool for signs of damage at regular intervals and make sure that all the controls function correctly.
Do not use the fastening tool if parts are damaged or if the controls do not function correctly.
Have a defective fastening tool repaired by Hilti Service.
Remove the gas can and then reinsert it. If the problem persists, use a new gas can.
Remove the battery and then reinsert it.
Fastener does not penetrate deeply enough into the material.
The system is unsuitable. The supporting material is too hard.
Switch to a Hilti DX system.
Drive energy too low.
Check the tool. Contact Hilti Service.
Surface of the material is too uneven.
Surface of the material is too uneven.
Switch to a Hilti DX system.
Disposal
Most of the materials from which
Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
Do not dispose of power tools, electronic equipment or batteries as household waste!
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.
FCC statement (applicable in US) / IC statement (applicable in Canada)
This device complies with Part 15 of the FCC Rules and RSS-210 of IC. Operation is subject to the following two conditions:
This device shall cause no harmful interference.
This device must accept any interference received, including interference that may cause undesired operation.