Quantity Updated
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
![]() |
Li-ion battery |
![]() |
Never use the battery as a striking tool. |
![]() |
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. |
![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Rated speed under no load |
![]() |
Revolutions per minute |
![]() |
Direct current (DC) |
![]() |
Diameter |
![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions. |
![]() |
The numbering in the illustrations reflects the order of the work steps in the illustration and may deviate from the numbering of work steps in the text. |
![]() |
Item reference numbers are used in the overview illustration. In the product overview section, the numbers shown in the legend relate to these item reference numbers. |
Drill |
SF BT 22‑A |
Generation: |
01 |
Serial no.: |
The product described is a hand-held cordless drill designed for drilling blind holes in steel using Hilti TX‑BT… stepped drill bits which is a prerequisite for driving Hilti X‑BT threaded studs.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group
Status |
Meaning |
---|---|
4 LEDs light. |
Charge status: 75 % to 100 % |
3 LEDs light. |
Charge status: 50 % to 75 % |
2 LEDs light. |
Charge status: 25 % to 50 % |
1 LED lights. |
Charge status: 10 % to 25 % |
1 LED blinks, the power tool is ready for use. |
Charge status: < 10 % |
1 LED blinks, the power tool is not ready for use. |
The battery has overheated or is completely discharged. |
4 LEDs blink, the power tool is not ready for use. |
The power tool is overloaded or has overheated. |
Rated voltage |
21.6 V |
Weight including battery B22⁄8.0 |
5.7 lb (2.6 kg) |
Torque |
≤ 7 ftlbf (≤ 9 Nm) |
Keyless chuck clamping range |
3/64 in … 25/64 in |
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The battery doesn’t engage with an audible double click. |
The retaining lugs on the battery are dirty. |
|
The control switch can’t be pressed, i.e. the switch is locked. |
The safety lock is engaged. |
|
The power tool doesn’t run. |
The battery is not fully inserted. |
|
The tool doesn’t work and one LED blinks. |
Low battery. |
|
The tool cuts out while operating, the 4 LEDs on the battery display blink. |
The overload cut-out has been activated. |
|
The overheating cut-out has been activated. |
|
|
The battery runs down more quickly than usual. |
Very low ambient temperature. |
|
The tool or battery gets very hot. |
The tool is overloaded (application limits exceeded). |
|
To see account specific prices and content, please choose appropriate account.