Update quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
![]() |
Read the operating instructions before use |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
![]() |
Do not transport by crane |
![]() |
Bluetooth (optional) |
Water management system |
DD-WMS 100 |
Generation |
01 |
Serial no. |
Operating button |
Description |
---|---|
![]() |
Off |
![]() |
Recycling mode |
![]() |
Water supply mode |
![]() |
Vacuum cleaner mode |
![]() |
Bluetooth (optional) |
Operating button |
LED status |
Description |
---|---|---|
![]() |
LED off |
Bluetooth is switched off. |
LED pulsing |
Bluetooth is switched on. No connection to another device. |
|
LED flashes |
Bluetooth is switched on. Coupling process is running. |
|
LED lights up continuously |
Bluetooth is switched on. Connected to another device. |
LED |
Description |
---|---|
![]() |
The water level is too low. Fill the water and waste material container up to the MAX mark. |
![]() |
The water level is too high. Switch to water supply mode until the indicator goes out. |
![]() |
No filter Fit the filter bag fitted correctly. |
Display icons |
Description |
---|---|
![]() |
The filter bag is missing or is not correctly installed. This WMS 100 is not ready for use. Fit the filter bag fitted correctly. |
![]() |
Too much water in the water and waste material container. The WMS 100 produces no vacuum. Switch on the water supply mode until the MAX service display goes out. |
![]() |
Too little water in the water and waste material container. A functioning water supply is no longer ensured. Fill the water and waste material container up to the MAX mark. |
DD-WMS 100 |
|
---|---|
Protection class |
I |
Protection class |
IPX4 |
Weight in accordance with EPTA procedure 01/2003 |
43.4 lb (19.7 kg) |
Weight of the hose set |
4.0 lb (1.8 kg) |
Operating temperature |
37 ℉ … 104 ℉ (3 ℃ … 40 ℃) |
Recommended temperature range for transport and storage (without water in the container) |
−13 ℉ … 158 ℉ (−25 ℃ … 70 ℃) |
Suction hose length |
16 ft (5 m) |
Pressure hose length |
16 ft - 9 in (5.1 m) |
Supply cord length |
15 ft - 9 in (4.8 m) |
Container capacity |
32 ℓ |
Water capacity |
14 ℓ |
Volumetric flow rate (air) |
≤ 74 ℓ/s |
Water flow rate |
≤ 3 ℓ/min |
Water pressure |
≤ 100 psi (≤ 7 bar) |
Frequency band |
2,400 MHz … 2,483 MHz |
Maximum emitted transmission power |
10 dBm |
Malfunction |
Possible cause |
Action to be taken |
---|---|---|
![]() |
Too much water in the water and waste material container. |
|
The float is stuck. |
||
![]() |
Too little water in the water and waste material container. |
|
![]() |
The filter bag is missing or is not fitted correctly. |
|
The connection between the water hose and the appliance is stiff to operate. |
The connecting nipple is dry and/or dirty. |
|
The filter bag holder is pulled up when the top section of the appliance is lifted |
Internal water connector parts are dry and/or clogged. |
|
No water or too little water flows although there is adequate water in the container. |
The prefilter is blocked. |
|
The water hose connector nipple is blocked. |
|
|
The mesh filter on the drilling machine water connection is clogged. |
|
|
No suction or reduced suction performance. |
The filter bag is clogged. |
|
The flow indicator sight glass is dirty. |
Dirt deposits. |
|
The appliance doesn’t start in REC or VAC mode. |
The float is stuck. |
|
Another diamond core drilling machine has automatically connected to the accessory used (e.g. water treatment system) via Bluetooth. |
Several diamond core drilling machines are connected to the same accessory. The accessory always connects automatically to the diamond core drilling machine that enables the connection to be established fastest. |
|
The WMS 100 is not found by the Hilti Connect app or the diamond core drilling machine. |
(app only): The WMS 100 is connected to a diamond core drilling machine. |
|
(also diamond core drilling machine): Bluetooth is deactivated. |
To see account specific prices and content, please choose the appropriate account.